Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release07 September 2022Digital IndustriesNuremberg
New technology functions for Sinumerik One simplify operation and increase productivity
Under the motto "Accelerate digitalization for a sustainable tomorrow", Siemens will be demonstrating at this year's AMB how the enormous potential for optimizing machine tools can be utilized thanks to the continuous analysis of production data.
With the new Y-turning
function, Sinumerik One can now be used for machines that turn from the Y-axis,
enabling up to 3 times the feed rate and resulting in increased productivity.
New tool types were created for this purpose and all turning functionalities
and cycles were adapted for these tools.
The Advanced Rapid Movement
function is also one of the innovations in the technology functions. It enables
time-optimized movement, which means that faster movements take place between
machining operations. The part program does not have to be changed for this.
Overall, machining can be up to ten percent faster. The function must be
implemented together with the machine builder.
With Reduced Dynamic Mode,
there is now a function that reduces wear on the machine and thus increases its
availability. The NCK function enables the machine tool builder to
automatically transfer the machine tool to reduced operation, for example if
the axis becomes too warm. On the other hand, the machine can also be returned
to full load. In this way, the Reduced Dynamic Mode enables individual
operation in motion.
In the area of hardware,
there are also innovations for the Sinumerik One that are designed to simplify
operation: The new keyboards and Machine Control Panels (MCPs) are now
available from 15 to 24 inches consistently to match the HMI. And the Simatic
Industrial Thin Clients (ITCs) and industrial PCs are being launched with
increased performance and a resolution of up to 1920 x 1080 pixels.
The new MCPs are also
integrated in the digital twin of Sinumerik One (Create and Run MyVirtual
Machine), so that the appearance and operation here correspond to the real CNC
in every respect. In addition, the digital twin of Sinumerik One has been given
new features that simplify engineering and work preparation. To mention just a
few of the many innovations: The /3D option offers support for a second
channel. In addition, each tool can be assigned an individual color, so that
the ablated surfaces are color-coded depending on the tool used. The import of
STEP format is an important feature especially for complex geometries of the
clamping situation of a turning operation. Collision detection now also offers
extensive functionalities such as the display of all collided bodies, NC
program line and much more, so that the cause of collisions can be quickly
investigated and eliminated.
Background information Sinumerik One
Sinumerik One plays a
central role in the transformation of machine tools in the age of Industry 4.0,
outperforming previous generations of controllers in terms of PLC and CNC
performance in machine operation, cutting speed, and data capture and
processing power. With its integrated Simatic S7-1500F PLC, it offers up to 10
times faster PLC cycle times. With the Simatic S7-1500F PLC, Sinumerik One is
fully integrated into the TIA Portal engineering framework, enabling
standardization of all engineering tasks for operators of larger plants.
Sinumerik One is fully compatible with the previous Sinumerik 840D sl
controller generation in terms of programming and operation. This makes the
changeover to Sinumerik One even easier.
With Sinumerik One, Siemens
offers the technology to easily create and work with digital twins of machine
tools. Work preparation and engineering departments can also benefit from the
digital twin. Siemens offers a comprehensive user interface for Sinumerik One
that enables convenient, flexible, and efficient operation of machine tools
across all technologies.
For this press release
Follow us on social media channels
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 72,000 employees internationally.
Siemens AG (Berlin and Munich) is a technology company focused on industry, infrastructure, transport, and healthcare. From more resource-efficient factories, resilient supply chains, and smarter buildings and grids, to cleaner and more comfortable transportation as well as advanced healthcare, the company creates technology with purpose adding real value for customers. By combining the real and the digital worlds, Siemens empowers its customers to transform their industries and markets, helping them to transform the everyday for billions of people. Siemens also owns a majority stake in the publicly listed company Siemens Healthineers, a globally leading medical technology provider shaping the future of healthcare. In addition, Siemens holds a minority stake in Siemens Energy, a global leader in the transmission and generation of electrical power. In fiscal 2021, which ended on September 30, 2021, the Siemens Group generated revenue of €62.3 billion and net income of €6.7 billion. As of September 30, 2021, the company had around 303,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.