- Research project for an optimized transport system (OTS)
- Mobility offering for the first and last mile
- Testing the interplay of intelligent infrastructure, cloud-based software services and autonomous electric vehicles
Siemens Mobility is launching a field test for autonomous driving at the Siemens campus in Munich-Perlach, Germany. Working with partners IAV GmbH, Institute for Climate Protection, Energy and Mobility (IKEM) e.V., emm Solutions GmbH, UTB Projektmanagement GmbH and the Technical University of Munich (TUM), Siemens Mobility is initiating a research project and field test. The test route runs through the campus and enables traffic simulation in a variety of real-life situations.
Connected and self-driving vehicles are on the horizon. Autonomous taxis and minibuses could cover the last mile between homes and public mass transit and long-distance transport hubs, helping make private cars superfluous in cities and relieving congestion. In rail transport as well, fully automated systems and connectivity can help satisfy the rapidly growing demand for mobility. Making vehicles and infrastructure more intelligent can ensure better availability and make mobility safer. All this adds up to vastly improved urban environments.Siemens is working with municipalities, public transit authorities and research institutes to develop these transport concepts.
- 18 Desiro HC double-decker trains enter service in Franconia and southern Thuringia in December
- more seats, high level of comfort, cutting-edge technology
- 30-minute service intervals between Nuremberg and Bamberg
- over 10,000 additional seats per day
- eight more trains coming as of June 2024
The movement to
modernize regional transport continues to gain momentum: When the timetable
changes in December 2023, 18 new Desiro HC double-decker trains from Siemens
Mobility will inaugurate service for the Franconia-Thuringia Express. With a
top speed of 160 kilometers per hour, 380 seats, spaces for 36 bicycles, WiFi
service, high-frequency windowpanes that significantly improve cellphone
reception, as well as an electronic passenger information system with 27
monitors, the new Franconia-Thuringia Express operated by DB Regio Bayern
offers a special experience for its passengers. The new trains will operate on
many routes in the future, such as between Nuremberg and Bamberg daily between
5:00 a.m. and 10:00 p.m. every 30 minutes in both directions. The trains will
provide over 10,000 additional seats on this route. DB Regio Bayern and
Bayerische Eisenbahngesellschaft (BEG), which plans, finances and controls
regional and S-Bahn transport on behalf of the state of Bavaria, presented the
new train today together with Siemens Mobility at the Bamberg main station,
followed by a press tour through Franconia. The states of Bavaria and Thuringia
are investing a total of €320 million in the new train fleet to expand regional
transport capacities.
- Charging infrastructure for one of Australia’s leading bus manufacturers
- Siemens digital depot management solution for reporting and monitoring function
- Supports uptake of low emission transport across Australia
One of Australia’s leading bus manufacturers, Custom Denning, has selected Siemens’ electric bus charging stations and digital depot management solution forits fleet of fully Australian designed and built Element electric buses. The charging stations will support the bus manufacturer’s prototype electric buses and be available for future eBus orders of its customers.
- 90 new trains in size XXL
- For the first time, all cars are completely integrated and set new standards
with a train length of over 200 meters
- Financing guaranteed by
the State of Bavaria
Passengers on Munich’s S-Bahn can soon look
forward to traveling on the most modern S-Bahn trains in Germany. Siemens
Mobility will deliver 90 superlative new S-Bahn trains worth more than two
billion euros after winning an EU-wide tender. The contract includes an option
for additional trains. Financing for the trains is guaranteed by the State of
Bavaria through a leasing model.
- Campus Nyland test, training and signaling simulation center opens
- European Rail Traffic Management System (ERTMS) latest in intelligent infrastructure
- Nordlandsbanen will open first digital signaling railway in October 2022
Bane NOR and Siemens Mobility celebrated the opening of Campus Nyland, a test, training and signaling simulation center which will help the rail network operator prepare for the digitalization of the entire system. Norway has committed to becoming the first country to operate with a single digital interlocking and ERTMS signifies one of the country’s largest digitalization projects. In 2022, the first digital line, Nordlandsbanen, will open. In advance, the Campus Nyland center will prepare workers for working within the digital system, ERTMS. The intelligent infrastructure behind ERTMS will reduce operating costs and increase capacity throughout the network. In addition, it will enhance safety, with real-time visibility of trains across the network. When complete in 2034, the system will include 4,200 km of track and more than 350 stations.
- New
fleet with significant improvement in services
- Increased climate-friendly
mass transit
- State-of-the-art train interiors
DB Regio Bayern and train manufacturer Siemens
Mobility will put a total of 57 new trains in service in Bavaria beginning in
December 2023. Twenty-six Desiro HC trains are currently being built for the
Franconia-South Thuringia network, along with 25 Desiro HC double-decker trains
and six Mireo trains for the Danube-Isar network. The 18 Desiro HC trains will
operate in the Franconia-South Thuringia network as four-car units beginning in
December 2023 and eight Desiro HC trains as six-car units in June 2024. They
travel almost as fast as the ICE, for example between Coburg and Erfurt at 190
kmh. In the Danube-Isar network, the 31 new trains will inaugurate service in
December 2024.
Bane NOR, the state-owned agency responsible for the Norwegian national railway infrastructure, has contracted Siemens to upgrade the signaling equipment of the entire Norwegian rail network to the European Train Control System (ETCS). Commissioning of the rollout lines is scheduled to be completed by 2034. The contract also includes services for 25 years and is worth around 800 million euros in total.
- Siemens Energy Corporate Center in Berlin
- Joint location and structural concept planned with the State of Berlin
- Company's administrative
headquarters remain in Bavaria
Siemens Energy, as a stand-alone company,
will locate its Corporate Center in Berlin. The energy technology company with
worldwide 91,000 employees, which in 2019 generated revenue of €28.8 billion,
is thus returning to its roots: Werner von Siemens and Johann Georg Halske
founded their company in Berlin in 1847 and with the discovery of the
electrodynamic principle in 1866 laid a foundation for today's Siemens Group
and therefore today's Siemens Energy.
The VAG Verkehrs-Aktiengesellschaft Nuremberg has ordered 27 type G1 four-car metro trains from Siemens Mobility. The contract also includes an option for a total of a further 7 trains. These trains are earmarked for service on Nuremberg's U1 line. The trains will be built in the Siemens Mobility plant in Vienna. Core components of the G1 will be manufactured in the Nuremberg metropolitan area and include such products as the drive converters, traction motors, auxiliary converter units and control equipment. The project management, development and service support will be provided from Erlangen.