Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Greater comfort and more attractive offers for regional rail: 57 new trains will serve the Franconia-South Thuringia and Danube-Isar networks
Mireo Danube-Isar network
Desiro HC Franconia-South Thuringia network/Danube-Isar network
Mireo Danube-Isar network
Mireo Danube-Isar network
Mireo Danube-Isar network
Desiro HC Franconia-South Thuringia network/Danube-Isar network
Desiro HC Franconia-South Thuringia network/Danube-Isar network
Desiro HC Franconia-South Thuringia network/Danube-Isar network
Facts and figures
Siemens Mobility has been commissioned by DB Regio Bayern to deliver 18 four-car and eight six-car Desiro HC double-decker electric trainsets for the Franconia-South Thuringia network. Passenger service with the four-car Desiro HC is scheduled to begin in December 2023. The trains will be used on the lines RE 20 Nuremberg – Bamberg – Würzburg, RE 42 Nuremberg – Bamberg – Lichtenfels – Saalfeld, RE 49 Nuremberg – Bamberg – Lichtenfels – Coburg - Sonneberg, and RB 25 Bamberg – Kronach.
In December 2024, the new Desiro HC and Mireo trains will also be inaugurated in the Danube-Isar network. The Desiro HC trains are designated for use on the line RE 3 Munich – Landshut– Plattling – Passau and on the line RB 33 (Munich) – Freising – Moosburg – Landshut until the opening of the second main S-Bahn line through Munich. The Mireo trains will be used on the line RE 22 Munich Airport Terminal – Landshut– Regensburg. Following the opening of the second main S-Bahn line in Munich, the RB 33 trains will be used to increase the frequency of service between Munich and Regensburg or Plattling during rush hours. The four-car Desiro-HC-trains have 360 seats in 2 nd class and 20 seats in 1 st class. Up to three Desiro HC trains can be coupled for greater flexibility and capacity. The double-decker trains are barrier-free for passengers with limited mobility. At platforms with a standard height of 76 cm, wheelchair users can board and exit the trains without assistance. There is also a doorway lift for wheelchair users to facilitate boarding and exiting at stations with lower platforms.