- New Edge applications for workpiece and process quality, machine availability and process optimization
- Analyze MyWorkpiece /Vision and Optimize MyMachining /Magazine based on artificial intelligence
- Manage MySinumerik Edge for the central control and condition monitoring of Edge devices
Siemens has extended its Industrial Edge offerings for the machine-oriented Sinumerik Edge to include more new applications. With the new software, the company is helping machine tool users to improve workpiece and process quality, increase machine availability, and further optimize machine processes. With Edge Computing, large volumes of data can be processed locally on the machine tool. This also reduces storage and transmission costs for users, as large data volumes can be preprocessed and only the relevant data then transferred to a cloud or IT infrastructure.
- Using proven hardware and software, Siemens develops a solution for social distancing at the workplace
- Companies can simulate and manage the possible risks to their employees while at the same time increasing the productivity of their plants
- Simatic Real-time Locating Systems (RTLS) plus SieTrace software provide location information which customers can use to control their manufacturing processes and to design their operating procedures future-proof
Siemens uses a combination of hardware and software to offer a new solution for the challenges that companies face as a result of the Covid-19 pandemic. The solution enables companies to quickly and efficiently control how employees interact with one another, with the production line and with the plant setup. The integrated digital twin helps the company to simulate the safety of employees, to test and optimize the setup of work areas, to validate safety measures, and thus to design future-proof production lines.
- New version 8.0 facilitates integration of Simatic S7-1500 controller as well as mixed operation with Simatic S7-400 controller operation with the Simatic S7-400 controller
- Improved production and batch transparency with new MES reporting options
- Enhanced safety concept with new functions
- Lean Edition for micro breweries and craft brewers
Siemens is presenting a new version of the Braumat brewery process control system at the BrauBeviale in Nuremberg: The latest version 8.0 is based on the Simatic S7-1500 controller and has been optimized in the areas of reporting, weighing systems and security. Already installed Simatic S7-400 controllers can still be used, including in mixed operation. Existing Braumat installations can be expanded or modernized with Simatic S7-1500 controller. Production downtimes caused by new installations are thus avoided.
- AnalyzeMyWorkpiece /Monitor enables continuous monitoring of workpiece production
- Quality control takes place immediately during production
- New application extends the range of existing applications for quality assurance
With AnalyzeMyWorkpiece /Monitor, Siemens is extending its software portfolio for machine tools for workpiece quality. The Edge application based on high-frequency data, which will be presented at EMO 2019, enables continuous monitoring of workpiece production in machine tools. Measured values such as position data, torque values or control deviations together with context information, for example the tool currently being used, are acquired from the machine with high frequency and without feedback via Sinumerik Edge. The measured values are compared continuously with a reference model. In the event of deviations that exceed a predefined level, the application logs the result, sends it to the machine tool and enables prompt responses by the operator. This means, for example, that unique process-parallel quality control is supported during production.
- First-of-its-kind drilling rig project will implement customized BlueDrive™ system to replace obsolete system
- New system will use existing footprint, cabling and communication points for greater safety and quick commissioning
Siemens was awarded a contract by Arabian Drilling Company to modernize a complete and integrated drilling-drives lineup, including auxiliaries and controls, that will be installed on an offshore jackup drilling rig for a customer in the Middle East. In addition to new features and benefits, the upgrade will also enable the customer to meet the latest safety standards. Delivery of the new system is planned for the early part of 2021.
- New devices for electrical installations in industrial and infrastructure environments with a lower nominal current of 0.1 to 0.4 amperes
- Firmware update with improved control and diagnostic functions
- Failsafe group shutdown function without additional wiring
Siemens Smart Infrastructure is adding four new devices to its portfolio of Simatic ET 200SP motor starters, which can be used to start electric drives with a power output from 0.1 to 0.4 amperes (A). These types of drives are found in fans and coolant pumps, for example. The compact motor starters are installed in control cabinets and are designed to start single and three-phase motors of machines and systems, protecting them against overloads and short-circuits. They are each available in standard and safety variants.
- Simatic PCS 7 Plant Automation Accelerator V3.0 plant and automation engineering software closes the gap between plant engineering and the process control system
- More powerful, more open version
- Increased system openness based on GSDML and NE150 standards
- Seamless engineering through the integration of various Simatic components
Siemens has extended its engineering software for planners and automation engineers, Simatic PCS 7 Plant Automation Accelerator 3.0 (PAA), to include new functions for even more flexible and integrated automation engineering. With this latest software version, Simatic PCS 7 automation projects can be configured even more easily and efficiently. With Version 3, the PAA software closes the gap between plant engineering and the process control system. The entire plant structure including measuring point data can be generated easily and synchronized between the systems. Automation engineers are supported in all phases from tender preparation (such as bills of material), automatically generated process control data from electrical engineering in the Siemens Simatic PCS 7 process control system (including controlled mass data engineering), to as-is documentation of the process automation.
- Simatic WinCC Unified: Completely new developed visualization system based on native Web technologies
- Fully scalable in hardware and software - from machine-level applications to the distributed SCADA solution
- Open programming interfaces and option packages enable the implementation of industry-specific requirements
- Tried-and-tested engineering in the TIA Portal
At the "SPS – Smart Production Solutions" 2019, Siemens will present a completely new overall system for industrial operator control and monitoring. The web-based visualization system consists initially the Simatic WinCC Unified visualization software as well as the new generation of HMI panels, Simatic HMI Unified Comfort Panels. The new system provides the user with a solution for HMI and SCADA applications, and in the future also for Industrial Edge, Cloud and Augmented Reality scenarios.
- New development – Simatic PCS neo sets new standards in process automation
- Intuitive usability and a single workbench for all tasks
- Consistent object-oriented data management
- Unique, global, web-based collaboration in engineering and operation
- Scalable from small process modules up to the largest process plants in the world
Siemens sets new standards in process automation and is launching an innovative web-based process control system for all industries at the Hannover Messe. Simatic PCS neo is a brand-new system software, which offers companies in the process industry unique opportunities in the age of digitalization. Main features include global web-based collaboration in engineering and operation and intuitive handling representing all relevant information in a single workbench.