Siemens has received an order from the regional grid operator EWE Netz GmbH to supply the key components of a Siharbor shore power supply system in Cuxhaven. The order includes the complete transformer station as well as the cable feed system for ro-ro (roll-on/roll-off) ships. The plant owner will be the northern German Gesellschaft für Hafeninfrastruktur Niedersachsen Ports (NPorts). With a power output of 630 kilowatts (kW), the plant will supply these ships with electricity during their lay time. They will thus be able to turn off their diesel generators, significantly lowering exhaust gas and noise pollution. The berth is located next to the new factory for wind turbines operated by Siemens Gamesa, which will be the plant's main user in the future. Siemens Gamesa will ship wind turbine components to its sister factory in Hull, UK. The Siharbor system is expected to go into operation by April 2018.
- Faster processor and more memory space for complex applications
- Increased connectivity
- Efficient refrigeration control with inbuilt electronic expansion valves drivers
With the new Climatix C600 models the Siemens Building Technologies Division is extending its range of controllers for heating, ventilation and air conditioning (HVAC). These are designed for complex applications comprising up to 8,000 objects, for example a ventilation with integrated chiller unit. The new model series includes easy cloud connection for digitalized services for applications like chillers, heat pumps, district heating stations, air handling units and roof top units. Original equipment manufacturers (OEMs) are thereby enabled to develop new business fields or to increase service efficiency.
Siemens has developed new base holders for Neozed fuses in one-pole and three-pole designs and sizes D01 and D02. Made of heat-resistant plastic, the new bases replace the existing Siemens devices. Eight new variants for 16 A and 63 A rated currents were developed. The compact devices are especially safe to use and, thanks to new terminals, can be easily mounted in distribution boards. For the first time, the devices are available with LED indicators that clearly show whether the fuse has been tripped due to an overload or short circuit and must be replaced.
With the 3WL10, Siemens has developed a new air circuit breaker in the especially compact size 0 that can handle rated currents of up to 1,250 amperes (A). With this development, Siemens has closed the last gap in the portfolio and now offers circuit breakers for nearly every application, in four sizes and five performance classes from 630 to 6,300 A. The 3WL10 communication-capable circuit breakers reduce space requirements in the switchgear to a minimum. With two individual electronic trip units and various connection options, they can be installed in switchgear in accordance with IEC61439- and be integrated in energy management systems via communications modules and the internal metering function.
- Siemens to deliver 47 self-service bicycle parking facilities at Dutch railway stations
- Secure and convenient parking solution for seamless transition from bicycle to boarding at railway stations
- Contract includes system monitoring for eight years
The Siemens Building Technologies Division (BT) is working with NS Stations, the operator of railway stations in the Netherlands, to optimize bicycle parking at 47 Dutch railway stations with the user-friendly and secure self-service bicycle parking solution from Siemens. The unmanned bike parking facilities will be available for parking privately owned as well as rental bikes. In addition to modernizing and equipping the parking stations, Siemens will provide 24/7 system monitoring to ensure system availability as well as predictive maintenance for a period of eight years. The volume of the contract is 14.2 million euros. Furthermore, Siemens will continue to work with NS Stations to jointly develop future innovations in access systems for manned bicycle parking facilities using RFID technology (Radio Frequency IDdentification).
- Smart thermostat for residential heating control
- Fast commissioning with integrated navigation assistant
- App for iOS and Android with numerous functions
The Siemens Building Technologies Division will launch a new smart thermostat for residential heating control in November 2017. The RDS110 smart thermostat takes just a few minutes to commission and can be controlled via a mobile phone app.
- Siemens EnergyIP software will manage nearly five million meters by 2022
- Con Edison is the first U.S. energy providers capable of recording and processing electric meter data in near real-time
- Solution underpins the utility's strategy to transform to a new energy system, part of New York's "Reforming the Energy Vision" (REV) strategy
Con Edison Company of New York and Orange & Rockland Utilities (O&R), both regulated operating companies of Consolidated Edison, Inc., have begun their advanced metering rollout after the successful initial implementation of Siemens EnergyIP meter data management software. The software solution was implemented by Omnetric Group, the Siemens and Accenture technology services company, dedicated to the energy sector.
- New Siemens SVC PLUS Mobile (Mobile STATCOM) solution can be located anywhere in order to rapidly restore power grids
Siemens is providing Dominion Energy, a subsidiary of one of the largest producers and transporters of energy in the US, with the company's first Mobile SVC STATCOM technology. The solution keeps the grid stable during disturbances and faults by providing fast and controlled reactive power. Mobile STATCOM gives the utility an unprecedented level of flexibility to move the device anywhere grid support is needed, especially in cases of unexpected outages from extreme weather or unplanned events. Instead of several years of planning and executing a permanently installed substation project, the Siemens STATCOM technology can be moved within days.
Siemens will design and install twelve microgrids for the Brazilian utility Centrais Elétricas do Pará (CELPA). These microgrids will be built in power generation plants (distributed energy systems) in the state of Pará. A central control center in Belém will be able to monitor and control these self-contained island networks. Siemens will deliver and install the suitable automation, protection and control technology. This will improve the analysis of plant data and thus increase the availability and reliability of the plants. It will also make it possible to optimize and better plan the service and maintenance work of the service teams, so that fewer deployments on site are necessary. The two power plants furthest apart are at a distance of 890 kilometers from each other. The systems are scheduled to go into service at the beginning of 2018.
- Alarm visualization and processing in a 3D model
- Collaboration with Intel supports real-time monitoring
- Addition to Integrated Data Center Management Suite (IDCMS)
The new release of Datacenter Clarity LC* Version 3.0, the DCIM (Data Center Infrastructure Management) software from the Siemens Building Technologies Division, seamlessly integrates the Desigo CC building management platform, further improving the management of data center infrastructures. The critical alarms managed in Desigo CC can now be administered directly in Clarity LC via a web service. The system visualizes and processes critical alarms in a 3D model which shows the affected asset in real time. Once the appropriate solution for the alarm has been created in the 3D model, a workflow is set up that tasks the IT and facility management team with the physical implementation of possible changes in the data center. This optimizes the troubleshooting process across disciplines and departments.