Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release06 November 2017Building TechnologiesZug
New smart thermostat from Siemens

The picture shows the handling of the Smart Thermostat RDS110 from Siemens Building Technologies on the cell phone.
The thermostat with integrated sensors for room temperature, air quality, humidity and the presence of occupants can be combined with external sensors for outside temperatures or switches for opening windows. The touch screen displays the essential information for an easy operation. A Green Leaf symbol indicates whether the heating equipment is running at top energy efficiency. The thermostat is equipped with a presence sensor and automatically switches on the comfort level as soon as occupancy is detected. The weekly time programs for heating and domestic hot water are visible on the mobile app and can be easily adjusted. Thanks to numerous control functions via app and touchscreen, intuitive operation and sensor-based monitoring of room air quality, the smart thermostat creates perfect places based on the requirements of room users.
Thermostat control is intuitive using the mobile app or the local touchscreen. The smart thermostat is connected to a WLAN compatible router that ensures data is transferred to the Siemens cloud. Users can access this data from the app and conveniently control up to 12 thermostats from their mobile phones. The app is available in a number of languages, including German, English, French, Italian, Spanish and Chinese.
The smart thermostat has a self-learning algorithm that determines the best heating strategy for achieving the desired comfort level with maximum energy-efficiency. The thermostat selects the optimal heating start time depending on the sensor readings. Within a day, the thermostat adjusts the heating strategy to the room and the heating devices in use, thus contributing significantly to lower energy consumption and reduced energy costs.
The premium design of the 90mm black touchscreen reflects the superior technology of the RDS110 smart thermostat from Siemens. The touchscreen responds to the lighting conditions in the room and ensures optimal readability. The screen and its diverse information and control options can be fully protected against unauthorized access.
The thermostat can be installed and commissioned in very little time. Installation does not require a WLAN. An integrated navigation assistant facilitates commissioning, the entire process is complete within minutes in just a few steps.
The smart thermostat is eu.bac Class AA certified and meets eco-design Class IV for optimal energy efficiency.
For more information about the Building Technologies Division, please visit www.siemens.com/buildingtechnologies
For more information about the smart thermostat, please go to www.siemens.com/smart-thermostat.
For more information about the Building Technologies Division, please visit www.siemens.com/buildingtechnologies
For more information about the smart thermostat, please go to www.siemens.com/smart-thermostat.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.