Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release11 October 2017Energy ManagementErlangen
Microgrids from Siemens to improve distributed energy supply in Brazil

Siemens will design and install twelve microgrids for the Brazilian utility Centrais Elétricas do Pará (CELPA). These microgrids will be built in power generation plants (distributed energy systems) in the state of Pará.
The twelve plants are powered with diesel generators and are geographically distributed across the Brazilian state of Pará. With a total output of 80 megawatts they supply power to approximately 160,000 people. The plants are located in Afuá, Alenquer, Faro, Gurupá, Juruti, Monte Alegre, Muaná, Oeiras do Pará, Porto de Moz, Prainha, São Sebastião da Boa Vista and Terra Santa. The region in which the plants are located features rough and almost impassable terrain, and is mainly accessible by river. From Belém to Terra Santa takes about seven days by boat.
"We offer a complete, easy-to-operate system for simple and reliable energy management. In this way we can improve monitoring and control systems and thus increase generation rates, while reducing fuel consumption and improving the reliability of the plants. Another advantage of this system is that downtimes are reduced and the plants can be operated with the highest efficiency parameters," states Sérgio Jacobsen, CEO of Siemens Digital Grid in Brazil.
The scope of delivery from Siemens also includes the equipment for collecting and monitoring local data such as the RTUs (remote terminal units) and the communication interfaces. The protection technology components are supplied by Reyrolle. A monitoring station where all data can be viewed will be installed in each of the 12 plants. Monitoring of all plants will be carried out by a control center based on Sicam SCC. Siemens is to install and set the parameters of all components of the microgrid and will also provide service and training for the plant operators.
For further information on Division Energy Management, please see new.siemens.com/global/en/products/energy.html.
For further information on microgrids, please see www.siemens.com/microgrids and
Microgridcontroller.
For further information on microgrids, please see www.siemens.com/microgrids and
Microgridcontroller.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.