Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release21 November 2017Energy ManagementErlangen
Siemens offers new 3WL10 circuit breaker in compact size 0

The picture shows the new 3WL10 circuit breaker 3WL10.
Circuit breakers are the heart of the electrical power distribution and reliably protect electrical installations against damage or fire as a result of short circuits, ground faults, or overload faults. 3WL air circuit breakers from Siemens act as incoming-feeder, distributor, coupler, and outgoing-feeder circuit breakers in electrical systems in industry, buildings, and infrastructure applications. They switch all operational and fault currents and protect motors, capacitors, generators, transformers, busbars, and cables. Thanks to this expansion of the 3WL portfolio, Siemens now covers the power range from 630 A to 6,300 A in four different sizes. The entire portfolio can be used worldwide up to 70°C (without derating up to 55°C) and complies with IEC-60947-2 and DIN VDE 0690 part 1. Furthermore, all circuit breakers with functions for communication and energy data acquisition can be configured via Profibus or Modbus.
For further information on 3WL, please see www.siemens.com/3WL
For further information on Siemens at the SPS IPC Drives 2017, please see
www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2017
For further information on 3WL, please see www.siemens.com/3WL
For further information on Siemens at the SPS IPC Drives 2017, please see
www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2017
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world’s largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 372,000 employees worldwide. Further information is available on the Internet at www.siemens.com.