- SICAM 8 delivers a universal automation platform for all applications in the field of power supply
- Incorporates SICAM HMI, elevating process visualization to the next level
- Includes the SICAM S8000 software solution for power automation
- SICAM 8 platform forms part of the Siemens Xcelerator portfolio
Siemens Smart
Infrastructure has launched the highly scalable SICAM 8 power automation
platform. Designed with scalability and security at its core, the platform helps
customers achieve resilient and secure grid operation, while allowing for the
incorporation of additional applications in the future. It also includes two
new software solutions: the SICAM HMI (Human Machine Interface) visualization
tool and the SICAM S8000 software solution for power automation, and forms part
of the Siemens Xcelerator portfolio, an open digital platform that enables
customers to accelerate their digital transformation easier, faster, and at
scale.
Whether for workpiece handling, retooling, postprocessing or parallel
machining, robots and machine tools are working ever more closely together.
Companies in almost all industrial sectors already benefit from robots today.
But integrating robots into automation and exploiting their full potential poses
many challenges. Under the motto "Seamless and fast integration of robot
kinematics into automation", Siemens will be presenting at this year's
automatica (Hall B6, Booth 302) how companies can overcome these
challenges and how the digital and real worlds can be connected through
robotics and automation solutions.
- Prototype Megawatt Charging System [MCS] from Siemens successfully delivered a 1MW charge
- The new technology highlights the potential for megawatt charging to redefine long haul trucking
- The Siemens SICHARGE Megawatt Charging System used is based on its SICHARGE portfolio with a customized MCS dispenser
Siemens Smart Infrastructure has completed the first successful 1MW charge, in a pilot which brought together a prototype MCS charging station from Siemens and a long-haul prototype eTruck from a well-established OEM.
- Bustanica, the Dubai-based vertical farming company, requires 95% less water than a conventional plot, and yields more than 1 million kg of produce free of pesticides, herbicides and chemicals
- Siemens provided building systems and automation hardware and software from its Digital Industries and Smart Infrastructure portfolios
- Building systems, automation software and hardware are part of Siemens Xcelerator
Siemens provided automation and building technology
to the recently opened Bustanica vertical farm in Dubai, the world’s largest of
its kind. The $40 million facility is owned by Emirates Crop One, a joint venture
between Emirates Flight Catering, one of the world’s largest catering
operations serving more than 100 airlines, and Crop One Holdings Inc., an
industry leader in technology-driven indoor vertical farming.
- Y-turning and Advanced Rapid Movement for even more machine tool productivity
- Reduced Dynamic Mode reduces wear and increases availability
- End-to-end keyboard and machine control panel portfolio from 15 to 24 inches
Siemens is expanding its
offering around the Sinumerik One "digital native" CNC. The new CNC
generation from Siemens, which was introduced to the market in 2019, is also
coming up with innovations in software and hardware this year. With the new
Sinumerik V6.20 software, there are new technology functions for the Sinumerik
One that simplify operation, reduce machine wear, and increase productivity.
Siemens is thus demonstrating once again how the powerful Sinumerik One machine
tool control system can be optimally used for digital transformation in a
highly productive, flexible, and modular way.
- Performance optimized, easy to use and future-proof servo drive system
- Flexible and compact – scalable depending on the application
- Easy engineering thanks to integration in TIA, integrated web server and one-button tuning function
With Sinamics S200, Siemens is launching a new servo drive system designed
for a variety of standard applications in the battery, electronics as well as other
industries. It consists of a precise servo drive, powerful servo motors and
easy-to-use cables and offers high dynamic performance. Applications that
require precision in speed and torque, such as winding and unwinding machines in
battery manufacturing and cell assembly, particularly benefit from the new
servo drive system. For this purpose, Sinamics S200 offers optimized speed
ripple, cogging torque compensation, 17/21-bit ST and 21-bit MT encoders, and
cycle-synchronous communication for optimized performance by
Profinet IRT in minimum 250us.
- Desigo PXC7 building automation controller enables tailor-made and scalable solutions for larger buildings
- Speeds up and simplifies engineering and commissioning process
- Higher resilience and availability thanks to BACnet Secure Connect communication
After the
launch of the PXC4 and PXC5 controllers for the optimized control of small and
medium-sized buildings, Siemens has added the PXC7 to its Desigo portfolio to
offer even more flexibility to building automation practitioners. This new
addition allows professionals to program heating, ventilation and air
conditioning (HVAC) applications for larger buildings. Thanks to its simplified
integration capabilities, the Desigo PXC7 controller supports
system integrators in providing
a complete automation solution.
- New V6 software generation with new functions like a single positioner to reduce the load of the controller, and EtherNet/IP to allow third-party controllers to be connected
- Simulation via DriveSim Advanced enables virtual commissioning in advance, ensuring drive process requirements are met efficiently and cost-effectively
- New hardware architecture with functional enhancements like a second encoder interface and 3C3 (H2S and SO2) coating increases precision and robustness
Siemens is innovating the well-established Sinamics S210 servo drive system with a new hardware architecture and new V6 software generation that expand the system's range of applications. The servo drive system is especially suitable for applications with high dynamics in the power range between 50 W and 7 kW: for example, machines for packaging, pick & place applications, and digital printing.
- Siemens presents a new CNC for woodworking machines at the Ligna
- Sinumerik MC is the open CNC for customized processing machines
At the Ligna Woodworking Trade Fair 2019, Siemens is showcasing the Sinumerik MC control as a universal, open CNC system. Its optimized motion control, high-performance automation and the integrated Windows 10 operating system make it the ideal control, especially for wood, glass and stone cutting machines. With its open operating concept, the control system is also suitable for additive manufacturing, adhesive application, plate cutting, straightforward grinding, and laser or water jet cutting.
- New NCU 1740 for higher scalability of Sinumerik One
- Sinumerik Run MyRobot /Direct Control V2.0 and Run MyRobot /Direct Handling V2.0 available for Sinumerik One
- New functions for the Digital Twin in Create MyVirtual Machine and Run MyVirtual Machine
Siemens is expanding its offering for the "Digital Native" CNC Sinumerik One. Two years after its market launch, the technology company is presenting numerous innovations in hardware and software for the Sinumerik One at EMO Milano and the virtual Siemens Machine Tool Days. In this context, Siemens is demonstrating how the powerful machine tool controller can be used in a highly productive, flexible, and modular way and in the best possible way for digital transformation. In terms of hardware, the new NCU 1740 complements the existing NCU 1750 and 1760 as well as the PPU 1740, thus expanding its use in modular machines.