Siemens is rigorously executing its announced €2 billion investment strategy. Of this amount, the company plans to invest around €1 billion in Germany, thereby boosting the country’s innovative strength.
Siemens turns ski lifts into high-tech systems
- Siemens and UL Solutions demonstrate a transformative shift from relying
solely on physical tests to reliable integrating digital simulations.
- Reduced costs, accelerated time-to-market and seamless integration of
digital modeling tools will redefine the future of verification.
- Siemens’ digital twin technology breaks through traditional testing
boundaries, serving as a testament to the industrial metaverse’s potential
for reshaping product development possibilities.
For the first time ever, an industrial product has been certified for the United States
after parts of the required tests were conducted through digital simulation. That
simulation was verified and validated with physical testing. This remarkable
achievement is a global first in a national safety-certification process. To make this
advance possible, Siemens collaborated with UL Solutions, an esteemed global
leader in applied safety science. The result is a testimony to the remarkable
accuracy and reliability of modern digital twin simulations. It marks a step forward
into a future in which digital twins and the industrial metaverse streamlines product
development, enhances innovation, safety and accelerates time-to-market.
- Attica-Crete interconnection will ensure a more secure power supply and increase integration of renewable energy
- HVDC project will reduce half a million tons of CO2 emissions in first year of operation
- Total order volume for Siemens-led consortium €370 million
A consortium led by Siemens Gas and Power (Siemens Energy) has been awarded a turnkey contract for two converter stations for the Greek high-voltage direct-current (HVDC) link that will connect Crete, Greece’s largest and most populous island, with the mainland of Greece. The project will enable an exchange of electricity of up to 1,000 megawatts (MW) to enhance reliability of the power supply and facilitate integration of renewable energy sources in the power grid. Customer is Ariadne Interconnection S.P.S.A., a wholly owned entity of the Greek independent power transmission operator IPTO. Commissioning of the interconnector is scheduled for mid-2023. Total order volume for the consortium is €370 million.
- Low-loss transmission of wind
energy for 1.1 million households
- Further contribution toward
decarbonizing energy supplies
Siemens Energy is supplying the
high-voltage direct-current (HVDC) power transmission technology for a further
offshore connection in the German North Sea. A corresponding contract was just
signed by the German-Dutch network operator TenneT and the BorWin5 Offshore
Consortium, consisting of Siemens Energy and Dragados Offshore. In 2025, the
platform BorWin epsilon, which is part of the BorWin5 project, will begin the
low-loss transmission of electricity produced by the EnBW He Dreiht wind farm
off the island of Borkum to the Garrel/Ost converter station around 230
kilometers distant. The transmission capacity of 900 megawatts is calculated to
serve over 1.1 million households with electricity. The project is a further
contribution toward decarbonizing Germany’s energy supply. BorWin5 marks the
seventh HVDC offshore grid connection project undertaken by Siemens Energy in
Germany with TenneT.
- Siemens will upgrade control and protection system of Moyle Interconnector
- Refurbishment increases security of supply, improves integration of renewable energy and enhances provision of ancillary services
Siemens Gas and Power (Siemens Energy) has been awarded the project to refurbish the Moyle Interconnector, a high-voltage direct-current (HVDC) link between Ballycronan More in County Antrim, Northern Ireland, and Auchencrosh, Scotland. Owned and operated by Mutual Energy, the Moyle Interconnector control and protection system is almost 20 years old and is being modernized to enhance its operation. The refurbishment of the 500-megawatt interconnector will increase the security and reliability of the power supply to consumers in the United Kingdom. The project to upgrade the technology originally installed by Siemens in 2001 is now underway and the refurbishment is scheduled to be completed in September 2022.
- Dynamic load flow control solution for grid stabilization and resilience
- UPFC PLUS controls load flow in milliseconds
- Facilitating the increasing integration of renewable energy
With its new Unified Power Flow Controller, called UPFC PLUS, Siemens Energy is expanding the options for grid stabilization. The UPFC PLUS will help system operators stabilize the grid by dynamically controlling the load flow in alternating-current grids. Easy to integrate into existing infrastructure, the UPFC PLUS improves the efficiency of today’s power grid while providing the grid stability and resilience required in the ever-changing energy landscape.
The digital transformation of the producing industry is gaining momentum. Companies from a wide variety of industries are already unlocking this potential – they are using end-to-end digitalization to create a lasting competitive edge by reducing time to market and increasing flexibility, efficiency, and quality. With Siemens Digital Enterprise solutions the technical prerequisites for the implementation of Industrie 4.0 are available and can be deployed in every application and companies of all sizes. At the SPS IPC Drives in Nuremberg, Germany, from November 27 to 29, 2018 – which took place this year under the motto "Digital Enterprise – Implement now" – Siemens showed in hall 11 how this can be done.