With the 3WL10, Siemens has developed a new air circuit breaker in the especially compact size 0 that can handle rated currents of up to 1,250 amperes (A). With this development, Siemens has closed the last gap in the portfolio and now offers circuit breakers for nearly every application, in four sizes and five performance classes from 630 to 6,300 A. The 3WL10 communication-capable circuit breakers reduce space requirements in the switchgear to a minimum. With two individual electronic trip units and various connection options, they can be installed in switchgear in accordance with IEC61439- and be integrated in energy management systems via communications modules and the internal metering function.
- A total of 219 light rail vehicles built at Siemens Sacramento manufacturing hub
- Largest order for light rail vehicles ever received by Siemens in the United States
The first Siemens-built light rail vehicle for San Francisco, U.S., entered revenue service. The new light rail vehicles will be built at the Siemens plant in Sacramento, California. In total, the company will deliver 219 light rail vehicles for San Francisco's Municipal Transportation Agency (SFMTA), Siemens' largest order for light rail cars placed in the U.S.
- Siemens to deliver 47 self-service bicycle parking facilities at Dutch railway stations
- Secure and convenient parking solution for seamless transition from bicycle to boarding at railway stations
- Contract includes system monitoring for eight years
The Siemens Building Technologies Division (BT) is working with NS Stations, the operator of railway stations in the Netherlands, to optimize bicycle parking at 47 Dutch railway stations with the user-friendly and secure self-service bicycle parking solution from Siemens. The unmanned bike parking facilities will be available for parking privately owned as well as rental bikes. In addition to modernizing and equipping the parking stations, Siemens will provide 24/7 system monitoring to ensure system availability as well as predictive maintenance for a period of eight years. The volume of the contract is 14.2 million euros. Furthermore, Siemens will continue to work with NS Stations to jointly develop future innovations in access systems for manned bicycle parking facilities using RFID technology (Radio Frequency IDdentification).
- Multifunctional platform as a new type of device for Simatic Advanced Controllers – combines conventional control tasks with typical PC tasks
- Reusable high-level language applications are easily created with Eclipse or, model-based, with Matlab Simulink
- With just one item of hardware for less programming effort and a smaller space requirement
- The Advanced Controller portfolio has two new technology CPUs and handling functions for Motion Control tasks
Siemens has expanded its Simatic S7-1500 Advanced Controller portfolio for more challenging applications to include a new type of multifunctional platform that combines control and PC functions in a single device. Two new technology CPUs also widen the portfolio for midrange Motion Control tasks.
- Logo! Web Editor for the Logo! 8 logic module: Define and design individual web pages for smartphone, tablet and PC easily
- Simplest operation and user-friendliness without requiring knowledge of HTML
- Free download – with a library of operating and display elements for a quick start
- Load your own background photo to complement visual sensor data or switching elements, and then control the logic module from a smartphone, tablet or PC
Siemens is complementing its Logo! 8 logic module series with the Logo! Web Editor. With the free web editor for the new Logo! 8 version, which will become available in December, makes it very easy for users to define and design their own web pages for smartphone, tablet and PC. Thus they can visualize and control their Logo! 8 switching and automation solution for building installations, control cabinet, machine or apparatus construction individually and easily via the web. For example, users now use a real photo of their individual automation object as background photo, which could be a photo of a building, and complement it with self-defined visual sensor data or switching elements. They then use a smartphone, tablet or PC to switch their heating or alarm system, or to monitor and regulate the temperature of their swimming pool. Particular importance was placed on making the web editor as easy as possible to use and so user-friendly that no additional knowledge, such as HTML, is required. For a quick start, simple operating and display elements are already included in the library supplied. Additional elements can be easily created and added to the library.
- Firmware 4.8 enables Sinamics S120 converters to operate with synchronous reluctance motors
- System operation with or without position sensor using new Sinamics reluctance control license
- Durable in any operating environment due to field-oriented vector control
- High energy efficiency even at low speeds
Firmware version 4.8 allows Simotics synchronous reluctance motors to also be operated with Sinamics S120 converters, enabling them to benefit from the complex functionalities of the modular S120 product portfolio. The new Sinamics reluctance control license used in combination with the Sinamics Booksize Modules means that precise drive control down to a complete standstill is now possible with and without a position sensor. This applies both for motor and generator operation. Field-oriented vector control across the whole of the operating range makes for a tangibly more robust drive system. Unlike U/f-based methods, for instance, any possibility of motor stalling in the event of load jumps is excluded. Sensorless control also enhances the energy efficiency of the drive, as even in the low speed range it allows the achievement of low values normally only possible using a sensor.
- Structural changes in markets for Power and Gas Division and Process Industries and Drives Division make consolidation of global setup necessary
- Reduction of about 6,900 jobs worldwide, half of them in Germany
- Increased investments in future growth markets offer opportunities
Siemens is responding to the rapidly accelerating structural changes in the fossil power generation market and the commodity sector. A consolidation plan for the Power and Gas Division (PG), the Power Generation Services Division (PS) and the Process Industries and Drives Division (PD) aims to increase capacity utilization at production facilities, drive efficiency and enhance expertise by bundling resources.
- Higher performance and new application areas for Siplus HCS4200 Heating Control System with two new power output modules
- Versatile control of electrical heating elements in 45, 75, 110, 230/277 and 400/480 V power grid
- Current measurement integrated in output for diagnosis of heating elements connected in parallel
- Simple, easy engineering and commissioning of industrial heating processes with TIA Portal and Proneta
Siemens has equipped the flexible, modular Siplus HCS4200 Heating Control System for switching and controlling heat emitter arrays and heating elements with two new power output modules (POM). Each output is now even more powerful and it is possible to control voltages from 45 V, making this versatile heating control system even more flexible, and suitable for use in safety extra-low voltage applications, for example.
- "Realize the value of the Digital Enterprise Suite – Industrialize Additive Manufacturing" as this year's booth slogan
- Seamless integrated software and automation solutions for additive manufacturing aimed at machine builders and users
- Innovative value-add services to further speed up the industrialization of additive manufacturing
- Engineering and printing services through to complete additive manufacturing of parts by Material Solutions and Mobility Services
At this year's formnext, the leading trade fair for additive manufacturing (AM), Siemens will be showcasing its seamless integrated solutions for additive manufacturing with the Digital Enterprise Suite. At its booth stretching over an area of around 150 square meters, the company will be demonstrating its portfolio along the entire AM value chain at the show from 14 to 17 November under the banner "Realize the Value of the Digital Enterprise Suite – Industrialize Additive Manufacturing". Products featured at the show cover everything from design and engineering software, simulation tools and matching hardware for complete machine and factory automation through to machine networking with the cloud-based IoT operating system MindSphere. Designed to address the requirements of both machine builders and additive manufacturing users, this unique offering from Siemens aims to demonstrate how companies working in the field of additive manufacturing can use digitalization to significantly boost the flexibility and efficiency of their production, reduce both engineering time and time to market, and so consolidate and expand their competitive standing in the global marketplace.
- Simatic MV540 is the first of a new generation of optical read devices
- Higher computing output speeds up the read process
- Read reliability improved through in-depth evaluation of image information
- Versatile process connection to automation technology and MindSphere
Siemens is expanding its portfolio of optical read devices to include the Simatic MV500 series with significantly improved functionality and a modern design. The first device of the new series is the optical reader Simatic MV540. Despite versatile innovations, it offers compatibility with the predecessor model Simatic MV440 both mechanically and in terms of programming and interfaces. Key to the new, improved performance of the Simatic MV540 is its higher computing power, which significantly accelerates the read process to up to 100 reads per second. In addition, in-depth evaluation of the image information enables improved read reliability under even the most adverse conditions. High-performance accessories such as lenses with electronic focus enable a change of focus within just 200 milliseconds.