Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release20 November 2017Digital Factory Nuremberg
Multifunctional controller platform for automation

The picture shows the Simatic S7-1500 Advanced Controller with the CPU 1518(F)-4 PN/DP MFP multifunctional platform.
The CPU 1518(F)-4 PN/DP MFP multifunctional platform is a new type of device for Advanced Controllers that enables high-level language functions to be integrated and stand-alone applications to be easily created and reused. The multifunctional platform combines a typical controller with tasks that had previously been outsourced to a PC – such as model-based and high-level language programming and solutions with databases. Existing technological C/C++ algorithms can continue to be used, and the data exchange between PC and controller, which previously had to be programmed, has been simplified. Furthermore, the configuration has been standardized and the space requirement reduced, while at the same time the overall solution has been made more resilient on one item of hardware with a stable Simatic embedded operating system. The user programs controller-independent C/C++ applications, such as protocol converters and database applications, with standard commercial programming tools, such as Eclipse. These now run as stand-alone C/C++ applications in parallel to the control program on the multifunctional platform. The additional PC hardware previously required has been eliminated. Users can now also use model-based development tools, such as Matlab Simulink, and transfer their complex functions into the new Simatic Advanced Controller CPU 1518(F)-4 PN/DP MFP. The new multifunctional platform can be used with TIA Portal V15 or higher.
The new technology CPU 1516T-3 PN/DP and fail-safe technology CPU 1516TF-3 PN/DP combine standard, safety, and Motion Control functionalities, such as gearing and camming, in one device. The new CPUs complement the already available range of Advanced Controllers. Midrange Motion Control tasks can be easily implemented in conjunction with the Sinamics V90 PN and S210 servo drive systems. The Motion Control functionalities of all Simatic S7-1500 technology CPUs have also been extended to include the control of 2D to 4D kinematics. This now makes additional handling applications possible, such as Pick & Place, Cartesian Portal, Delta-Picker and Scara robots.
Background information:
Siemens offers the right controller for an extremely wide range of automation requirements. The scalable Simatic range of controllers, comprising Basic, Advanced, Distributed and Software Controllers, all have the same range of functions. The S7-1200 Basic Controllers are used for compact automation solutions, and the S7-1500 Advanced Controllers for complex tasks, while the ET 200SP Distributed Controllers are suitable for distributed applications, and the Software Controllers for PC-based applications.
For further information, refer to www.siemens.com/s7-1500
Further information about Siemens at the SPS IPC Drives 2017 at www.siemens.com/sps-ipc-drives and www.siemens.com/press/sps2017
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 372,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Contact
Gerhard Stauss
Siemens AG
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (911) 895-7945