- Plug & play solution comprising Simatic ET 200SP TM ECC PL ST and TM ECC CCS calibration kit for convenient charge controller calibration
- Reduced engineering effort and simplified commissioning of DC fast charging systems for electric vehicles
- Stable charging process and up to 50 percent less servicing required to remedy charging interruptions
Siemens offers charging system suppliers a new plug & play solution, which for the first time enables calibration of the Powerline signal level in line with CCS (Combined Charging System) CharIN Association Implementation Guidelines for the conductive charging of electric vehicles. The solution comprises the Simatic ET 200SP TM ECC PL ST charge controller and the TM ECC CCS calibration kit. When calibrating the signal quality of a DC CCS charge controller using the Siemens solution, there is no need for a spectrum analyzer, which makes the process quicker and easier. Manufacturers of charging stations can also save engineering effort as well as time and costs during commissioning and can reduce servicing to remedy charging interruptions by up to 50 percent. Engineering is in the TIA (Totally Integrated Automation) Portal.
- Charging infrastructure to power 24 new electric buses for the Ostrava Transit Authority in Czech Republic
- Software to automatically adapt the charging processes to the bus schedules and to optimize energy consumption
- Operations are scheduled to start in mid-2022
Siemens Smart Infrastructure will provide a charging solution for Dopravní podnik Ostrava (Ostrava Transit Authority), which will expand its fleet with 24 Solaris electric buses. The largest order for electric buses in the Czech Republic to date will include four Sicharge UC charging stations from Siemens. These high-power chargers provide an effective maximum of 400 kW each. Furthermore, Siemens will deliver 28 mobile chargers, electrical infrastructure as well as energy automation software.
Media representatives got a first-hand impression of the new Vienna Metro during a test drive on the 14th April 2021 – in the presence of Public Transport City Councillor Peter Hanke, Wiener-Linien Managing Director Günter Steinbauer and Siemens Mobility CEO Arnulf Wolfram. After the successful approval of operation, the so-called 'X-Wagen' will be in use for all Viennese on the four lines U1 to U4 from 2022. With the completion of the new U5 in 2026, the new vehicles will also be running fully automatically.
S-Bahn Berlin GmbH has signed a framework contract with the consortium of Stadler Pankow GmbH and Siemens for the delivery of up to 1,380 vehicles. A firm order was placed for the first 106 trains. The 85 four-section and 21 two-section trains have a high triple-digit million-euro order volume. S-Bahn Berlin, a subsidiary of Deutsche Bahn, plans to use the new trains on the Ringbahn lines (S 41 and S 42) as well as on the system's southeastern feeder lines S 47, S 46 and S 8. These lines comprise roughly one-third of the entire S-Bahn network in Berlin. The first ten vehicles will be ready to enter service as of 2020. Subsequently, all remaining vehicles will be delivered continuously to the Berlin system up to 2023. The vehicles will be manufactured and assembled at the Berlin plant operated by Stadler Pankow GmbH.
Shifting freight transport to rail has its limitations. Therefore, a share of this transport will need to be carried out by trucks that combine reliable service with minimum environmental impact. The eHighway system is twice as efficient as conventional internal combustion engines. This Siemens Mobility innovation supplies trucks with power from an overhead contact line. This reduces local air pollution and contributes significantly to the decarbonization of the transport sector.
- Reliable protection with minimal space requirements
- For power distribution and industrial plants
Siemens Smart Infrastructure presents the new Siprotec 5 Compact device, specially designed to address the demands of industrial applications, infrastructure and distribution grids. With its compact size, large number of inputs and outputs, and universal range of functions, it can be configured to meet the specific requirements associated with protecting feeders and motors. As a space-saving universal device, it is ideally suited to help optimize investment and operating costs in power distribution.
- „Infinite opportunities from infinite data“ is this year's trade fair motto
- Leveraging the full potential of data from merging the virtual and physical worlds
- "Digitalization knows no end"
- Expansion of the portfolio for edge computing in industry
Under the motto "Infinite opportunities from infinite data", Siemens is demonstrating at the "Digital Enterprise Virtual Experience" at Hannover Messe 2021 how the merging of the physical and virtual worlds enables industrial enterprises to act flexibly and sustainably, as they are facing huge challenges: The Covid 19 pandemic has changed markets and requirements almost overnight. Added to this are the growing individualization and the urgent need for more sustainability. This can only be mastered with the help of digitalization and automation. Siemens brings together the data generated in this process in a continuous cycle between the virtual and physical worlds. This enables companies to better understand and use data. Traditional silos between previously separate industrial domains are breaking down and new opportunities for sustainable and flexible production are being created. This enables employees in industrial enterprises to make appropriate decisions based on data or, for example, to react a lot faster to changes such as suddenly increased resource consumption.
- High transparency through integrated communication and measurement functionality
- Faster response to faults minimizes downtime
- Easy retrofitting of existing systems without additional space requirements
Siemens Smart Infrastructure has launched the new Sentron 3NA COM LV HRC fuse link with integrated communication and measurement functionality. The compact device is designed for 400 volts low-voltage grids and can be used in secondary substations and industrial plants. The LV HRC fuse link protects grids and plants against short circuits and overloads and is capable of measuring current. The collected data is sent wirelessly to the new 7KN Powercenter 1000 data transceiver where it can be retrieved. In addition, it can be transferred to local or cloud-based grid and energy management systems. Among other things, the data provides insight about the current network load, phase symmetry and any irregularities. This makes it possible to increase the supply security and optimize maintenance and service. Thanks to faster fault detection and location, the duration of power outages can be significantly reduced.
In line with the motto "Infinite opportunities from infinite
data", Siemens will be demonstrating at the Digital Enterprise Virtual
Experience how industrial companies can master the rapidly changing challenges
of our time with the help of digitization, automation and intelligent use of
the resulting data. With the Hannover Messe 2021 Digital Edition, the leading
trade fair for the manufacturing industry, energy sector and logistics will
take place completely virtually from April 12 to 16. Siemens is participating
with its own virtual presentation at the trade fair. In an almost real 3D
environment, participants can virtually experience products, solutions and
concrete application examples.
Register here:
www.siemens.com/VE-Registration
- Monitoring of machine conditions with IIoT sensors, gateway and app
- Multisensor transmits vibration and temperature data via Bluetooth to an industry gateway and on to the cloud
- System detects potential incidents through machine learning
Siemens is presenting Sitrans SCM IQ, a new Industrial Internet of Things (IIoT) solution for Smart Condition Monitoring, at the Hannover Messe 2021. It enables potential incidents to be detected and prevented at an early stage, thus reducing maintenance costs and downtimes, and increasing plant performance by up to ten percent. The wireless, robust Sitrans MS200 multisensors form the hardware basis for installation on machinery such as pumps, gear units, compressors, and drive trains, where they collect vibration and temperature data. Via a Bluetooth connection, this data is sent to the Sitrans CC220 industry gateway where it is encrypted before being transmitted from there to the cloud, in this case the MindSphere industrial IoT-as-a-Service solution. The anomaly detection of the Sitrans SCM IQ system is based on machine learning. It constantly monitors and analyzes all sensor values and detects deviations from the normal operating state in advance. Anomaly notifications are sent via SMS and/or email, depending on the configuration and defined user group. The app can be used to document the anomalies of machinery behavior and makes them available to a specific circle of users. The Sitrans SCM IQ system comprises multisensors, gateway and app, and can be used in all industrial plants with mechanical or rotating components. It is scheduled to be available from summer 2021.