- Siemens Mobility provided rolling stock, rail infrastructure, system integration, and will take care of service and maintenance
- Delivered and installed 35 new three-car trains, 19 new stations, and 28 km of additional track
- Extension provides greater capacity and enhanced passenger experience
Mass Rapid Transit Authority of Thailand (MRTA), Bangkok Expressway and Metro Public Company Limited (BEM) and CH. Karnchang Public Company Limited have officially implemented full passenger revenue service for the Blue Line Extension. In support of this project, Siemens Mobility integrated turnkey services delivered 35 three-car metro trains, installed the signaling, built the traction power supply, developed a passenger information system, implemented a SCADA system, provided depot workshop equipment, and instituted system integration by incorporating the telecommunications and platform screen door systems provided by ST Electronics Thailand into the project. In addition to delivering the overall project management, going forward, Siemens Mobility will also provide maintenance for 10 years. The fully completed Blue Line Extension adds 28-kilometers of track, 19 new stations, and an additional 35 three-car trains. The completed extension will now allow the Blue Line to carry approximately 500,000 passengers per day and seamlessly connects the Thonburi side of the Chao Phraya river to the rest of the city which suffers from traffic congestion.
- Two SGT-400 gas turbine compression packages sold for U.S. pipeline service
Siemens Gas and Power was awarded a contract to supply two SGT-400 gas turbine compression packages for Midcoast Energy, LLC’s CJ Express pipeline expansion project in east Texas. WHC Energy Services, supported by Universal Pegasus International, will be the engineering, procurement and contracting (EPC) provider for the pipeline expansion project.
- Latest generation S700 low-floor light rail vehicles
- Manufactured in the Siemens Mobility Sacramento plant
Siemens Mobility has been awarded a contract from the U.S. operator Sacramento Regional Transit (SacRT) for 20 new light rail vehicles (LRVs). This is the first new order from Sacramento since the late 1980s, when SacRT ordered 36 U2A vehicles from Siemens Mobility. The contract, including the 20 trains, spare parts and tools is approximately US$100 million.
- Cooperation agreement on using “green hydrogen” and promoting sector coupling
- Joint projects for the conversion of power plants
- Share of “green gas” to be gradually increased
Today,
Uniper and Siemens Gas and Power signed a cooperation agreement for the
development of projects on the decarbonization of power generation and
promoting sector coupling. It extends the long-standing partnership between the
two companies. It is important to look at the energy, mobility and industry
sectors together, because they all can and must contribute to reducing
greenhouse gases. One focus of the planned cooperation is the production and
use of “green hydrogen” – in other words, hydrogen from renewable energy
sources. The companies intend to implement projects in this field together,
addressing the entire value chain.
- 20 Mireo Plus B battery-powered trains for Baden-Württemberg
-
Maintenance contract for 29.5 years
- Delivery of trains by June 2023
Landesanstalt Schienenfahrzeuge Baden-Württemberg (SFBW) has ordered 20 Mireo Plus B trains from Siemens Mobility. The two-car electric trainsets with 120 seats can operate on rail routes with or without overhead power lines thanks to their battery hybrid drive, and are scheduled to operate in Network 8 of the Ortenau regional system. The contract also includes maintenance of the trains by Siemens Mobility for a period of just under 30 years. State Minister for Transport Winfried Hermann said: “This marks the first time battery-powered trains will be used in the state. With this innovative technology, the electrification of rail routes without continuous overhead power lines will also be possible.”
- Five industrial gas turbines for peak load and backup power plant
- Strengthening the power grid
For the third time in three months, Siemens has received an order from Belarus to supply SGT-800 industrial gas turbines. The new order covers five gas turbines, including associated auxiliary and electrical systems, for a peak load and backup power plant. The new plant will be built at the existing power plant location of the Berezovskaya combined heat and power plant in Beloozersk, Brest Region, in the south-western part of the country. The order was placed by Brest Republican Unitary Enterprise of Electricity Industry (Brestenergo). With an electrical capacity of 254 megawatts, the new plant will help further strengthen the power grid’s reliability and stability. Commissioning is scheduled for December 2021.
Siemens was awarded a contract to supply three boil-off compressor (BOG) packages for Venture Global’s Calcasieu Pass LNG Project. The new LNG export facility, Calcasieu Pass, is currently under construction in southwestern Louisiana’s Cameron Parish, approximately 50 miles south of Lake Charles. Once fully commissioned, the facility is expected to produce 10 MTPA of clean liquefied natural gas that will be exported to global markets.
- First-of-its-kind drilling rig project will implement customized BlueDrive™ system to replace obsolete system
- New system will use existing footprint, cabling and communication points for greater safety and quick commissioning
Siemens was awarded a contract by Arabian Drilling Company to modernize a complete and integrated drilling-drives lineup, including auxiliaries and controls, that will be installed on an offshore jackup drilling rig for a customer in the Middle East. In addition to new features and benefits, the upgrade will also enable the customer to meet the latest safety standards. Delivery of the new system is planned for the early part of 2021.
- Supply of six SGT-800 industrial gas turbines
- Increases grid reliability and flexibility
- Supports the transition to a new energy mix in Belarus
Siemens has received another order from Belarus to supply equipment for a peak load power plant. The order was placed by the state-run energy provider RUE Minskenergo. The six SGT-800 industrial gas turbines, like the five machines of the same type that Siemens is supplying for the Vitebsk region, will increase the grid’s reliability and flexibility and support the transition to a new energy mix in Belarus. Commissioning is scheduled for December 2021.