The foundation stone of the future converter station was laid on the morning of February 23rd in Folkestone by Jesse Norman, Minister for Industry and Energy signalling the start of the construction work for high-voltage direct-current (HVDC) project ElecLink. Siemens has been awarded an order to supply a link between the French and British power grids by customer ElecLink Limited, a wholly owned subsidiary of Groupe Eurotunnel SE. The ElecLink high-voltage direct-current (HVDC) link will enhance power supply reliability in both countries and promote the integration of renewable energy sources into the power grid. ElecLink, when complete, will supply enough electricity to power more than 1.65 million typical households per year. The HVDC link between France and Great Britain has been designated as one of the European Commission's projects of common interest to help create an integrated European Union energy market.
The wind service operation vessel (SOV) for the Dutch Gemini project has been christened "Windea la cour" today in Hamburg. The vessel is to set sail to start operations at the Gemini offshore wind power plant this summer. This is the third Siemens-chartered SOV which is supporting Siemens and its offshore service operations. Since June 2015, 'Esvagt Faraday' is supporting service operations at the Butendiek offshore wind power plant in North Sea and 'Esvagt Froude' is utilized for service at the EnBW Baltic II wind farm in the Baltic Sea. A fourth SOV will be utilized for service operations by Siemens at the Sandbank and Dan Tysk wind projects. SOVs are part of innovative approaches in the sector of service for offshore wind power of Siemens anc can make a vital contribution in the future to further reducing the costs for electricity generated by offshore wind farms.
The "Fortuna" combined cycle gas turbine (CCGT) power plant at the Lausward location in the port of Düsseldorf was successfully handed over to the customer and operator, the Stadtwerke Düsseldorf public utility company, on January 22, 2016. The power plant has broken three world records: in the acceptance test a maximum electrical net output of 603.8 megawatts (MW) was achieved and the net energy conversion efficiency was around 61.5 percent. In addition, "Fortuna" can also deliver up to around 300 MW for the district heating system of the city of Düsseldorf – a further international peak value for a power plant equipped with only one gas and steam turbine. This increases the overall efficiency of natural gas as a fuel to 85 percent. The heart of the "Fortuna" CCGT power plant is the extremely powerful SGT5-8000H gas turbine from Siemens. Highly efficient and flexible CCGT power plants ideally complement renewable energy sources such as the wind and the sun, which are subject to fluctuations in their power outputs.
The Dresser-Rand business, part of Siemens Power and Gas, has commissioned its first micro-scale natural gas liquefaction system at the Ten Man liquefied natural gas (LNG) facility in Pennsylvania, U.S. The modular, portable LNGo technology enables distributed production of LNG and can be installed in a short period of time to meet local demand for LNG. This cost-effective solution, developed by the Dresser-Rand business, allows the operator, Frontier Natural Resources, to monetize stranded gas assets at Tenaska Resources LLC's Mainesburg field, located in the Marcellus shale play. Frontier Natural Resources is an independent natural gas producer focused on developing conventional and unconventional resources.
The scope of supply included a standardized LNGo solution consisting of four different modules, each handling one step of the liquefaction process. The whole LNGo system can be transported on eight trucks. It is deployed directly at the gas field and has a footprint of approximately 508 square meters, roughly the size of a basketball court. The Ten Man facility commenced production just four months from contract signing, and has produced approximately half a million liters of LNG in the first 20 days.
"This project demonstrates our unique capabilities to deliver innovative solutions for oil and gas applications that help our clients maximize the value of their assets," said Michael Walhof, sales director Distributed LNG Solutions for the Dresser-Rand business. "We are proud to provide Frontier Natural Resources with a reliable, robust solution to liquefy natural gas and cost-effectively move it to market."
The LNGo technology makes it possible to monetize stranded gas deposits due to its relatively low capital and operating costs. The micro-scale LNGo solution can be deployed in rough terrain or remote regions, eliminating the need to establish an expensive gas pipeline infrastructure or arrange for long-distance trucking of LNG from centralized plants to point of use. It can function as a decentralized solution where the requisite pipeline infrastructure is lacking, or as an onsite transformation solution to reduce or eliminate flaring of petroleum gas at, for example, oil rigs or producing gas fields.
Siemens AG is constructing a modern and sustainably designed Siemens Campus Erlangen in the southern part of the city of Erlangen, Germany. By 2030, the company's research center in the south of the city will have been transformed step-by-step into one of Siemens' most advanced locations worldwide. Future-oriented office, research and laboratory jobs will be located on the campus. Equipped with the most advanced building and energy technologies, it will be developed over the long term into Siemens' first CO
2-neutral location worldwide. A new urban residential and living environment will arise on the campus grounds. Siemens will be part of the community as never before. Designed by the Frankfurt architects KSP Jürgen Engel Architekten, the campus's open plan will link the company and society and provide a basis for the exchange of ideas.
The construction project has a planned investment volume of some €500 million and will cover an area of 54 hectares. Siemens Campus Erlangen underscores the company's long-term commitment to its Erlangen location and will be a symbol of innovative power for employees and for the region. The project was planned and designed in close cooperation with the state of Bavaria and the city of Erlangen.
- Largest private cogeneration project to date for Siemens in Mexico
Siemens has received an order to supply an
H-class gas turbine, one SST-800 steam turbine and two associated generators as
well as four switchgear units for the Altamira combined cycle cogeneration
power plant in Mexico. The entire power plant will have an electrical capacity
of around 350 megawatts (MW) and will also provide process steam, making this
the largest private cogeneration project to date for Siemens in this country.
In total, Siemens has now received orders for seven
H-class gas turbines from Mexico, including this order. Siemens’ customer is
the Mexican company Avanzia Instalaciones. The end customer is Alpek S.A.B. de
C.V., a subsidiary of Grupo Alfa, S.A. de C.V. Commissioning of the overall
facility is scheduled for end of 2018.
Within a period of just a few weeks, Siemens
has received orders from customers in Great Britain and the United States for a
total of nine compact steam turbines. The turbines are to be manufactured at
Siemens' production site in Frankenthal, Germany. Three SST-040 turbines have
been ordered by the Dutch energy provider Kara Energy Systems B.V. for biomass
power plants in Great Britain, while the U.S.-based company Airclean Energy in
Seattle, Washington, has placed an order for six SST-110 compact steam turbines.
Siemens has received its first order from
China for the
delivery of four SGT-800 gas turbines and the
associated generators.
The turbines will be installed in the Shanxi Guoxin
Baode and Xiyang decentralized
energy projects in Central China. The two combined cycle power plants with heat
extraction will have an overall capacity of 308 megawatts (MW). The
customer is Shanxi Natural Gas Limited Company, a subsidiary of Shanxi
Provincial
Guoxin Energy Development Group Co., Ltd.. Commercial
operation of the plants is scheduled for July 2017.
Siemens has received an order from Israel
for the first time for the turnkey construction of two industrial combined
cycle power plants. The two natural gas-fired power plants, Alon Tavor and
Ramat Gabriel, are to be built in northern Israel. Alon Tavor will supply a
creamery with electricity and process steam, while Ramat Gabriel will supply a
fiber factory. The Israeli energy provider, RD Energy, is the customer for both
power plants. Commissioning of the plants is scheduled for mid-2018.
Together with Munich Mayor Christian Ude, Siemens President and CEO Peter Löscher has laid the foundation stone for the company's new headquarters building, which will be completed on Wittelsbacherplatz in Munich by the end of 2015. The future inner-city complex will provide employees with a 21st-century working environment and be freely accessible to the general public at ground level. Siemens has set the highest standards for sustainability for its new headquarters, and will fulfill the criteria for minimum energy consumptions in buildings.