Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release21 June 2016Power and GasErlangen
Siemens wins first order for SGT-800 gas turbines in China

Four gas turbines of type SGT-800 will be installed in the Shanxi Guoxin Baode and Xiyang combined cycle power plants.
Siemens delivers four gas turbines of type
SGT-800 with the 54-MW rating to China. Two gas turbines and two generators are
to be installed in a 2x1 combined cycle power plant with heat extraction at
each site. Siemens also supplies all associated auxiliary systems as well as installation and commissioning services for the projects. Both
combined cycle power plants will be fired with coalbed methane, a form of
natural gas from an unconventional gas reservoir with high hydrogen content.
The SGT-800 is able to fire this gas due to its high fuel flexibility.
"This first order of SGT-800 gas
turbines is a breakthrough success for us on the fast developing Chinese
decentralized energy
market," said Yao Zhen Guo, Country Division Lead for Power and
Gas and Wind Power and Renewables in China. "As a trustworthy partner, we are
happy that we can support Guoxin Energy with world leading gas turbine
technologies."
"We are pleased to cooperate with Siemens for our
key decentralized energy project," said Liang Xiehu, Chairman of Shanxi
Provincial Guoxin Energy Development Group Co., Ltd.. "The success
of the project requires strong and committed
partners, and we are convinced
that
with its technology expertise and proven successful references across the
globe, Siemens is the right one."
Worldwide 297 SGT-800 gas turbines have been sold and the fleet has
accumulated about 4 million operating hours. The efficiency and steam-raising
capability of the SGT-800 makes the turbine especially suitable for
cogeneration and combined cycle applications. The high reliability and high
efficiency of the gas turbine promote both a low life-cycle cost and a small
environmental footprint.
According to China's 12
th
Five-Year Plan for Renewable Energy Development, China will pay high attention
to develop the decentralized energy market, especially fueled by natural gas.
Siemens supports these ambitious goals with the delivery of gas turbines for
the Shanxi Guoxin Baode and Xiyang power plants.
For further information on the Siemens gas
turbine SGT-800, please see:
www.energy.siemens.com/hq/en/fossil-power-generation/gas-turbines/sgt-800.htm
For further
information on Power and Gas Division, please see:
www.siemens.com/about/en/businesses/power-and-gas.htm
For this press release
Follow us on Twitter
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of gas and steam turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2015, which ended on September 30, 2015, Siemens generated revenue of €75.6 billion and net income of €7.4 billion. At the end of September 2015, the company had around 348,000 employees worldwide. Further information is available on the Internet at
www.siemens.com.