Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Feature18 January 2017,
updated19 January 2017Gas and PowerErlangen

The Dresser-Rand business, part of Siemens Power and Gas, has commissioned its first micro-scale natural gas liquefaction system at the Ten Man liquefied natural gas (LNG) facility in Pennsylvania, U.S. The modular, portable LNGo technology enables distributed production of LNG and can be installed in a short period of time to meet local demand for LNG. This cost-effective solution, developed by the Dresser-Rand business, allows the operator, Frontier Natural Resources, to monetize stranded gas assets at Tenaska Resources LLC's Mainesburg field, located in the Marcellus shale play. Frontier Natural Resources is an independent natural gas producer focused on developing conventional and unconventional resources.
The scope of supply included a standardized LNGo solution consisting of four different modules, each handling one step of the liquefaction process. The whole LNGo system can be transported on eight trucks. It is deployed directly at the gas field and has a footprint of approximately 508 square meters, roughly the size of a basketball court. The Ten Man facility commenced production just four months from contract signing, and has produced approximately half a million liters of LNG in the first 20 days.
"This project demonstrates our unique capabilities to deliver innovative solutions for oil and gas applications that help our clients maximize the value of their assets," said Michael Walhof, sales director Distributed LNG Solutions for the Dresser-Rand business. "We are proud to provide Frontier Natural Resources with a reliable, robust solution to liquefy natural gas and cost-effectively move it to market."
The LNGo technology makes it possible to monetize stranded gas deposits due to its relatively low capital and operating costs. The micro-scale LNGo solution can be deployed in rough terrain or remote regions, eliminating the need to establish an expensive gas pipeline infrastructure or arrange for long-distance trucking of LNG from centralized plants to point of use. It can function as a decentralized solution where the requisite pipeline infrastructure is lacking, or as an onsite transformation solution to reduce or eliminate flaring of petroleum gas at, for example, oil rigs or producing gas fields.
The scope of supply included a standardized LNGo solution consisting of four different modules, each handling one step of the liquefaction process. The whole LNGo system can be transported on eight trucks. It is deployed directly at the gas field and has a footprint of approximately 508 square meters, roughly the size of a basketball court. The Ten Man facility commenced production just four months from contract signing, and has produced approximately half a million liters of LNG in the first 20 days.
"This project demonstrates our unique capabilities to deliver innovative solutions for oil and gas applications that help our clients maximize the value of their assets," said Michael Walhof, sales director Distributed LNG Solutions for the Dresser-Rand business. "We are proud to provide Frontier Natural Resources with a reliable, robust solution to liquefy natural gas and cost-effectively move it to market."
The LNGo technology makes it possible to monetize stranded gas deposits due to its relatively low capital and operating costs. The micro-scale LNGo solution can be deployed in rough terrain or remote regions, eliminating the need to establish an expensive gas pipeline infrastructure or arrange for long-distance trucking of LNG from centralized plants to point of use. It can function as a decentralized solution where the requisite pipeline infrastructure is lacking, or as an onsite transformation solution to reduce or eliminate flaring of petroleum gas at, for example, oil rigs or producing gas fields.
Press Pictures
Infographics