Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens to supply nine compact steam turbines to Great Britain and the United States

The energy provider Kara Energy has placed an order for three compact SST-040 steam turbines to power biomass power plants in Great Britain.

"These new orders underscore the growing demand for small units to serve distributed energy-producing solutions," emphasizes Volker Neumann, Siemens' location manager at the Frankenthal plant. "With both these orders, we are contributing to sustainable energy supply in Great Britain and the United States."
The three SST-040 turbines, designed to deliver an electrical generating capacity of 300 and 420 kilowatts (kW), will be deployed in three biomass power plants in Great Britain. These power plants are scheduled to begin operation between November 2016 and February 2017. Siemens has already received three identical orders from Kara over the course of the past twelve months.
This marks the first time that Siemens is supplying an SST-040 with an output higher than 300 kW. The unit is based on the technology of the existing SST-040 turbine, but expanded due to growing customer demand for turbines with outputs over 300 kW. This technical advancement enables the SST-040 to now achieve electrical generating capacities of up to 750 kW. The turbine, gearing, electrical generator and all related equipment units are installed on a common base frame. Weighing some 4,500 kg, this virtually maintenance-free machine is a lightweight among steam turbines. Thanks to the compact design, the unit requires just a very small foundation.

Six compact SST-110 steam turbines will be deployed in process steam systems at industrial facilities in the Midwestern U.S.

The U.S. company Airclean Energy is integrating the six compact SST-110 steam turbines into complete facilities. The turbines with an output of 3 megawatts each will be deployed in process steam systems at industrial facilities in the Midwestern U.S. They will replace steam pressure reducing valve (PRV) stations, optimizing the efficiency of the steam cycle. This type of retrofit is subsidized by many utilities in a number of U.S. states. 
Pressure reducing valve stations are used to reduce boiler steam pressure to the pressure needed by the system. Different systems within an industrial facility have different operating pressure demands. When steam pressure is reduced through a valve, significant energy is lost. Airclean Energy is recovering this lost energy by reducing the steam pressure through the Siemens turbine and running a generator that will offset electrical energy consumption at the facility. The benefit of the SST-110 is its ability to reduce pressure to two different pressure levels at once, satisfying multiple consumers through one turbine. Many industrial facilities run at two different pressure levels, making this turbine an ideal choice for industry.
For further information on compact steam turbines, please see:
www.energy.siemens.com/hq/en/fossil-power-generation/steam-turbines/steam-turbine-products.htm

For this press release

Press Folders

Follow us on Twitter

Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 165 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is No. 1 in offshore wind turbine construction, a leading supplier of gas and steam turbines for power generation, a major provider of power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2015, which ended on September 30, 2015, Siemens generated revenue of €75.6 billion and net income of €7.4 billion. At the end of September 2015, the company had around 348,000 employees worldwide. Further information is available on the Internet at  www.siemens.com.
Read more
Reference Number: PR202001175766en

Contact

Uwe Schuetz

+49 203 605-2521