- Both companies kick off developments to ensure quality and trust in
a machine-to-machine (M2M) connected world
- The aim is to provide instant accessibility to quality and safety
information with a single source of truth to enable disruptive business models
- Anchoring physical products in the digital world using smart
contracts, blockchain and industrial edge
Merck, a leading science and technology
company, and Siemens, an innovation leader in automation and digitalization,
Germany, plan to develop and implement solutions that offer unprecedented
levels of digital trust in M2M connected industrial value chains. This would
help industrial customers to comply with stricter regulations in the value
chain in different countries and enable disruptive business models in a variety
of industrial sectors, ranging from the food and beverage, pharmaceuticals and
electronics industries to the automotive industry.
The best of two
worlds – EMO 2021, Siemens is going hybrid. Under the motto
"Digitalization in Machine Tool Manufacturing - Infinite opportunities
from infinite data", Siemens will be demonstrating at EMO Milano and at
the virtual Siemens Machine Tool Days 2021, which will be held at the same
time, how the full potential of data can be used for higher productivity. This
is because combining the real world with the digital world enables
manufacturers and users of machine tools to act flexibly and sustainably.
You can experience the Siemens solutions live and meet with the experts in person at the EMO exhibition booth (Hall 7 | E06) in Milan. Or visit the Siemens Machine Tool Days (SMTD) online – Virtual Experience with virtual showroom, auditorium and Meet-the-Expert sessions.
Register here:
www.siemens.com/emo
- Two new edge devices enable scalability of industrial edge offering for machine tools
- Analyze My Workpiece /Capture now also captures
data from external sensors
- Software applications available via Machine
Tool Software Store
Siemens is
expanding its Industrial Edge offering for machine tools with two new edge
devices. In addition to the already available IPC227E, there is now the
IPC127E, an entry-level device, and the IPC427E, the most powerful edge device
for machine tools. The IPC127E serves as an entry-level solution to provide
connectivity and performance for simple use cases. With the IPC427E, Siemens is
launching a device with sufficient computing power to meet the demands of
AI-based edge applications and sophisticated data analytics. The new Simatic
ET200 adapter also offers the possibility of connecting additional external
sensors and acquiring their data at a sampling rate of up to 10kHz. For this
purpose, the already known edge application Analyze MyWorkpiece /Capture has
received an update. In addition to data on the workpiece, tool and tool path,
this app can now also record data from external sensors in high temporal
resolution. As a novelty, the app can also stream process data via MQTT to an
external MQTT endpoint. In addition, users can visualize the workpiece of a
5-axis machining operation with the newly developed online coordinate
retransformation from the machine coordinate system to the workpiece coordinate
system. This is interesting because the visualization of the machining axes in
visualization applications such as Analyze MyWorkpiece /Toolpath gives no
indication of the machined workpiece. All other recorded data can subsequently
be visualized and analyzed with Analyze MyWorkpiece /Toolpath. The insights
gained enable optimization of the CAD/CAM model and the generated NC program. In
addition, Analyze MyWorkpiece /Toolpath now allows the creation of a realistic
surface reconstruction using process data recorded with Industrial Edge for
Machine Tools. This allows the workpiece quality to be evaluated before a
workpiece has even been manufactured, because the surface reconstruction also
works with process data from an air cut.
- Sinumerik One is in operation at the BMW Group plant in Steyr, Austria
- High performance through integrated Simatic S7-1500F
Siemens supplies automation hardware and software to the BMW Group. The automation solution includes, among other things, the new generation of the Sinumerik One CNC control, which offers digital possibilities to increase productivity in production. The new automation portfolio will be used at the Steyr production plant in Austria to produce the electric drive housing. It will also help to transform production for the digital age. Siemens and the BMW Group have a long-standing partnership. The success of both companies is based on driving innovation and developing forward-looking technologies, while at the same time focusing on sustainability.
- New NCU 1740 for higher scalability of Sinumerik One
- Sinumerik Run MyRobot /Direct Control V2.0 and Run MyRobot /Direct Handling V2.0 available for Sinumerik One
- New functions for the Digital Twin in Create MyVirtual Machine and Run MyVirtual Machine
Siemens is expanding its offering for the "Digital Native" CNC Sinumerik One. Two years after its market launch, the technology company is presenting numerous innovations in hardware and software for the Sinumerik One at EMO Milano and the virtual Siemens Machine Tool Days. In this context, Siemens is demonstrating how the powerful machine tool controller can be used in a highly productive, flexible, and modular way and in the best possible way for digital transformation. In terms of hardware, the new NCU 1740 complements the existing NCU 1750 and 1760 as well as the PPU 1740, thus expanding its use in modular machines.
- Enables secure, on-demand remote access to OT applications and systems
- Delivers Zero Trust OT/IT security approach for office and production networks
- Improves plant uptime and efficiency with secure remote access
Siemens and Zscaler, Inc. (NASDAQ: ZS), the leader in cloud security, are partnering to enable customers to securely access Operational Technology (OT) systems and applications in the production network from the workplace – whether in the office or working remote. These new capabilities enable users to remotely manage and control quality assurance or diagnoses issues.
Matthias Rebellius, Member of the Managing Board of Siemens AG and CEO of Smart Infrastructure, will highlight and discuss the latest trends in the field of infrastructure and the integration of eMobility. Cedrik Neike, Member of the Management Board of Siemens AG and CEO Digital Industries, as well as other executives, will give you a closer look at the developments around all things mobility and what the future has in store.
- Launch of Simulytic, a Siemens venture, accelerates the move to safe, autonomous mobility
- World premiere of Siemens Autonomous Charging System
- Partnership with Verein Sozialhelden e.V.: Siemens committed to easing use of charging infrastructure by the disabled
- Siemens is official charging infrastructure partner for the Blue Lane Road at IAA Mobility 2021
- #MoveToTransform campaign in Munich embodies the spirit of the IAA Mobility and shows the faces behind mobility’s transformation
For Siemens,
it’s a home game of a special kind: taking as its motto #MoveToTransform, the
company is exhibiting at the IAA Mobility 2021, which is being held for the
first time in Munich, Bavaria’s capital and Siemens’ hometown. As a focused
technology company, Siemens is presenting a holistic look at mobility for today
and for the future. The focus is on how the real and digital worlds are combined
in technical products and digital solutions to make industry, infrastructure
and transportation more intelligent, efficient and sustainable.
- Siemens Large Drives Applications (LDA) to deliver a high voltage (HV) motor with 105 MW and a 40 MW starting frequency converter for an energy storage project in China
- The motor will have an efficiency of beyond 98 percent
Siemens LDA has received an order from a Chinese customer to deliver a special machine with dual shaft extension. It can be used in motor operation with a power of 105 MW and as generator with up to 129 MVA in power generation mode. The motor will have an efficiency of beyond 98 percent and will be a world-leading 2-pole electric motor.
Beside the motor, the contract includes the delivery of a 40 MW Sinamics GL150 starting frequency converter. This LCI-converter (load commutated inverter) is designed for single-motor applications with variable and constant torque characteristics. As a result of the low switching losses and the low loss thyristor technology, the efficiency of the LCI converter is extremely high and lies at 99 percent.