- New Intelligent Valve with heat exchanger optimization for heating groups and air handling units
- Reliable automatic commissioning via direct download of parameters from the cloud
- Flexible mounting options to fit the space available
The Intelligent Valve is the first self-optimizing dynamic valve for heating groups and air handling units from Siemens Smart Infrastructure that can be connected to the cloud. The device controls the flow, measures temperature and output, and automatically adjusts the valve settings to the heat exchanger. The valve can be commissioned quickly and reliably via wireless LAN using the Siemens ABT Go app. It fits the space available thanks to flexible mounting options, allowing the flow sensor, valve and controller box to be installed separately. Because additional functions can be downloaded from the cloud at any time, the Intelligent Valve is always up to date.
- Buildings connected in a microgrid support decentralized energy markets of the future
- Flexible energy consumption, storage and load balancing
- Ecological benefits for society as well as new revenue streams for buildings customers
Siemens Finland has created a new business to expand its virtual power plant activity: Vibeco (Virtual Buildings Ecosystem) is an innovative approach to increase the benefits of increasingly decentralized energy systems. The heart of the virtual power plant is a software platform, operated by Siemens, that intelligently balances electrical loads from buildings that have been connected in a microgrid, incorporating renewable energy and energy storage.
At this year's "The smarter E-Europe," Siemens is demonstrating its role in shaping an increasingly decentralized energy landscape. Siemens will show how the digitalization of renewable energy generation, storage and distribution positively impact the energy transition and sustainability goals.
- New IP routers and IP interfaces ensure secure data and access-proof KNX communication over IP
- KNX IP Secure devices meet the highest security requirements in smart buildings
- More flexibility in power supply minimizes KNX bus current consumption
Siemens Smart Infrastructure expands the proven Gamma instabus building system with new IP routers and IP interfaces that support the latest KNX IP Secure standard. This extension of the KNXnet/IP protocol enables fully encrypted transmission of data telegrams, thus ensuring secure data- and access-proof communication between KNX IP routers within a single network.
- Spectrum Power ADMS to provide reliable energy supply for 1.5 million people
- One multi-site system to handle all voltage levels
Hafslund Nett, Norway's largest grid company has contracted Siemens to supply a new Advanced Distribution Management System (ADMS) for the operation of the regional power grid in Akershus, Oslo and Østfold. The fully integrated grid operating center will enable monitoring and control of the complete power grid covering all (high-, medium-, low-) voltage levels. At the same time, it will allow easy integration of third-party IT/OT systems, such as customer information systems, workforce management or geographical information systems. The project is expected to be operational at the beginning of 2022.
- New rail-mounted devices added to Gamma instabus product line
- New switch actuators with load current detection, new switching/dimming actuators and new sun protection actuators
- Powerful and universal applications across all devices, short installation times, low maintenance costs
Siemens Smart Infrastructure is expanding its Gamma instabus KNX-based product line with new switch actuators with load current detection, new switching/dimming actuators and new sun protection actuators. The new actuators are designed for residential and commercial buildings and provide reliable switching and monitoring of loads, switching and dimming of fluorescent lamps via 1 to 10 Volt control outputs, and control of alternating current motors for sunshades and ventilation valves.
- Safer and more efficient: Catania Airport is updated with integrated building automation by Siemens
- More reliable and accurate fire detection using Sinteso connected to the Desigo CC building management software
- Cloud-based Navigator software to optimize energy consumption
With almost ten million passengers in 2018, Catania Airport is continuing to grow, solidifying its number one position in southern Italy. This makes the hub an increasingly important strategic part of the Mediterranean aviation network. As a result, however, it faces greater security and energy efficiency challenges. This is the context in which the Sicilian airport made the decision to entrust Siemens with its integrated building automation project, intended to increase security levels and monitor overall energy consumption at the hub.
- Stimulating two senses through acoustic (EN 54-3) and optical (EN 54-23) alarm devices
- Voice messages can be emitted in two languages for faster evacuation
- High alarming reliability thanks to daily disturbance-free tests
Siemens Smart Infrastructure has launched new ceiling- and wall-mounted alarm devices. The expanded portfolio includes both acoustic and optical alarm devices in accordance with European Standards EN 54-3 / EN 54-23 and EN 54-17. One highlight of the expanded portfolio are the voice sounders with built-in voice messages because they improve the reaction time to alarms.
With the Junelight Smart Battery, Siemens is offering its first battery storage specially geared to the requirements in private homes for the storage and use of self-generated energy. The lithium-ion storage combines functions for intelligent and safe energy management and a modern design. Homeowners can use it to maximize the share of their self-generated energy, e.g. from photovoltaic systems, for their own consumption, to minimize their energy procurement costs and to make a long-term contribution towards the reduction of CO2 emissions. The Junelight Smart Battery coordinates the predictive charging and discharging procedures depending on the weather-related yield forecast of the photovoltaic system and the individual consumption profile of the household. Using the mobile Junelight Smart App, all energy flows – from production, through storage, right down to consumption and grid in-feed – can always be monitored in real time. The storage capacity can be flexibly adapted to individual needs at any time, encompassing up to 19.8 kilowatt hours (kWh). The Junelight Smart Battery is now available in Germany and will be launched in Austria in April 2019.