Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Intelligent Valve from Siemens: self-optimizing and connected to the cloud

The picture shows a self-optimizing dynamic valve.

The picture shows a self-optimizing dynamic valve.

Intelligent Valve optimizes heat exchangers
Temperature, flow rate and energy are measured continuously. Based on the measurements, the Intelligent Valve checks whether its settings are line with the heating or cooling behavior of the heat exchanger. The valve adjusts automatically, e.g., to changing values caused by contamination during operation, thus avoiding repeated manual readjustments across the life cycle of the system. At the same time, the Intelligent Valve's heat exchanger optimization feature ensures that heating, ventilation and air conditioning (HVAC) systems operate energy-efficiently at all times. For instance, the valve detects the flow rate at which additional energy from the heat exchanger can no longer be efficiently converted into higher heating or cooling output.
Commissioning of the Intelligent Valve is automatic, quick and reliable. Different methods can be used to transfer the datasets to the valve. The twin datasets can be downloaded directly to the valve from the Desigo ABT Site commissioning tool or using the ABT Go app. Connecting the valve directly to the cloud is an even more convenient option, allowing values set during the planning phase to be adjusted later on via remote access. Values can be optimized at any time, even during operation. In addition to wireless LAN and direct cloud connection, the Intelligent Valve offers a third communications interface: BACnet/IP.
Flexible mounting options
Since space is often tight during renovations and modifications, the Intelligent Valve offers very flexible mounting options. To save space, the ultrasonic flow sensor can be installed in the flow and the valve in the return. The controller box can be mounted parallel or crosswise to the pipe, allowing sufficient space for insulation work, or separately on the wall. Color-coded plug-in connectors make connecting the flow sensor, valve and controller box fast, easy and error-free.
The Intelligent Valve's control functions allow for automatic dynamic balancing of the hydronic system, similar to PICVs (pressure-independent combi valves). Dynamic hydronic balancing automatically compensates for pressure fluctuations, thereby avoiding temperature variations in the building and improving the comfort level for building users. There is no need for circuit control valves, balancing throttles or complicated hydronic calculations.
In the Siemens Building Operator cloud application, the Intelligent Valve creates reports with valve settings and energy consumption values. The reports can be viewed at any time and used for system acceptance and energy monitoring. If the valves are integrated into the Desigo building management system, they can be easily adjusted to changing operating conditions. Automated function tests or energy-optimized solutions can be downloaded into the valves later on.

For further information on Siemens Smart Infrastructure, please see
www.siemens.com/smart-infrastructure
For further information on the Intelligent Valve, please see
www.siemens.com/intelligentvalve
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 71,000 employees worldwide.
Read more
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2018, which ended on September 30, 2018, Siemens generated revenue of €83.0 billion and net income of €6.1 billion. At the end of September 2018, the company had around 379,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR2019050263SIEN

Contact

Catharina Bujnoch-Gross

Siemens AG

Theilerstrasse 1a
6300 Zug
Schweiz

+41 (79) 566-0778