At "SPS – Smart Production Solutions" 2019, Siemens will present sector-specific applications and future technologies for the digital transformation of the discrete and process industries. At the heart of the 4000 square meter booth will be new products, solutions and services from the Digital Enterprise portfolio, which can be used to merge the real and virtual world.
On November 26, the first day of SPS, Klaus Helmrich spoke at the Siemens press conference, which took place in the trade show Convention Center. Mr Helmrich discussed the latest trends in digitalization and the next stage of digital transformation in the discrete and process industries.
- New Version V16 of the TIA Portal engineering framework with focus on standardization and continuous integration
- Enhanced engineering efficiency with distributed working in the developer team
- Increased software quality thanks to integrated Test Suite
- Transparent operation with cross-vendor OPC UA communication
With the new TIA Portal V16 (Totally Integrated Automation Portal), Siemens has expanded its engineering framework with practical new functions for various phases from planning, to engineering, to commissioning. The innovations concentrate on the continuous integration of the development process. These include standardization, integrated engineering spread across teams and an integrated function test. This enables users to increase the quality of their software, shorten commissioning times and reduce engineering costs.
- Digital Enterprise portfolio aimed at meeting increasing requirements for greater productivity and flexibility as well as environmental efficiency
- New platform innovations ensure integration and flexibility across all stages of the value chain
- Growing ecosystem for Industrial Edge and Cloud enables scalability from the shop floor to the Cloud
Through innovations and the integration of cutting-edge technologies into the Digital Enterprise portfolio, Siemens helps companies from all sectors to achieve a more flexible and environmentally efficient production. “The Digital Enterprise portfolio is already well established globally in all industries for the implementation of Industrie 4.0. Many applications demonstrate the tangible benefits of these solutions for our customers,” explains Klaus Helmrich, Member of the Managing Board of Siemens AG and CEO of Digital Industries, at SPS. “Now we are taking the next step: with numerous innovations und cutting-edge technologies, we are taking the Digital Enterprise portfolio and therefore Industrie 4.0 to a new level.”
- Sustainable technological cooperation for the future of industrial wireless communication
- Joint Proof of Concept in a real industrial environment using the 3.7-3.8 GHz band
- Researching the capabilities of 5G standalone networks for industrial applications
Siemens and Qualcomm Technologies, Inc. have implemented the first private 5G standalone (SA) network in a real industrial environment using the 3.7-3.8GHz band. Both companies have joined forces in this project: Siemens is providing the actual industrial test conditions and end devices such as Simatic control systems and IO devices and Qualcomm Technologies is supplying the 5G test network and the relevant test equipment. The 5G network was installed in Siemens’ Automotive Showroom and Test Center in Nuremberg. Automated guided vehicles are (AGV) displayed here which are primarily used in the automotive industry. New manufacturing options and methods are also developed, tested and presented before they are put into action on customer sites. This allows Siemens’ customers, such as automated guided vehicle manufacturers, to see the products interact live.
At SPS 2019, Siemens presents its latest solutions
for smart and networked drive technology. By networking entire drive systems, machine
and plant builders as well as users can simulate machines and plant more
accurately using digital twins, perform commissioning, reduce downtimes and therefore
increase productivity.
- Exact recording of energy consumption and electrical parameters
- Secure data transfer over existing communication networks
- Flexible use in industrial and commercial buildings as well as data centers
Siemens Smart Infrastructure has added the 7KM PAC3220 and 7KM PAC3120 measuring devices to its Sentron power monitoring portfolio. These devices capture energy and system data from buildings, infrastructure and industrial facilities and transfer them via standard communication protocols to higher-level energy management, automation and IoT systems. This data can then be used to identify energy hogs, detect system malfunctions as early as possible and proactively prevent downtimes. This allows companies to sustainably boost their energy efficiency and system availability. The new devices offer higher accuracy than the previous models and have a new design.
- Easy connection to Simatic controllers using plug-in connectors
- Integration
in TIA Portal supports quick commissioning
Simatic
Micro-Drive F-TM Servodrive is the newest member of the Simatic Micro-Drive
family. The servo drive system comprises a Simatic Micro-Drive F-TM Servodrive
drive controller module, the Simatic ET 200SP and universal motors and plug-in
cables. It adds to the Simatic Micro-Drive PDC (ProfiDriveControl) and
completes the drive portfolio in the protective extra-low voltage range for EC
motors from 24 to 48 volts. The drive controller module supports dynamic and
accurate positioning in a small amount of space in the performance range up to
280 watts.
Control rooms of process engineering plants are usually
as old as the plant itself, often 30 years and more. Today, digital
transformation is placing new demands on automation: Simatic PCS neo is a brand-new system software, which
offers companies in the process industry unique opportunities in the age of
digitalization. Main features include global web-based collaboration in
engineering and operation and intuitive handling representing all relevant
information in a single workbench.
Under the motto "Thinking industrialized Additive Manufacturing further", Siemens will be presenting its comprehensive portfolio for the industrialization of additive manufacturing at formnext 2019, the leading trade fair for additive manufacturing and 3D printing, tailored to the respective industries. With the concept of the Digital Enterprise portfolio, Siemens is pursuing a holistic approach - from the point of view of machine builders and machine users alike. With the Digital Enterprise portfolio, Siemens offers a holistic, end-to-end solution to leverage a seamless value chain from functional design through manufacturing to value-added services.The range of industrial software and automation also includes leading simulation software and CNC technology. The Digital Enterprise portfolio enables the full utilization of digital twins that reflect the real world for machine users and machine manufacturers to ensure "first-time-right" printing.
Siemens at Formnext 2019 can be found in Hall 12.1 D81.
- Simatic S7-1500 controller with expanded motion control functionality and Sinamics S120 drive control in one device – thus saving space
- Powerful for high-end applications, with integrated safety functionality for the controller and drive
- Extensive communication interfaces, technology I/Os, as well as cross-PLC synchronous operation for an easy implementation of modular machine concepts
- Proven engineering in the TIA Portal
Siemens is expanding its product portfolio of technology CPUs with the Simatic Drive Controller. The new controller combines a Simatic S7-1500 controller with motion control, technology and safety functionality with a Sinamics S120 drive control in one device, thus saving space. This makes it easy to implement requirements for powerful, compact and flexible automation solutions. The high performance of the new controller is particularly beneficial for applications with many axes where a multi-axis drive system is used – for example in packaging, printing and textile machines.