Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser
Press Release26 November 2019Digital IndustriesNuremberg
Engineering framework ready for continuous software development

During the development process, the focus is on distributed working concepts and teamwork. On the TIA Portal project server, the user can now exclusively access server projects via the new Exclusive Engineering function – with features such as project revision and change protocol, as well as automated reporting and archiving. This means there are no functional restrictions when organizing automation tasks on a device, object or function-oriented basis. No special license is required for using Exclusive Engineering. To enable projects to be commissioned by teams, TIA Portal V16 has been expanded with an “asynchronous commissioning” mode, whereby loading to the Simatic S7-1500 controller is carried out by a second TIA Portal instance running in the background. The TIA Portal instance running in the foreground can be operated again immediately, enabling load times to be considerably shortened. TIA Portal V16 includes the new Version Control Interface (VCI) to external versioning systems such as GIT, SVN and TFS. The import and export of software objects via the TIA Portal interface allows versioning to be seamlessly integrated into the development process. This enables object-granular, completely transparent versioning of all software objects outside the TIA Portal. Another innovation is the TIA Portal Test Suite. In addition to allowing automated creation and checking of adherence to programming guidelines, the so-called Styleguide Check, it is also possible to generate and carry out application tests with the virtual S7-PLCSIM Advanced controller. This support reduces engineering and commissioning times and enhances the quality of the software.
With TIA Portal V16, all Simatic S7-1200 controllers are now equipped with OPC UA server functionality. Connection to higher-level systems, such as manufacturing execution systems, can be implemented for vertical data integration. Controller-controller communication throughout all Simatic controllers is also now possible using OPC UA. Standardized interfaces, known as companion specifications, are simple to import with the TIA Portal, making it easy to integrate machines in production lines or plants. The SiOME Siemens OPC UA Modelling Editor helps the automation engineer with the interconnection of tags and simplifies their import into the Simatic machine control. The SiOME also has some new functions such as the creation of data blocks based on OPC UA information models, or the option of checking OPC-UA information models and companion specifications for conformity. Users can now model server interfaces or companion specifications in the TIA Portal V16. In simplified form and without the need for specialist knowledge, it is possible to create a server interface or use a companion specification. The OPC UA server functionality for the Simatic S7-1500 controllers has also been supplemented with additional diagnostic buffer entries: OPC UA messages can now be combined to only appear once in the diagnostic buffer.
The new Simatic Drive Controller has been integrated for motion control applications. It combines a Simatic S7-1500 control system with motion control, technology and safety functionality with a Sinamics S120 drive control in a single device, thus saving space. The new package also enables Simatic users to perform advanced motion control tasks, such as those involving multi-axis drive systems, in a familiar environment. Simatic WinCC Unified is also available in TIA Portal V16: The completely redesigned visualization system provides solutions for HMI and SCADA applications, and in the future also for Industrial Edge, Cloud and Augmented Reality scenarios. It includes a new generation of HMI devices which can be configured with TIA Portal V16, namely the Simatic HMI Unified Comfort Panels. In the latest TIA Portal version, the Simatic Energy Suite includes a load management function. This option automatically prevents load peaks by using intelligent strategies to switch generators and loads on and off, without influencing the production process. The Simatic Energy Suite engineering takes place in the TIA Portal: The user configures the load management via the screen form in the TIA Portal, program generation is completed, and the corresponding visualization configured.
Background information:
The TIA Portal (Totally Integrated Automation Portal) was launched by Siemens in 2010 and enables users to perform automation and drive tasks quickly and intuitively through efficient configuration. The software architecture is designed for high efficiency and ease of use and is suitable for both new and experienced users. It offers a standardized operating concept for controllers, human machine interfaces (HMIs) and drives for shared data storage and consistency, for example during configuration, communication and diagnostics, as well as powerful and comprehensive automation object libraries. The simple engineering in the TIA Portal facilitates full access to the entire spectrum of digitized automation, from digital planning and integrated engineering up to transparent operation. Alongside PLM (Product Lifecycle Management) and MES (Manufacturing Execution Systems) within the Digital Enterprise Software Suite, the TIA Portal complements the holistic range of software available from Siemens for companies on the path toward Industry 4.0.
For further information on Simatic WinCC Unified System, please see
www.siemens.com/wincc-unified
Additional Information about Simatic Drive Controller can be found at
www.siemens.com/drive-controller
Additional information about Siemens at SPS 2019 can be found at
www.siemens.com/press/sps19 and www.siemens.com/sps19
www.siemens.com/wincc-unified
Additional Information about Simatic Drive Controller can be found at
www.siemens.com/drive-controller
Additional information about Siemens at SPS 2019 can be found at
www.siemens.com/press/sps19 and www.siemens.com/sps19
For this press release
Siemens Digital Industries (DI) is an innovation leader in automation and digitalization. Closely collaborating with partners and customers, DI drives the digital transformation in the process and discrete industries. With its Digital Enterprise portfolio, DI provides companies of all sizes with an end-to-end set of products, solutions and services to integrate and digitalize the entire value chain. Optimized for the specific needs of each industry, DI’s unique portfolio supports customers to achieve greater productivity and flexibility. DI is constantly adding innovations to its portfolio to integrate cutting-edge future technologies. Siemens Digital Industries has its global headquarters in Nuremberg, Germany, and has around 76,000 employees internationally.
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at www.siemens.com
.
Contact
Andreas Friedrich
Digital Industries
Gleiwitzer Str. 555
90475 Nuremberg
Germany
90475 Nuremberg
Germany
+49 (1522) 2103967