- Voltage variant of Sinamics G120X for USA and Latin America
- Save space with new size for the Sinamics V20
- Adapter kit to physically and thermally separate power module and control unit for Sinamics G120
With numerous innovations, Siemens is extending its drive portfolio, improving user-friendliness and offering space-saving installation options. The Sinamics G120X converter, designed specifically for use in water/wastewater applications and in HVAC systems, is now also available in a three-phase 3AC 200V voltage variant in the power range up to 55 kW. This means that the converters can now be integrated seamlessly into applications in the USA and in Latin America. Due to its robust construction and the coating of the PCBs according to 3C3 standard the converter is suitable for harsh environments. The new module for extending the digital and analog inputs and outputs increases the flexibility and the optimal control of converter-guided applications. The Sinamics G120X now also supports the communication protocols Profibus, Modbus RTU, USS and BACnet MS/TP. It is equipped with extensive interfaces and can be easily integrated into existing or new systems.
- Siemens announces projects to be supported in the Third Funding
Round
- Up to US$ 30 million in funding to be awarded
- Siemens Integrity Initiative's
funding volume exceeds US$ 100 million
As part of the Siemens Integrity Initiative, which has a funding volume
of more than US$ 100 million, Siemens AG has named new projects to receive
funding in order to promote corruption-free markets.
- New power output module boosts HCS4300 heating control system performance
- HCS4200: space-saving solution for use in flat control cabinets with new CIM4210C central interface module
- Simple, convenient engineering and commissioning of industrial heating processes with TIA Portal
Siemens
has equipped the modular Siplus HCS heating control systems for
switching and controlling heater fields and elements with a new power output
module (POM) and a central interface module (CIM). With more power per output
and a space-saving solution for mounting in flat control cabinets, the flexible
heating control system is now even more versatile, and can be used for example
in applications with heat registers.
- Shorter development and commissioning times
- Software libraries enable standardization
- Commissioning tests on virtual test rack
The new Sinumerik One CNC generation is at the heart of digital transformation for machine tools. As a digital native, the controller features not only a new hardware platform, but also versatile software for the creation of a digital twin. It closes the gap between the virtual and the real world and helps to reduce development and commissioning times considerably.
- Kayser
to take on new role at beginning of 2020
- Current
head, Jochen Eickholt, is moving to Siemens Energy
Horst J. Kayser
(58) will be the new Chairman of the Siemens Portfolio Companies (POC),
effective January 1, 2020. In this capacity, he is succeeding Jochen Eickholt, who
is becoming a member of the future Executive Board of Siemens Energy, where he
will be responsible for the Power Generation and Oil & Gas units. Kayser is
currently still Head of Strategy at Siemens AG. Until further notice, he will
continue to lead this department on an acting basis in addition to his new role.
As POC Chairman, Kayser will report directly to Deputy CEO Roland Busch.
- Next generation of Simatic ET
200eco PN: New functions for modern machine concepts and requirements
- For use in redundant,
high-availability systems thanks to S2 redundancy
- High current-carrying capacity with
power supply via L-coded plug
- High-quality industrial enclosure with IP65/67
protection for outdoor use
Siemens has launched a new generation of machine-level block I/O
devices in the form of the Simatic ET 200eco PN. The new I/O family with
IP65/67 degree of protection includes five digital I/O devices as well as an IO-Link master device and offers users a whole range of new
functions for modern machine concepts and requirements. In their new industrial
metal enclosure, the devices are reliably protected from UV radiation and
harmful substances even under adverse environmental conditions, making it
possible to use the devices outside of factory buildings. The devices are
supplied with power via an L-coded plug, resulting in a considerably higher
current-carrying capacity. In turn, this enables longer cable routes in the
field, and the supply and connection of more energy-intensive components (such
as valve terminals) without the need for more supply cables.
- Simatic S7-1500
firmware V2.8: Secure data integration, versatile diagnostics function for OPC
UA server
- Simatic S7-1200 firmware V4.4:
Improved cross-platform data transfer, OPC UA Data Access as server, OPC UA
Modelling Editor
Siemens announces the release of two firmware updates for
Simatic controllers that provide new functions. The Simatic S7-1500 firmware
V2.8 from Siemens improves cross-device capabilities for data integration and
diagnostics functions. The new Simatic S7-1200 firmware V4.4 extends the
communication functions of the Simatic S7-1200, enhancing cross-platform data
transfer with other controllers and higher-level or cloud-based systems such as
ERP, SCADA and Mindsphere. The applications are numerous, ranging from
industrial use to agriculture and infrastructure projects.
- Managing Board members’ individual
responsibility to have greater weight
- In addition to capital market
performance, sustainability targets included for first time
- Contractual maximum compensation
agreed
- New compensation system makes
Siemens a pioneer among DAX companies
Siemens intends
to adjust the compensation system for its Managing Board members in order to
align the system more closely with the company’s sustainable development and
thus with the Vision 2020+ company strategy. By implementing the new system, Siemens
is taking on a pioneering role because the new approach already reflects the
draft version of the German Corporate Governance Code of May 9, 2019, and the
draft version of the act transposing the European Union’s Second Shareholder
Rights Directive into German law. In addition, the new concept not only
considers performance on the capital market, but also places emphasis on
targets for environmental protection, professional development of employees and
customer satisfaction. In the future, the broad-based MSCI World Industrials
Index – instead of a comparison with five main competitors – will be the yardstick
for the comparisons that determine the value of the stock awards. The new Managing
Board compensation system, which already applies as of fiscal 2020, will be
submitted to shareholders for endorsement at the Annual Shareholders’ Meeting on
February 5, 2020.
- Most
of the inventors are from Germany, the others come from the U.S., Russia, China, the UK, Spain,
Italy and Romania
- Thirty-one
inventions per day in fiscal 2019
Siemens has honored 23 particularly resourceful researchers as Inventors of the Year 2019. Together, these scientists are responsible for some 1,450 inventions and 1,500 individual patents. Most of the inventors are from Germany, the U.S., Russia, China, the UK, Spain, Italy and Romania. Their inventions cover the whole spectrum of Siemens. They range from 3D animation for early detection of breast cancer to a new solution for electrifying old rail lines without the need for modifications to bridges and tunnels and continue all the way to a postcard-sized module for industrial controllers that uses artificial intelligence and is thus capable of revolutionizing automation in factories.
- New Version V16 of the TIA Portal engineering framework with focus on standardization and continuous integration
- Enhanced engineering efficiency with distributed working in the developer team
- Increased software quality thanks to integrated Test Suite
- Transparent operation with cross-vendor OPC UA communication
With the new TIA Portal V16 (Totally Integrated Automation Portal), Siemens has expanded its engineering framework with practical new functions for various phases from planning, to engineering, to commissioning. The innovations concentrate on the continuous integration of the development process. These include standardization, integrated engineering spread across teams and an integrated function test. This enables users to increase the quality of their software, shorten commissioning times and reduce engineering costs.