Deutsche Bahn
(DB) and Siemens Mobility are driving forward the climate-friendly transition
in transport and are testing the use of hydrogen for rail for the first time.
The aim is to test a completely new overall system consisting of a newly
developed train and a newly designed filling station.
Siemens Mobility to install a 2,000 km state-of-the-art high-speed rail network that will connect 60 cities throughout the country with trains that can operate up to 230 km/h. The integrated system will create the 6ᵗʰ largest high-speed rail network in the world, and will provide 90% of Egyptians access to a modern, safe, and affordable transportation system. The fully electrified network will cut carbon emissions by 70% compared to current car or bus transport, further supporting Egypt’s efforts in transforming its mobility to a more sustainable one. Siemens Mobility will deliver 41 Velaro high-speed trains, 94 Desiro High Capacity regional train sets, and 41 Vectron freight locomotives. This contract also includes the development of eight depots and yards and 15 years of maintenance.
Siemens Mobility's Vectron locomotives are used for both freight and passenger service. During the development of the locomotive, the focus was on providing a future-proof design, investment security, environmental compatibility, fungibility, retrofitting capability and convertibility. The Vectron can be delivered as a purely electrical version for operating with alternating current (AC) or direct current (DC) power systems as well as a multisystem (MS) variant in the power classes 5.2 MW, 5.6 MW and 6.4 MW. Along with the desired national train control system, the locomotives can also be equipped with the latest European Train Control System (ETCS). The locomotives are built in the Siemens Mobility plant in Munich-Allach, Germany. For freight transport in Germany, Siemens Mobility also offers the Smartron standard locomotive and the Vectron Dual Mode, a combination of diesel and electric locomotive.
Siemens AG has
launched an open digital business platform, Siemens Xcelerator, to accelerate
digital transformation and value creation for customers of all sizes in
industry, buildings, grids and mobility. The business platform makes digital
transformation easier, faster and scalable.
Deutsche Bahn (DB) and Siemens Mobility have
developed the world’s first train that operates by itself in rail traffic. Dr.
Richard Lutz, CEO of DB, and Dr. Roland Busch, CEO of Siemens AG, together with
Dr. Peter Tschentscher, Mayor of Hamburg, presented the train on the 11th
October 2021 as it made its premiere run as part of the Digital S-Bahn Hamburg
project.
Since
October 2019, Siemens Mobility and ViP (Verkehrsbetrieb Potsdam GmbH) have been
jointly researching a fully automated tram depot. One year before, the
cooperation partners presented a test vehicle of an autonomous tram at
InnoTrans 2018. On this basis, the consortium started further research together
with the Karlsruhe Institute of Technology (KIT), the Institute for Climate
Protection, Energy and Mobility (IKEM) and Codewerk GmbH. The market readiness
of the autonomous tram in the depot is planned for 2026.
The three-year project called “AStriD” (Autonomous Tram in Depot) is funded by the Federal Ministry for Transportation and Digital Infrastructure (BMVI) as part of its “Modernity Fund” (mFUND) research initiative.
- Mireo Plus H hydrogen train reduces CO2
emissions on routes around Augsburg
- Passenger service starts in mid-2024
Siemens Mobility has
completed the first test runs with the Mireo Plus H hydrogen-powered train in
Bavaria. The two-car trainset will enter passenger service in mid-2024 on
routes between Augsburg and Füssen and Augsburg and Peissenberg on the rail
network of Bayerische Regiobahn (BRB). Pilot operations of the train are
planned for 30 months and are supported by the State of Bavaria. Siemens
Mobility and Bavaria signed the corresponding development partnership in 2021.
Turkish State Railways (TCDD) has ordered Velaro high-speed trains from Siemens Mobility.The first Velaro Turkey was ordered in 2013 and went into passenger service between Ankara and Konya in May 2015. At the same time, TCDD signed a second contract with Siemens for six eight-car high-speed trains. The last twelve eight-car Velaro TR trains were ordered in 2018 and 2019. The contract included maintenance, repair, and cleaning of the trains for a period of three years. With the delivery well ahead of schedule, a record time for the start of passenger operation could be achieved. On average, the time between the contract signing and passenger operation amounts to 24 months.