- 22 trains from Siemens Mobility and Bozankaya in passenger service
- Enhanced passenger experience and more capacity
In Bangkok, Thailand, all 22 metro trains delivered by the consortium of Siemens Mobility and Turkish railway manufacturer Bozankaya are now in operation on the existing BTS (Skytrain System) Green Lines including its extensions. The last train entered service on the inaugurated Green Line extensions in October 2019. By the 4th of December 2019, Bangkok Mass Transit System Public Company (BTSC) will commence passenger service on the newly completed section of the Green Line from Kheha Station to Kasetsart University Station. In total, 22 four-car trains have been delivered with the scope of Siemens Mobility delivering bogies, drive and brake systems, auxiliary services as well as the project management, engineering, design and commissioning of the trains. The trains were built at the Bozankaya plant in Ankara, Turkey. Siemens Mobility will maintain the trains over a period of 16 years.
- Five sensors in a single device for optimal ambient conditions and maximum energy savings
- Control of lighting, ventilation and heating systems
- Precise readings, monitoring and control of energy consumption
- Fast installation thanks to a single KNX cable
The new presence detector WIDE UP 258Dx1 from Siemens Smart Infrastructure can now for the first time contribute to energy-efficient lighting and climate control without having to rely on additional accessories thanks to its built-in multi-sensor technology. It is part of the GAMMA instabus building system technology portfolio, a series of products based on the worldwide KNX standard and with five different sensors for HVAC and lighting control. Dedicated sensors record presence, brightness, temperature, humidity and CO2 levels, guaranteeing perfect room conditions in commercial buildings with substantial room depth and high occupancy fluctuations.
- New
signaling means seamless transition to automated train operation (ATO)
- Communications-Based Train Control (CBTC)
- Two
stations and 20 trains will be equipped
Siemens
Mobility, along with consortium partners ST Engineering and BES Engineering
Corporation, has been awarded a contract to deliver the signaling and
communications for two new stations at Taoyuan Airport terminal three. The
airport currently services more than 45 million passengers and with the opening
of terminal three capacity is expected to grow to up to 86 million passengers
per year. The mass transit system will provide access to the terminal for both current
and future passengers. Siemens Mobility will provide the signaling system,
which will include CBTC that will allow for automated train operations (ATO).
Two stations, with an option for a third, and 20 trains will be equipped. The
first station will be commissioned in September 2022, the second is planned for
in June 2024.
- New devices for electrical installations in industrial and infrastructure environments with a lower nominal current of 0.1 to 0.4 amperes
- Firmware update with improved control and diagnostic functions
- Failsafe group shutdown function without additional wiring
Siemens Smart Infrastructure is adding four new devices to its portfolio of Simatic ET 200SP motor starters, which can be used to start electric drives with a power output from 0.1 to 0.4 amperes (A). These types of drives are found in fans and coolant pumps, for example. The compact motor starters are installed in control cabinets and are designed to start single and three-phase motors of machines and systems, protecting them against overloads and short-circuits. They are each available in standard and safety variants.
At "SPS – Smart Production Solutions" 2019, Siemens will present sector-specific applications and future technologies for the digital transformation of the discrete and process industries. At the heart of the 4000 square meter booth will be new products, solutions and services from the Digital Enterprise portfolio, which can be used to merge the real and virtual world.
On November 26, the first day of SPS, Klaus Helmrich spoke at the Siemens press conference, which took place in the trade show Convention Center. Mr Helmrich discussed the latest trends in digitalization and the next stage of digital transformation in the discrete and process industries.
- Exact recording of energy consumption and electrical parameters
- Secure data transfer over existing communication networks
- Flexible use in industrial and commercial buildings as well as data centers
Siemens Smart Infrastructure has added the 7KM PAC3220 and 7KM PAC3120 measuring devices to its Sentron power monitoring portfolio. These devices capture energy and system data from buildings, infrastructure and industrial facilities and transfer them via standard communication protocols to higher-level energy management, automation and IoT systems. This data can then be used to identify energy hogs, detect system malfunctions as early as possible and proactively prevent downtimes. This allows companies to sustainably boost their energy efficiency and system availability. The new devices offer higher accuracy than the previous models and have a new design.
- Railsystems RP GmbH orders two locomotives from Siemens Mobility
- Sustainable concept: a combined diesel and electric locomotive
- Delivery at the end of 2020
Railsystems RP GmbH has ordered two Vectron Dual Mode locomotives from Siemens Mobility, marking the first order for the new locomotive that can be operated either as a diesel or electric unit. Siemens Mobility first presented the concept at the InnoTrans 2018.
- VAG Nürnberg orders 12 Avenio trams
- Option for up to 75 additional trams
- Innovative interior concept for enhanced passenger comfort
VAG
Verkehrs-Aktiengesellschaft Nürnberg has ordered 12 four-section Avenio trams.
The contract includes options for a total of up to 75 additional trams. The
trams will serve on possible new lines or be used to expand VAG’s existing offering.
Commissioning is planned for the end of 2022.
- Third Mireo order from DB Regio
- Service in the Karlsruhe 7b network
- Passenger comfort and sustainably increased value over entire lifecycle
DB Regio, the regional transport business of Deutsche Bahn AG, has
ordered seven Mireo trains from Siemens Mobility. The trains will operate on
the regional express route between Karlsruhe and Heidelberg/Mannheim via
Bruchsal in the Karlsruhe 7b network. They will be built at the Siemens
Mobility plant in Krefeld, Germany, and their delivery is planned for the end
of 2022.
- New trend to supply renewable energy for mines as secure and cost-efficient alternative to fossil fuels
-
- Siemens' proven microgrid controller serves as technical basis for juwi's Hybrid IQ microgrid solutions
- Two projects in Australia successfully delivered, paving way for partners to roll-out solution in other countries
Siemens and the renewable energy developer juwi have joined forces to enter into a strategic technology partnership to focus on microgrids in the mining industry. A corresponding agreement was signed today. The two companies aim to roll-out and continually develop the advanced microgrid control system that enables the seamless integration of power from renewable energy to a mine's off-grid power supply. The Siemens Sicam based microgrid control platform is a proven and tested technology which is the basis for juwi's Hybrid IQ microgrid controller. juwi, on the other hand, brings industry-specific domain know-how and an excellent track record of planning and executing renewable energy projects at mine sites.