- Enhanced reliability and efficiency through easier energy monitoring without data cables
- Suitable for the transmission of more than double the electricity of comparable systems
- Modular design for flexible planning and cost-effective expansion
At this year’s Light+Building, Siemens Smart Infrastructure is introducing LData, a busbar trunking system specially designed for data centers wanting to improve their efficiency, availability and adaptability. The more internet traffic, mobile users as well as Internet of Things connections increase, the more data has to be processed. That is why high-performance data centers are emerging as the backbone of a digital society. These data centers must offer the highest degree of availability to protect critical data as well as business-critical applications and industrial processes. At the same time, they must be energy efficient as well as easy to plan, install and expand. The energy distribution system plays a major role in this regard.
- New devices for electrical installations in industrial and infrastructure environments with a lower nominal current of 0.1 to 0.4 amperes
- Firmware update with improved control and diagnostic functions
- Failsafe group shutdown function without additional wiring
Siemens Smart Infrastructure is adding four new devices to its portfolio of Simatic ET 200SP motor starters, which can be used to start electric drives with a power output from 0.1 to 0.4 amperes (A). These types of drives are found in fans and coolant pumps, for example. The compact motor starters are installed in control cabinets and are designed to start single and three-phase motors of machines and systems, protecting them against overloads and short-circuits. They are each available in standard and safety variants.
- Safer and more efficient: Catania Airport is updated with integrated building automation by Siemens
- More reliable and accurate fire detection using Sinteso connected to the Desigo CC building management software
- Cloud-based Navigator software to optimize energy consumption
With almost ten million passengers in 2018, Catania Airport is continuing to grow, solidifying its number one position in southern Italy. This makes the hub an increasingly important strategic part of the Mediterranean aviation network. As a result, however, it faces greater security and energy efficiency challenges. This is the context in which the Sicilian airport made the decision to entrust Siemens with its integrated building automation project, intended to increase security levels and monitor overall energy consumption at the hub.
- Spectrum Power ADMS to provide reliable energy supply for 1.5 million people
- One multi-site system to handle all voltage levels
Hafslund Nett, Norway's largest grid company has contracted Siemens to supply a new Advanced Distribution Management System (ADMS) for the operation of the regional power grid in Akershus, Oslo and Østfold. The fully integrated grid operating center will enable monitoring and control of the complete power grid covering all (high-, medium-, low-) voltage levels. At the same time, it will allow easy integration of third-party IT/OT systems, such as customer information systems, workforce management or geographical information systems. The project is expected to be operational at the beginning of 2022.
Siemens has received an order from the regional grid operator EWE Netz GmbH to supply the key components of a Siharbor shore power supply system in Cuxhaven. The order includes the complete transformer station as well as the cable feed system for ro-ro (roll-on/roll-off) ships. The plant owner will be the northern German Gesellschaft für Hafeninfrastruktur Niedersachsen Ports (NPorts). With a power output of 630 kilowatts (kW), the plant will supply these ships with electricity during their lay time. They will thus be able to turn off their diesel generators, significantly lowering exhaust gas and noise pollution. The berth is located next to the new factory for wind turbines operated by Siemens Gamesa, which will be the plant's main user in the future. Siemens Gamesa will ship wind turbine components to its sister factory in Hull, UK. The Siharbor system is expected to go into operation by April 2018.
- Siemens provides sustainable heating, cooling and ventilation solutions and thus, supports partners and customers in the decarbonization of buildings
- One of the highlights will include an energy efficient magnetic expansion valve, with which OEMs can gain up to 21% more heating capacity
- Also being showcased is a heat pump automation system as part of Siemens Xcelerator
At this year's Mostra Convegno Expocomfort (MCE) trade show, Siemens Smart Infrastructure will present a broad range of innovative and sustainable products, systems, and solutions for Original Equipment Manufacturers (OEM) and installers to accelerate the decarbonization of real-estate. The global marketplace and event, that takes place from March 12 to 15 in Milan, Italy, brings together companies and industry experts from the heating, ventilation, air conditioning and refrigeration (HVACR), renewable energy sources and energy efficiency fields.
- Siemens has supplied 200 VersiCharge wallboxes and an intelligent charging management system to the Portuguese Infinity building
- The contract includes SICAM Dynamic Load Management, a solution to use grid capacity in an efficient way
- Hardware and software are part of Siemens Xcelerator, an open digital business platform that enables customers to accelerate their digital transformation
Siemens Smart Infrastructure has supplied and installed 200 VersiCharge wallboxes and an intelligent charging management
system to the Infinity building, one of the tallest residential sites in
Lisbon, Portugal.
- Siemens exhibition at ISH 2023 introduces IoT-based smart building solutions which marks a major shift for sustainable operations
- Addressing simple small buildings as well as complex campuses
ISH 2023, Frankfurt a. M. (Germany),
March 13 – 17, hall 10.2, booth C55
- ETH Zurich runs unique research project on automation and energy supply for buildings in different climate zones
- Project includes one-of-a-kind artificial sun
- Siemens supplies digital building technologies, part of Siemens Xcelerator, for lab
ETH Zurich,
one of the world’s most renowned universities, has just opened a unique
research facility: the Zero Carbon Building Systems (ZCBS) Lab. It allows research
into the behavior of building components and systems in different climate
zones. The new building, located on the university campus in Zurich, comprises
two floors with different test cells, climate chambers, and experimentation
rooms. As part of its existing industrial partnership with ETH Zurich, Siemens
has equipped the new research facility with state-of-the-art digital building technologies,
including for building operations and management. The technologies are part of
the Siemens Xcelerator portfolio.
- Samotics joins Siemens Xcelerator partner ecosystem with its leading monitoring system for AC motors and rotating equipment based on electrical signature analysis (ESA) technology
- ESA technology has been integrated into NXpower Monitor, delivering asset health and energy efficiency insights for electric-driven equipment
- ESA will extend NXpower Monitor’s capabilities to deliver an end-to-end asset monitoring offering for the entire energy distribution system
Siemens Smart
Infrastructure has integrated electrical signature analysis (ESA) from Samotics
into NXpower Monitor, its industry-leading digital caretaker for electrical
networks. Using ESA and machine learning, Samotics provides real-time
actionable insights to help global industrial companies eliminate industrial
energy waste and unplanned downtime. This new capability leverages the
ecosystem of Siemens Xcelerator, an open digital business platform that enables
customers to accelerate their digital transformation easier, faster, and at
scale.