- Reliable protection with minimal space requirements
- For power distribution and industrial plants
Siemens Smart Infrastructure presents the new Siprotec 5 Compact device, specially designed to address the demands of industrial applications, infrastructure and distribution grids. With its compact size, large number of inputs and outputs, and universal range of functions, it can be configured to meet the specific requirements associated with protecting feeders and motors. As a space-saving universal device, it is ideally suited to help optimize investment and operating costs in power distribution.
- New Grid Diagnostic Suite offers unique comprehensive insights
- Gain a grid-wide view of energy automation systems
- Market launch of initially four cloud-enabled applications
- Enhances cost efficiency and availability of smart grids
- Support through digitalization in increasingly complex power grids
Siemens is presenting for the first time its new Grid Diagnostic Suite at the European Utility Week in Paris. The Grid Diagnostic Suite initially includes four cloud-based applications which collect data from new or existing field devices for protection, distribution automation and power quality. These data are stored and analyzed in the cloud. This requires almost no additional engineering effort. Distribution grid operators and operators of electricity grids in industrial parks can quickly tap into useful information from devices installed anywhere in the smart grid. This will enable grid faults, for example, to be detected at an early stage and quickly rectified. After information is collected, vulnerabilities can be identified, and necessary measures can be implemented before any damage occurs. In this way, Internet of Things (IoT) applications in the Grid Diagnostic Suite enhance the availability of power grids while enabling them to be operated cost-efficiently.
- System based on Siemens Spectrum Power supports second-by-second control of all assets and integration of RWE wind and solar farms
- Improved combination of electricity generation from renewables and conventional fuel is a major milestone for the energy transition
RWE is making its power station control system fit for the future by adopting a new technology. Optime, a new SCADA system based on Siemens Spectrum Power, gives RWE a uniform control technology. SCADA stands for 'Supervisory Control and Data Acquisition' – in other words monitoring and managing technical processes using a computer system. Previously, there were two separate systems: one for power plants in Germany and another for the Netherlands and Belgium. The new solution combines the two, while integrating RWE’s renewable energy assets in Europe. It can also accommodate additional units such as battery storage systems and diesel-powered backup generators.
- Siemens drives forward digital transformation in the machine tool industry with a brand new Sinumerik generation
- Sinumerik ONE enables seamless interaction between virtual and real world for significantly increased productivity in the production and use of machine tools
- Scalable CNC-portfolio for highest performance requirements and optimum surface quality
With Sinumerik ONE, the first digital native CNC, Siemens is driving forward digital transformation in the machine tool industry. The new controller works with software to create the machine controller and associated digital twin from one engineering system and thus contributes to the seamless integration of hardware and software. Thanks to its seamless interaction between virtual and real world as well as high-performance hardware, Sinumerik ONE is setting new standards in terms of productivity, performance and digitalization. It is the future-proof CNC for machine tools in the increasingly digital world of manufacturing. Both machine manufacturers and machine operators benefit from the universal digital twin for the product, production and performance.
- Portfolio serving entire power range from 50 to 600 kW
- Flexible combination with connection options as cable and pantographs
- For fast and secure charging at the depot and en route
- Cloud-based control and monitoring of charging processes
At Busworld 2019, Siemens is presenting its Sicharge UC family for charging electric buses, trucks and duty vehicles at the depot and en route. The Sicharge UC charging system covers the entire power range from 50 to 600 kilowatts (kW) and can be combined with several connection options such as charging plugs and offboard or onboard pantographs. To meet growing demands from the vehicle industry for higher voltages, the station can operate at up to 1,000 volts (V). Electric vehicles with various technologies and batteries can therefore be charged flexibly, either en route or at the depot. The charging processes can be monitored and controlled via a MindSphere application. MindSphere is the cloud-based, open IoT operating system from Siemens.
- Managing Board members’ individual
responsibility to have greater weight
- In addition to capital market
performance, sustainability targets included for first time
- Contractual maximum compensation
agreed
- New compensation system makes
Siemens a pioneer among DAX companies
Siemens intends
to adjust the compensation system for its Managing Board members in order to
align the system more closely with the company’s sustainable development and
thus with the Vision 2020+ company strategy. By implementing the new system, Siemens
is taking on a pioneering role because the new approach already reflects the
draft version of the German Corporate Governance Code of May 9, 2019, and the
draft version of the act transposing the European Union’s Second Shareholder
Rights Directive into German law. In addition, the new concept not only
considers performance on the capital market, but also places emphasis on
targets for environmental protection, professional development of employees and
customer satisfaction. In the future, the broad-based MSCI World Industrials
Index – instead of a comparison with five main competitors – will be the yardstick
for the comparisons that determine the value of the stock awards. The new Managing
Board compensation system, which already applies as of fiscal 2020, will be
submitted to shareholders for endorsement at the Annual Shareholders’ Meeting on
February 5, 2020.
- Enhanced reliability and efficiency through easier energy monitoring without data cables
- Suitable for the transmission of more than double the electricity of comparable systems
- Modular design for flexible planning and cost-effective expansion
At this year’s Light+Building, Siemens Smart Infrastructure is introducing LData, a busbar trunking system specially designed for data centers wanting to improve their efficiency, availability and adaptability. The more internet traffic, mobile users as well as Internet of Things connections increase, the more data has to be processed. That is why high-performance data centers are emerging as the backbone of a digital society. These data centers must offer the highest degree of availability to protect critical data as well as business-critical applications and industrial processes. At the same time, they must be energy efficient as well as easy to plan, install and expand. The energy distribution system plays a major role in this regard.
- AnalyzeMyWorkpiece /Monitor enables continuous monitoring of workpiece production
- Quality control takes place immediately during production
- New application extends the range of existing applications for quality assurance
With AnalyzeMyWorkpiece /Monitor, Siemens is extending its software portfolio for machine tools for workpiece quality. The Edge application based on high-frequency data, which will be presented at EMO 2019, enables continuous monitoring of workpiece production in machine tools. Measured values such as position data, torque values or control deviations together with context information, for example the tool currently being used, are acquired from the machine with high frequency and without feedback via Sinumerik Edge. The measured values are compared continuously with a reference model. In the event of deviations that exceed a predefined level, the application logs the result, sends it to the machine tool and enables prompt responses by the operator. This means, for example, that unique process-parallel quality control is supported during production.
- New devices for electrical installations in industrial and infrastructure environments with a lower nominal current of 0.1 to 0.4 amperes
- Firmware update with improved control and diagnostic functions
- Failsafe group shutdown function without additional wiring
Siemens Smart Infrastructure is adding four new devices to its portfolio of Simatic ET 200SP motor starters, which can be used to start electric drives with a power output from 0.1 to 0.4 amperes (A). These types of drives are found in fans and coolant pumps, for example. The compact motor starters are installed in control cabinets and are designed to start single and three-phase motors of machines and systems, protecting them against overloads and short-circuits. They are each available in standard and safety variants.
- Safer and more efficient: Catania Airport is updated with integrated building automation by Siemens
- More reliable and accurate fire detection using Sinteso connected to the Desigo CC building management software
- Cloud-based Navigator software to optimize energy consumption
With almost ten million passengers in 2018, Catania Airport is continuing to grow, solidifying its number one position in southern Italy. This makes the hub an increasingly important strategic part of the Mediterranean aviation network. As a result, however, it faces greater security and energy efficiency challenges. This is the context in which the Sicilian airport made the decision to entrust Siemens with its integrated building automation project, intended to increase security levels and monitor overall energy consumption at the hub.