For Dutch tram operator HTM, today marks the start of passenger services with brand new Siemens trams in The Hague, Netherlands. The first Avenio will run on line 2, which connects the western suburb of Kraayenstein with Leidschendam in the northeast via The Hague's main station. The Siemens trams will also gradually progress to operating on lines 1, 9, 15 and 17, with test runs already being conducted on the next route earmarked for Avenio, line 11. HTM has ordered a total of 60 Avenio trams from Siemens.
- Further ten Vectron AC and eleven Vectron MS
- Three locomotives have just been delivered
- MRCE owns 56 Vectron locomotives
The locomotive leasing and service company Mitsui Rail Capital Europe B.V. (MRCE) has ordered 21 additional Vectron locomotives from Siemens. Ten of these locomotives are of the AC version for operation in Germany and Austria. The other eleven locomotives are equipped as multi-system locomotives and will be operated in Germany, Austria and Italy. All Vectron locomotives will be manufactured in the Munich-Allach locomotive production plant. The first three locomotives were pre-produced and have already been handed over to MRCE by Siemens. With this new order MRCE will now own a fleet of 56 Vectron locomotives.
- Class 700 Desiro City train arrived at newly constructed depot
- Set to transform passenger experience on Thameslink rail routes
- Start of passenger service planned in Spring 2016
Today, the first brand new Siemens-built Class 700 Desiro City train arrived in the United Kingdom (UK). The trains are set to transform passenger experience on the Thameslink rail routes when it rolls into action next year. Designed to provide much-needed extra capacity on the South-East’s busy commuter routes, the train arrived at the newly constructed Three Bridges traincare facility near Crawley, West Sussex.
- New bus route now in service
- eBus high power charging system from Siemens
- Powered by 100 % renewable electricity
The new electric bus route 55 between Lindholmen and Johanneberg in Gothenburg, Sweden, is now inaugurated. This nine-kilometer-route will be served by three all-electric buses and seven electric-hybrids, all from Volvo Buses. The vehicles are equipped with battery packs that will be charged with renewable electricity. Siemens, together with the communal energy supplier Göteborg Energi, has installed two high power charging stations, one at each end of the route, and supplied the complete charging system.
- 15 Vectron MS locomotives
- To operate on the D-A-CH-I-NL corridor
- Top speed of 200 km/h
The Swiss rail cargo specialist BLS Cargo has ordered 15 Vectron MS multisystem locomotives from Siemens that will be used in cross-border service in Germany (D), Austria (A), Switzerland (CH), Italy (I) and the Netherlands (NL). All traction and train control systems required for the north-south freight corridor are on board. The locomotive can reach speeds up to 200 km/h and has an output of 6,400 kW. Delivery will take place in three phases, and the first locomotives are scheduled to enter service in the second half of 2016.
- Complete electrified bus systems for cities
- First buses running in Hamburg, Germany, since December 2014
- In 2015, the cities of Gothenburg and Stockholm, Sweden, will follow
Volvo Buses and Siemens have signed a global agreement regarding supply of complete electrified bus systems to cities. Under the agreement, Volvo Buses will supply electric-hybrid buses and full-electric buses to customers, and Siemens will supply and install high-power charging stations (charging capacity of up to 300 kW) for the electric vehicles.