World Forum and Leading Show for the Process IndustriesUnder the motto "Accelerate the digital transformation – from integrated engineering to integrated operations." we presented at the Achema 2018 trade show specific applications for how to use the potential of digitalization to enhance efficiency, flexibility, and quality – and to shorten time to market. Production can be significantly optimized and made more flexible by integrating all components in instrumentation and control and management systems and by intelligently using all of the process data generated in a common data model – the digital twin of the overall plant. Maintenance effort and costs can also be slashed dramatically by using cloud-based applications and data-based services.
On the first day of the Hannover Messe, April 1, Klaus Helmrich welcomed you to the annual Siemens Press Conference. As member of the Managing Board of Siemens AG, Klaus Helmrich is responsible for the Digital Industries Operating Company. The Press Conference took place at 6:30 PM in the Trade Fair's Convention Center, Room 1 A/B.Mr. Helmrich talked about the latest developments of digitalization and the next step towards the digital transformation in the manufacturing and process industries under the theme "Digital Enterprise – Thinking industry further!".
- New MindSphere Version 3.0 on Amazon Web Services (AWS) provides access to Siemens APIs and AWS cloud services for faster development
- Simotics IQ: New IoT concept for motors
- New partnership financing service to boost the implementation of Industrie 4.0
- Study affirms annual productivity increase due to digitalization of up to 9.8 percent
Increasing demands by consumers for individual, high-quality products at favorable prices are posing new challenges for industrial enterprises which can only be resolved by digitalization. "With the Digital Enterprise portfolio, the technical conditions have been created for Industrie 4.0. To ensure successful implementation of Industrie 4.0, what we now need is an extended model for cooperative partnership based on mutual respect: Large-scale corporations supply platforms and components, medium-sized enterprises develop their own solutions and business models on this basis, and end customers integrate these into their digital value chain," explained Klaus Helmrich, Member of the Managing Board of Siemens AG at the SPS IPC Drives. Siemens will be showcasing a range of innovations at the show designed to shorten the time to market and to improve flexibility, efficiency and quality in the process and manufacturing industries. They range from the new Version 15 of the Engineering Framework TIA Portal through the IoT concept for motors Simotics IQ to the new Version 3.0 of the open cloud-based IoT operating system MindSphere. Siemens is also offering financing services such as pay-per-use models designed to simplify the implementation of digital solutions, aimed in particular at medium-sized enterprises.
- Firmware 4.8 enables Sinamics S120 converters to operate with synchronous reluctance motors
- System operation with or without position sensor using new Sinamics reluctance control license
- Durable in any operating environment due to field-oriented vector control
- High energy efficiency even at low speeds
Firmware version 4.8 allows Simotics synchronous reluctance motors to also be operated with Sinamics S120 converters, enabling them to benefit from the complex functionalities of the modular S120 product portfolio. The new Sinamics reluctance control license used in combination with the Sinamics Booksize Modules means that precise drive control down to a complete standstill is now possible with and without a position sensor. This applies both for motor and generator operation. Field-oriented vector control across the whole of the operating range makes for a tangibly more robust drive system. Unlike U/f-based methods, for instance, any possibility of motor stalling in the event of load jumps is excluded. Sensorless control also enhances the energy efficiency of the drive, as even in the low speed range it allows the achievement of low values normally only possible using a sensor.
- New drive system comprising Sinamics S210 and Simotics S-1FK2 motors
- High dynamic performance and precision plus simple One Cable Connection (OCC)
- Integrated safety functions, rapid engineering and commissioning
- Servo drive system in five power classes from 50 to 750 watts
With its Sinamics S210 converter designed specifically for use with the newly developed Simotics S-1FK2 motors, Siemens is offering a new servo drive system in five power classes ranging from 50 to 750 watts. The converters come with integrated safety functions and enable rapid engineering. They are connected to the higher-level controller over Profinet and allow simple commissioning using a web server and one-button tuning. Working in combination with the Simotics servo motors, they enable the highly dynamic movement of minimal loads as well as ultra-precise movement of medium and high loads. The motors are connected to the converters using a One Cable Connection (OCC). Typical uses for the new drive system include in particular packaging machines, handling applications such as Pick & Place, wood and ceramic processing as well as digital printing.
On the first day of the Hannover Messe, April 24, Klaus Helmrich welcomed you to the annual Siemens Press Conference. As member of the Managing Board of Siemens AG, Klaus Helmrich is responsible for the Digital Factory as well as Process Industries and Drives Divisions. The Press Conference took place at 6:30 PM in the Trade Fair's Convention Center, Room 1 A/B. Mr Helmrich talked about current digitalization trends in the manufacturing and process industries under the heading "Discover the value of the Digital Enterprise".
Digitalization is changing our world – and the world of industry – in tangible ways. The digital transformation is creating new competitive advantages and business models in many companies in the manufacturing and process industry. Machine builders and plant engineers can also take advantage of this development and make it usable for their customers. For digital enterprises systems and processes can be comprehensively and uniformly optimized throughout the entire lifecycle of products and plants. At the SPS IPC Drives in Nuremberg, Germany, from November 28 to 30, 2017 – which took place this year under the motto "Discover the value of the Digital Enterprise" – Siemens presented in hall 11 specific examples of applications to show how this can be done.
- Siemens demonstrates consistency of the digital twin using Easysnap application at the SPS IPC Drives 2017
- "Digital Enterprise Suite" features tools for creation of the digital twin
- Apps facilitate the use of plant data collected in MindSphere
At the SPS IPC Drives 2017, Siemens will be demonstrating the consistency of the digital twin over the entire machine life cycle using the example of a packaging machine manufactured by machine builder Easysnap. To achieve this degree of consistency, all the engineering tools required for design, configuration and commissioning interact seamlessly with each other to enable truly integrated engineering. Siemens supplies a comprehensive range of different tools embedded in its "Digital Enterprise Suite" solution portfolio which are designed to enable the creation of a digital twin and so bring about substantial improvements along the value chain. The digital twin can be created using tools such as the Mechatronics Concept Designer, which enables kinematic simulations, and the Sizer configuration tool which uses this data as the basis for determining the required electrical drive values and relevant products.
- New frame size FSAC for Sinamics V20 converter portfolio
- V20 frame size now 40% smaller than predecessor model
- Integrated radio interference suppression filter in V20 enables use in public networks
- Sinamics V90 frame size FSA now available as Profinet version with 200 V line voltage
- V90 with 18% smaller footprint and real-time transmission of process and diagnostic data
Siemens is extending its Sinamics frequency converter portfolio for standard applications Sinamics V20 to include a new frame size, the FSAC in the voltage range 1AC (Alternating Current) 200 V to 240 V 1.1 kW to 1.5 kW. FSAC is replacing the previous FSB frame (1AC 200V). 40% more compact than its predecessor, the new frame size offers even more flexible and exceptionally space-saving application possibilities.
- Sidrive IQ – the digital platform for drive systems across the entire life cycle
- Platform based on networked drive systems from Siemens
- Added productivity, reliability and serviceability value
- Predefined service packages to address specific customer needs
With Sidrive IQ, Siemens is offering a new digital platform for the evaluation and utilization of drive data based on MindSphere, the cloud-based open IoT operating system in use across wide-ranging industries. Users of networked drive systems are afforded direct access to new functionalities designed to support industrial production and maintenance tasks. The result: increased productivity, reliability and serviceability for complete drive systems over their entire life cycle. Sidrive IQ can be used to support an array of applications in different industries.