- Using proven hardware and software, Siemens develops a solution for social distancing at the workplace
- Companies can simulate and manage the possible risks to their employees while at the same time increasing the productivity of their plants
- Simatic Real-time Locating Systems (RTLS) plus SieTrace software provide location information which customers can use to control their manufacturing processes and to design their operating procedures future-proof
Siemens uses a combination of hardware and software to offer a new solution for the challenges that companies face as a result of the Covid-19 pandemic. The solution enables companies to quickly and efficiently control how employees interact with one another, with the production line and with the plant setup. The integrated digital twin helps the company to simulate the safety of employees, to test and optimize the setup of work areas, to validate safety measures, and thus to design future-proof production lines.
- Enhanced reliability and efficiency through easier energy monitoring without data cables
- Suitable for the transmission of more than double the electricity of comparable systems
- Modular design for flexible planning and cost-effective expansion
At this year’s Light+Building, Siemens Smart Infrastructure is introducing LData, a busbar trunking system specially designed for data centers wanting to improve their efficiency, availability and adaptability. The more internet traffic, mobile users as well as Internet of Things connections increase, the more data has to be processed. That is why high-performance data centers are emerging as the backbone of a digital society. These data centers must offer the highest degree of availability to protect critical data as well as business-critical applications and industrial processes. At the same time, they must be energy efficient as well as easy to plan, install and expand. The energy distribution system plays a major role in this regard.
- New version 8.0 facilitates integration of Simatic S7-1500 controller as well as mixed operation with Simatic S7-400 controller operation with the Simatic S7-400 controller
- Improved production and batch transparency with new MES reporting options
- Enhanced safety concept with new functions
- Lean Edition for micro breweries and craft brewers
Siemens is presenting a new version of the Braumat brewery process control system at the BrauBeviale in Nuremberg: The latest version 8.0 is based on the Simatic S7-1500 controller and has been optimized in the areas of reporting, weighing systems and security. Already installed Simatic S7-400 controllers can still be used, including in mixed operation. Existing Braumat installations can be expanded or modernized with Simatic S7-1500 controller. Production downtimes caused by new installations are thus avoided.
- AnalyzeMyWorkpiece /Monitor enables continuous monitoring of workpiece production
- Quality control takes place immediately during production
- New application extends the range of existing applications for quality assurance
With AnalyzeMyWorkpiece /Monitor, Siemens is extending its software portfolio for machine tools for workpiece quality. The Edge application based on high-frequency data, which will be presented at EMO 2019, enables continuous monitoring of workpiece production in machine tools. Measured values such as position data, torque values or control deviations together with context information, for example the tool currently being used, are acquired from the machine with high frequency and without feedback via Sinumerik Edge. The measured values are compared continuously with a reference model. In the event of deviations that exceed a predefined level, the application logs the result, sends it to the machine tool and enables prompt responses by the operator. This means, for example, that unique process-parallel quality control is supported during production.
- First-of-its-kind drilling rig project will implement customized BlueDrive™ system to replace obsolete system
- New system will use existing footprint, cabling and communication points for greater safety and quick commissioning
Siemens was awarded a contract by Arabian Drilling Company to modernize a complete and integrated drilling-drives lineup, including auxiliaries and controls, that will be installed on an offshore jackup drilling rig for a customer in the Middle East. In addition to new features and benefits, the upgrade will also enable the customer to meet the latest safety standards. Delivery of the new system is planned for the early part of 2021.
- New LRV’s will operate on Mid-Coast Trolley
Extension
- Completes the system’s transition to a fully
low-floor fleet
San Diego's Metropolitan Transit System (MTS) has awarded Siemens Mobility a contract for 25 S700 Low-floor Light Rail Vehicles. These cars will operate the entire 53-mile double-tracked MTS light rail network, including on the 11-mile Mid-Coast Trolley extension, which is scheduled to open in 2021. It will extend San Diego's current Blue Line from the heart of downtown north to University of California San Diego and University Town Center. They will replace Siemens Mobility's high-floor SD100 LRVs which were manufactured in the 1990s. This purchase and subsequent purchases will make San Diego's fleet fully low-floor and accessible. Delivery of the new LRVs is expected in 2021.
- At AMB, Siemens will be demonstrating new applications for Sinumerik Integrate
- Illustration of the whole tool cycle with Manage MyResources
- Optimize MyProgramming /NX CAM Editor revolutionizes CAM machine integration
- Consistent digitalization solutions increase efficiency, flexibility and competitiveness
Siemens is presenting two new applications for the open digitalization platform Sinumerik Integrate under the banner "Digitalization in Machine Tool Manufacturing – Implement now!" at AMB 2018. Using the Manage MyResources application, the complete tool cycle can be displayed for use in the CAD/CAM CNC chain. This provides the customer with a range of benefits including increased tool life. When combined with Manage MyResources, the user gains direct access to a set of NX CAM parameters using the second new application, Optimize MyProgramming /NX CAM Editor on Sinumerik, and can easily optimize and modify the NC programs generated there. The two new applications contribute to the highest possible level of tool availability and therefore to avoiding machine down time. Consistent digitalization solutions such as Sinumerik Integrate allow businesses in the machine tool industry to increase flexibility and production efficiency significantly, to reduce their development and launch times considerably, and thus to improve their competitiveness on the global market.
- New devices for electrical installations in industrial and infrastructure environments with a lower nominal current of 0.1 to 0.4 amperes
- Firmware update with improved control and diagnostic functions
- Failsafe group shutdown function without additional wiring
Siemens Smart Infrastructure is adding four new devices to its portfolio of Simatic ET 200SP motor starters, which can be used to start electric drives with a power output from 0.1 to 0.4 amperes (A). These types of drives are found in fans and coolant pumps, for example. The compact motor starters are installed in control cabinets and are designed to start single and three-phase motors of machines and systems, protecting them against overloads and short-circuits. They are each available in standard and safety variants.
- New version SW 4.8 SP3 release for Sinumerik 828Dand Display Manager for Sinumerik 840D sI
- External PC remote control for 828D enables operation via external PC with Sinumerik Operate
- 828D operation simplified by multi-touch display and side screen
- Second control channel and Collision Avoidance Eco simplify handling
- New Display Manager for 840D sI enables integration of standard and machine-specific functions into user interfaces
Siemens has updated its proven Sinumerik 828D and 840D sI machine tool controls. For 828D, a software update SW 4.8 SP3 with Panel Processing Unit (PPU) 4 has now been released. Users benefit not only from exceptionally robust hardware but also improved connectivity through the ability to access central data and programs, increasing operating safety. Another feature of the update is an external PC remote control facility for the simplified connection of other authorized PCs via Virtual Private Computing (VPC). In addition, the application for MindSphere ManageMyMachines now enables connection of Sinumerik 828D controls to the cloud based open IotT operating system MindSphere. For exceptionally simple operation, Siemens offers Smart Operation, a robust multi-touch display used in conjunction with a side screen. The CNC Sinumerik 828D now also offers a second control channel for use during milling operations, making available additional integration and control possibilities for automation systems or handling robots. Another invaluable feature is the Collision Avoidance Eco, which works on the basis of protected areas and distances which can be configured by the user. There is also a new update designed to make life more convenient for users of the Sinumerik 840D sl. The new Sinumerik Operate Display Manager allows the operator to fully leverage the possibilities offered by larger widescreen monitors, as both standard and machine-specific functions can be integrated into the user interface. These innovations allow rapid and comprehensive access to all the relevant data and allow more efficient, simpler machine control, as well as speeding up and simplifying process workflows. This saves both time and costs throughout the entire milling process.
- Safer and more efficient: Catania Airport is updated with integrated building automation by Siemens
- More reliable and accurate fire detection using Sinteso connected to the Desigo CC building management software
- Cloud-based Navigator software to optimize energy consumption
With almost ten million passengers in 2018, Catania Airport is continuing to grow, solidifying its number one position in southern Italy. This makes the hub an increasingly important strategic part of the Mediterranean aviation network. As a result, however, it faces greater security and energy efficiency challenges. This is the context in which the Sicilian airport made the decision to entrust Siemens with its integrated building automation project, intended to increase security levels and monitor overall energy consumption at the hub.