- Siemens Mobility and VTG Rail Europe collaborate to innovate rail freight transport
- Contract covers a one-year trial to prove the system’s operational capability
- Brake Monitoring System has European-wide market potential due to time and cost savings for rail-bound freight transport
Siemens Mobility GmbH and VTG Rail Europe GmbH signed a contract to test the innovative Brake Monitoring System (BMS) for automated brake testing of freight trains to prove the system’s operational capability. The BMS ensures an automatic brake test on each wagon of a train. The expected efficiencies generated for freight operators will result in a great market potential across Europe.
- Support reliable power supply for 965,000 citizens in Stockholm area
Ellevio, Sweden’s second largest grid company, has contracted Siemens Smart Infrastructure to deliver a new grid control system for its distribution network. The new grid control system based on Spectrum Power 7 will improve handling of increased network complexities, abnormalities, and security threats, whilst enabling improved ease and use for operators. Ellevio's control center in Karlstad is responsible for providing a reliable energy supply for 965,000 citizens in Sweden. The grid control is set up in a flexible multi-site operation with a main control center in Karlstad and a supporting control center in Stockholm for back-up.
- 2-loop fire control panel connects up to 252 devices
- EN 54-23 compliant alarm devices and dedicated peripherals
- Time-saving tools such as auto configuration and on-board web server
- License free programming
With the launch of the new version of the fire protection system, Cerberus FIT, Siemens Smart Infrastructure expands its offering for the small to medium-sized buildings market. Various small to medium-sized buildings can now be covered with a simple and cost-efficient solution. Cerberus FIT maximizes fire safety, thanks to greater functionality and enhanced productivity for those working on protecting the buildings. The intuitive interface as well as the auto configuration tool allow the technician to install, commission and maintain the system in a fast, easy and reliable way. With the delayed alarm function staff will be informed first to identify what an alarm is about in order to assess the situation. This ensures business continuity and reduces disturbances to occupants of smaller buildings such as small-to-medium sized hotels, kindergartens or nursing homes.
- Shorter development and commissioning times
- Software libraries enable standardization
- Commissioning tests on virtual test rack
The new Sinumerik One CNC generation is at the heart of digital transformation for machine tools. As a digital native, the controller features not only a new hardware platform, but also versatile software for the creation of a digital twin. It closes the gap between the virtual and the real world and helps to reduce development and commissioning times considerably.
- 660 km of modern, safe, and integrated rail system to link the Red and Mediterranean Sea for people and goods
- First
ever high-speed and electrified main rail line in Egypt
- Siemens Mobility to provide high-speed and regional trains, locomotives, rail infrastructure and related services
- To complete all aspects of the project the consortium will create more than 15,000 local jobs
- Contract covers the initial 660 km out of the 1800 km rail network planned
Siemens Mobility is honored to announce that it has signed a contract with the National Authority for Tunnels (NAT), in witness of the Egyptian Prime Minister and Minister of Transport, as well as the German Ambassador in Egypt to deliver a comprehensive rail system that will feature the first ever high-speed, electrified main and freight rail line that will transform transportation in the Arab Republic of Egypt. Together with partners Orascom Construction S.A.E. and The Arab Contractors, Siemens Mobility will provide its comprehensive turnkey services to design, install, commission, and maintain the systems for 15 years. The total contract value is approximately USD 4.5 billion, of which Siemens Mobility’s share is around USD 3 billion. The vast majority of the order intake is expected to be booked in 2022 after financial closing. It is the first contract to be signed from the MoU agreed upon between NAT and Siemens Mobility, Orascom Construction and The Arab Contractors in January 2021.The
contract signed today covers the initial 660 km out of the 1800 km rail network
planned. Additionally, it was agreed to discuss and finalize
the agreements on the two other high-speed railway lines including rail
infrastructure and trains, and maintenance in the coming months.
- Continuous monitoring of energy consumption in the terminal building and at the shore power connecting points
- IoT data platform enables data storage in MindSphere and easy remote access
- Systematic energy data management ensures efficient operations
The Port of Kiel commissioned Siemens Smart Infrastructure to implement a cloud-based power monitoring solution for its shore power system. The shore power system, also from Siemens, will cover the electricity demand of all ships at the Ostseekai and Schwedenkai with green power while they are berthed at the Port of Kiel. This saves more than 8,000 tons of CO2 per year. The new power monitoring solution makes it possible to measure the energy consumption in the shore power operations building and at the Ostseekai and Schwedenkai connecting points, and store the data in MindSphere, the cloud-based IoT system from Siemens. The operators have access to all relevant electrical values at any time and from anywhere, allowing them to determine consumption, identify faults, avoid downtimes, and plan maintenance routines better.
- Sinumerik One Dynamics - three technology packages to increase the efficiency of CNC users when programming in the shopfloor and executing CAM-generated CNC programs
- Top Surface and Top Speed Plus for excellent motion control and perfect workpiece surfaces
With the software version NCU-SW 6.14, Siemens is launching three powerful technology packages exclusively for the CNC Sinumerik One. The Sinumerik One Dynamics packages are available in three different packages: One Dynamics Operate, One Dynamics 3-axis milling and One Dynamics 5-axis milling. The software functions contained in the technology packages support users from machine-oriented programming in the jobshop to high-performance machining of CAD-CAM-programmed workpieces with high surface quality.
- Reliable protection with minimal space requirements
- For power distribution and industrial plants
Siemens Smart Infrastructure presents the new Siprotec 5 Compact device, specially designed to address the demands of industrial applications, infrastructure and distribution grids. With its compact size, large number of inputs and outputs, and universal range of functions, it can be configured to meet the specific requirements associated with protecting feeders and motors. As a space-saving universal device, it is ideally suited to help optimize investment and operating costs in power distribution.
- Improvement of machine tool availability through predictive maintenance with Analyze MyMachine /Condition
- Analyze MyMachine /Condition for Sinumerik Edge creates a mechanical fingerprint of the machine tool
- Condition evaluation, analysis and comparison of all connected machines using the Mindsphere application
Siemens is extending its edge application Analyze MyMachine /Condition with a corresponding Mindsphere application and thus demonstrating how edge computing and cloud computing can be intelligently combined. The Sinumerik Edge Application Analyze MyMachine /Condition, which the company presented last year at the EMO, uses high-frequency CNC data to create the mechanical fingerprint of a machine tool. In the application, users can capture and evaluate various parameters such as stiffness, friction, and backlash in the individual axes with the help of flexibly configurable measurement series. The measurement results can then be visualized and compared with reference data.