- Optimized for operating temperature of -40 to +75 degrees Celsius
- Addressing new and growing cybersecurity challenges
- New cybersecurity partners make their security applications available to Siemens customers
Siemens has expanded the Ruggedcom Multi-Service Platform product family of utility-grade communication devices by introducing a new, more powerful version of the Ruggedcom APE (Application Processing Engine) – an industrial application hosting platform designed for running third party software applications in harsh, mission-critical environments.
-
- Smartron locomotive can now also be ordered for Bulgaria and Romania
- First orders from E-P Rail and PIMK
- Authorization already received for first locomotive in Bulgaria
Siemens Mobility is now also offering its Smartron locomotive in Bulgaria and Romania. The locomotive is available exclusively in a standard preconfigured version, which ensures cost-efficient operation and high reliability for customers. E-P Rail has already ordered four Smartron locomotives for Romania, and PIMK in Bulgaria a total of three. Authorization for placing on the market for the first Smartron in Bulgaria has already been received.
- Agricultural
machinery company to use software solutions from Siemens including product
lifecycle management (PLM) to expand technological leadership
Siemens Digital Industries Software has announced that Maschinenfabrik Bernard
Krone GmbH & Co. KG, a leading agricultural machinery company based
in Germany, has selected the Siemens Digital Innovation Platform to help
establish its digitalization strategy. Using solutions including the Teamcenter
® portfolio and NX™ software, Krone will launch a new
digitalization program that will support processes over the entire product
lifecycle as well as collaborative work between departments by leveraging the
broad, integrated solutions that are part of the Siemens Digital Innovation
Platform.
- Viking Link ensures increased security of supply and integration of renewable energy
- Siemens to deliver both HVDC converter stations
Siemens has been awarded a contract to deliver two converter stations for the first high-voltage direct-current (HVDC) link between Great Britain and Denmark. Viking Link will enable the exchange of electricity up to 1,400 megawatts (MW) to provide increased power-supply reliability and security to consumers in both countries. By allowing transmission to flow in both directions, Viking Link will support the integration of renewable energy sources into the power grid. The interconnector is being jointly developed by National Grid Ventures (Great Britain) and Energinet (Denmark) via National Grid Viking Link Ltd. and Energinet Eltransmission A/S. Viking Link is scheduled to begin commercial operation at the end of 2023.
- 34 six-car Type X metro trainsets, suitable for
fully automatic operation and operation with driver
- Deliveries to begin in mid-2020 with a pre-series
train
- 24-year maintenance contract ensures
sustainable value creation over the entire lifecycle
The first painted car
body for the new Vienna metro was presented today together with the public
transport operator Wiener Linien at the Siemens Mobility plant in the Austrian
capital. The trains are the city's third metro generation supplied by Siemens and
are named "X cars." The first pre-series train is scheduled to be
delivered in mid-2020. A total of 34 six-car trainsets are to be built. Wiener
Linien also secured an option for an additional eleven trains. The trains are
designed for fully automatic operation as well as operation with a driver.
Plans call for them to be used fully automatically on the city's new Line U5,
which is currently under construction, and with drivers on Wiener Linien's
Lines U1 to U4.
- Increased power density and user-friendliness through easy handling
- Plug and play installation and rapid replacement of individual modules
- Increase in redundancy and degradation rates for fuel cell plants
Building on the success of the previous BZM34 and BZM120 fuel cell modules, Siemens aims to optimize the power density and user-friendliness of fuel cell plants on board of air-independent underwater vehicles with its new BZM evo fuel cell module. A single BZM evo has a nominal power of 40 kW. Future plants will be able to provide a maximum power of 320 – 480 kW, depending on the selected type of installation and number of fuel cell modules, without exceeding the footprint of an existing BZM34 or BZM120 plant.
- Siemens Mobility and Bytemark to provide new technology
- Will expand Smart Columbus operating system
- Public sector will manage passenger relationship for trip planning and ticket purchasing
- Enhanced passenger experience
Siemens Mobility announced it will work with Bytemark, a Siemens Mobility partially-owned subsidiary, to provide a common payment solution for Columbus, Ohio's Smart Columbus travel app – the first-ever platform managed by a city, rather than a transportation operator or private party in the United States. The single-payment system that allows for both public and private mobility services to be paid using a single account-based payment system.
- Brownfield Engine Exchange (BEX) delivers cleaner energy, long-term reliability, improved efficiency and more powerful performance
- Making Energy Greener is one of Siemens’ continuing core focus areas as the global energy landscape evolves and changes
- Over 30 engine exchange projects worldwide to date with several recent new orders
Siemens Gas and Power is focused on helping customers navigate the world’s most pressing energy problems, both for today and tomorrow. Essential applications include providing products, solutions and services that make fossil energy greener. A recent example is a project in Alabama where Siemens is has completed its first large gas turbine section exchange in the U.S. - delivering on that commitment. In this way Siemens is helping make energy greener and more sustainable in an evolving energy landscape.
- Contract of Chief Human Resources Officer Janina Kugel to expire by mutual agreement
At its meeting today, the Supervisory Board of Siemens AG
agreed to extend the appointment of Managing Board member Cedrik Neike (46) by
five years. The contract of the CEO of Siemens' Smart Infrastructure Operating
Company (SI) will now run until May 31, 2025. The contract of Chief Human
Resources Officer (CHRO) Janina Kugel (49) will expire by mutual agreement on
January 31, 2020.