- Siemens delivers Airval, its fully Automated People Mover
- Connects terminals at the Suvarnabhumi Airport
- Commissioning in 2020
Interlink Communication Public Company Limited has awarded Siemens to deliver its Airval fully Automated People Mover for the Suvarnabhumi Airport in Bangkok, Thailand. The Airval will connect the current airport terminal with the new satellite terminal. The line will be approximately one kilometer long with four parallel tracks and have two stations. Siemens is to deliver a total of six two-car trains and the Communication Based Train Control system (CBTC) for fully automated operation. The trains will be manufactured at the Siemens plant in Vienna, Austria. The project will be commissioned in 2020.
- Inventors come from Germany, Denmark, Austria and the U.S.
- 34 inventions per day in fiscal 2017
Siemens has honored 14 particularly resourceful researchers as Inventors of the Year 2017. Together, these scientists are responsible for some 1,300 inventions and 920 patents. Nine of the inventors are from Germany, two are from Austria, one is from Denmark and two others are from the United States. Their inventions range from a solution for the digital power grids of tomorrow to technologies that substantially improve medical diagnostics and extend all the way to current collectors that enable all-electric drive for conventional trucks.
Siemens received an award from the American Society of Mechanical Engineers (ASME) for its outstanding technological achievement with the first successfully 3D- printed and fully tested gas turbine blades.
- Pipelines 4.0 is an integrated approach to the engineering, supply and life cycle optimization of pipeline assets
- The solution builds upon Siemens' extensive pipeline experience, product breadth and expertise in rotating equipment, electrification, automation and digitalization
- Key features include equipment and turnkey packages for pipeline stations, as well as data analytics, life cycle service and cyber security
Siemens has launched Pipelines 4.0, an integrated approach to the engineering, supply and life cycle optimization of pipeline assets, tailored to meet the evolving needs of North American operators. The solution combines equipment and turnkey packages for pipeline stations with data analytics, life cycle service and cyber security, building on the company's extensive pipeline experience, product breadth and domain expertise in rotating equipment, electrification, automation and digitalization.
- New power plant projects in Misrata and Tripoli West
- Contracts volume, including long-term service, in the range of 700 million euros
Siemens has signed contracts with the state-owned utility General Electricity Company of Libya (GECOL) to expand Libya’s power generation capacity by approximately 1.3 gigawatts (GW). Under these contracts Siemens will build a 650 MW open cycle power plant in Misrata, equipped with two F-class gas turbines, and a 690 MW open cycle power plant in Tripoli West, equipped with four E class gas turbines. The total volume of EPC contracts, including long-term service agreements, is in the range of 700 million euros.
- Siemens will supply four 400 kV HVDC transformers for cross-channel link
- Efficient 2,000 MW power transmission link between France and the UK will supply up to 3 million homes with electricity
Siemens will deliver four transformers, each with a capacity of 400 kilovolts (kV) and 315 megavolt amperes (MVA), on behalf of the British grid operator National Grid. The grid operator will replace the old transformers in the high-voltage direct-current (HVDC) cross-channel link. The new transformers are quieter, have lower transmission losses and will significantly improve the system's reliability. The HVDC link connects France and England and makes it possible to efficiently exchange energy in both directions. The order includes the supply, installation and commissioning of the transformers for the Sellindge converter station in England. Siemens will complete the work by mid-2019.