- 12-car trains in service on the VDE 8 (German Unity Railway Project Nr. 8)
- Nineteen ICE 4 trains under way daily in Germany as of December 9
- Trains provide substantially more capacity
With the Deutsche Bahn (DB) timetable change on December 9, 2018, the ICE 4 will inaugurate service on the high-speed line between Berlin and Munich. In addition to the ICE 3 trains operating as Sprinters along the route, the ICE 4 will make more stops along the way. Compared to the Sprinter's five intermediate stops, the ICE 4 will make eight. The new trains will connect Berlin-Gesundbrunnen, Berlin Central Station, Berlin-Südkreuz, Lutherstadt Wittenberg, Leipzig, Erfurt, Bamberg, Erlangen, Nürnberg and Munich Central Station. With the launch of ICE 4 service and additional Sprinters, there will be around 3,000 more seats available on this route every day. The new DB flagship also operates on the Cologne-Rhine-Main route, and between Hamburg and Munich, and to Stuttgart. All in all, nineteen 12-car ICE 4 trains will be in service beginning on Sunday.
South-west Germany is counting on Siemens: from 2020 onward, DB Regio AG will be operating its Rhine Valley rail network exclusively with new trains from Siemens. The German Railways order covers 15 Desiro HC and 24 Mireo trains in total, and goes hand in hand with a restructuring of the rail transport services in the Rhine Valley. There is a clear separation between a rapid train system for fast cross-regional services and a regional suburban rail system (S-Bahn) with stops at all stations. The Mireo will be deployed as a regional train (RB) service along the line section from Offenburg via Freiburg to Basel/Neuenburg (Switzerland) as well as in the Kaiserstuhl area on Sundays between Freiburg and Endingen/Breisach. The line section from Karlsruhe via Offenburg and Freiburg to Basel (Switzerland) will be operated with the Desiro HC as a regional express service.
- Siemens Mobility begins extensive test program
- DB Regio to operate the Rhine Valley network as of 2020
- Profitable over the entire lifecycle with enhanced passenger comfort
The first trainset of the new Mireo regional train platform has been completed. In the coming months, a total of eight pre-production trains will be commissioned at the company's Test and Validation Center (PCW) in Wegberg-Wildenrath. Before the train is allowed to operate for the first time in Germany's rail network, an extensive test program must be completed at the PCW. In June 2020, the Mireo is scheduled to begin service in the Rhine Valley network in Southwest Germany that is operated by the DB Regio Regional Business Unit of Deutsche Bahn. DB Regio AG has ordered a total of 24 Mireo trains, the first order Siemens Mobility received for the newly developed platform.
- Trafikverket awards 75 million Euro contract
- Siemens Mobility, with Eltel Networks Infranet, to deliver intelligent infrastructure technology
- Communications, control and monitoring systems for tunneling
The Swedish Transport Administration, Trafikverket, has announced that it awarded Siemens Mobility a 75 million Euro contract to deliver communications, control and monitoring technologies for a section of the European route number four (E4), the Stockholm Bypass. The new bypass will connect the southern and northern parts of the surrounding Stockholm communities. The bypass is a 21-kilometer road, including 18 kilometers of tunneling around one of Europe's busiest capitals. It will relieve intercity and main thoroughfare congestion, significantly reducing delays for residents and visitors. The construction of the tunnel started in 2014 and is expected to be completed in 2026. Installation and testing of Siemens Mobility technologies will begin in 2021.
- VAG Verkehrs-Aktiengesellschaft Nürnberg exercises first option
- A total of 27 metro trains to be delivered
- Greater passenger comfort and optimized passenger flows
VAG Verkehrs-Aktiengesellschaft, Nuremberg's public transport operator, has ordered six additional type G1 metro trains from Siemens Mobility, exercising one of two options in the contract signed in December 2015. All in all, Siemens Mobility will now be supplying 27 new metro trains for Nuremberg. The new four-car G1 trains in the first option are planned for use on the U1 metro line as of 2021 and will replace twelve type DT2 two-car trains.The metro trains will be built at the Siemens Mobility plant in Vienna, Austria. Various vehicle components, such as drive converters, motors, auxiliary converters and control systems, will be manufactured in Nuremberg. Project management, development and service support will be handled in Erlangen.
- 94 metro trains for London based on the Inspiro platform
- Delivery beginning in 2023
- Digital services based on Siemens Mobility's Railigent
- New trains will be more spacious, air-conditioned, have walk-through carriages and improve accessibility
- Additional capacity, maximized throughput and improved passenger experience for millions of passengers
Siemens Mobility has been awarded a major contract in the United Kingdom. London Underground (LUL), a subsidiary of Transport for London (TfL), responsible for the urban rail system in Britain's capital, signed a contract with Siemens Mobility to design and build 94 new generation Tube trains worth around 1.5 billion GBP (1.54 billion Euro) to replace the existing 1970s fleet. The trains will serve the Piccadilly line and delivery will begin in 2023.
- ETCS Baseline 3 train equipment for cross-border operation
- Commissioning approved for 12-car train
- Service on the Berlin – Munich route planned for timetable change in December 2018
Germany's Federal Railway Authority (EBA) has approved the ICE 4 for operation with the European Train Control System (ETCS) in Germany. With this approval, the passenger service can begin as planned on the Berlin – Munich route, which is equipped with the system. The ICE 4 is scheduled to operate on this line when German train operator Deutsche Bahn (DB) changes its timetable on December 9, 2018.
- Awarded Suzhou Metro Line 5 and Nanjing Metro Line 7 fully automated signaling system projects
- Trainguard MT is the state-of-the-art Communications Based Train Control (CBTC) system
Siemens Mobility was recently awarded the fully automated CBTC system for two key Chinese metro lines in Eastern China: Suzhou Metro Line 5 and Nanjing Metro Line 7. The cities, which collectively have more than 12 million residents, are two of the largest cities in the region. China's rapid urbanization in both cities requires fast and intelligent planning of transportation systems that will ease congestion and provide passengers a more reliable and efficient commute. Initial operations for both lines are planned for 2021.
- Research project for an optimized transport system (OTS)
- Mobility offering for the first and last mile
- Testing the interplay of intelligent infrastructure, cloud-based software services and autonomous electric vehicles
Siemens Mobility is launching a field test for autonomous driving at the Siemens campus in Munich-Perlach, Germany. Working with partners IAV GmbH, Institute for Climate Protection, Energy and Mobility (IKEM) e.V., emm Solutions GmbH, UTB Projektmanagement GmbH and the Technical University of Munich (TUM), Siemens Mobility is initiating a research project and field test. The test route runs through the campus and enables traffic simulation in a variety of real-life situations.