- Demonstration running in California near two largest U.S. Ports of Los Angeles and Long Beach
- Siemens truck electrification technology has potential to reduce emissions and improve air quality
Siemens and the "South Coast Air Quality Management District (SCAQMD)" are running a one-mile, zero-emission eHighway demonstration in the Californian city of Carson, U.S., near the ports of Los Angeles and Long Beach. Three trucks hauling freight are running along the stretch of highway which uses Siemens technology to electrify select highway lanes via an overhead catenary system. This catenary system supplies the trucks with electric power, similar to how modern-day trolleys or streetcars are powered on many city streets. The system also allows for truck operation outside of the electrified sections of infrastructure.
Over 100 years ago, on August 5, 1914, the first electric traffic light was installed on a city street in Cleveland, Ohio, marking a milestone in traffic management. Berlin’s Potsdamer Platz (photo), at that time the busiest intersection in Europe, installed the famous five-sided traffic light tower made by Siemens in 1924. Today the red-yellow-green signals are an integral part of city landscapes worldwide. On the outside, traffic lights haven’t changed much over the last decades. But inside a traffic light, groundbreaking changes have taken place. Traffic lights have become more intelligent over the years: modern traffic management takes into account the current traffic situation and optimizes traffic flow, for example, by allowing "green waves" or by prioritizing emergency vehicles, buses, and trams.
More than 100 years ago - on August 5, 1914 - the first electric traffic light went into operation, a milestone for traffic control. Today, it is hard to imagine a world without the redyellow-green signals. And the success story of the traffic lights is continuing with "1-watt technology". This achievement has enabled Siemens to revolutionize the market and improve the energy efficiency of standard 230 V LED technology by up to 85 percent, a huge benefit for tight city budgets and for the environment. Equipped with the new technology, a typical intersection with around 55 traffic signals (red - yellow - green) avoids more than 6,000 kilograms of harmful carbon emissions a year.
Utmost reliability and maximum availability are critically important for ensuring the cost-efficient operation of rail vehicles and the infrastructure they use. After all, malfunctions and downtimes cost money, cause delays and frequently also lead to compensation claims from passengers, local transport purchasers and freight customers. Long before faults actually occur, their potential sources should be identified. To provide this information, Siemens is the first company in the rail industry to operate a special data analytics center, located in Munich, Germany.
Now things are getting down to business: following the initial test phase in the fall of 2016, the Siemens SiBike app is going live in Marburg. In the weeks between now and mid-November, dozens of cyclists will be subjecting this system – which gives priority to bicycles in city traffic – to a stress test that is taking place under realistic conditions. Beginning on October 5, 2017, SiBike is launching on a 700-meter stretch of the Erlenring road in Marburg, Germany. Dozens of volunteer "test pilots" will be helping optimize the "green wave" app. And beginning at the end of November, all Marburg residents will be able to download the SiBike app to their smartphones.
By the way: Marburg is a trendsetter. Since the project's successful start last year, numerous cities in Europe and the U.S. have already expressed interest in this technology.
- 10 Vectron MS and 20 Vectron DC
- Option for 20 additional locomotives
- MRCE fleet includes 111 Vectron locomotives
Mitsui Rail Capital Europe (MRCE), a full-service locomotive leasing company, has ordered 30 Vectron locomotives from Siemens. Ten of the units will be delivered as multisystem Vectron MS for cross-border operations in Germany, Austria, Italy, Switzerland and the Netherlands. Twenty further locomotives will be equipped as direct-current locomotives (Vectron DC) to operate in Italy. Delivery of the locomotives is scheduled to begin from January 2018. The contract with MRCE also includes an option for an additional 20 locomotives.
From 14 to 17 September 2017, representatives from the worlds of politics and industry met at the New Mobility World to shape the future of mobility across industries. The event took place within the context of the IAA 2017. Under the banner "Shaping future mobility systems – from understanding to optimizing," Siemens exhibited at Booth 39 in Hall 3.1 with an array of current applications and solutions surrounding the topics of charging technology for electric vehicles and intelligent communication systems linking vehicles and infrastructure. Siemens offers a wide range of products and solutions that help shape the future of mobility already today.
- First application starting 2020 in 24 DB-Regio Mireo trains
- New transformer type Tractronic® Thinity lighter and more efficient than existing models
- Rugged design allows flexible installation
Siemens will use the new transformer type Tractronic® Thinity for the first time in 24 articulated trains based on the Mireo train platform. The railway transformer is a key component since it feeds the train's power supply and thus guarantees interference-free rail traffic. Thanks to the new design, the transformer is considerably lighter and more efficient than existing models with the same rating. It also offers maximum flexibility for all installation situations with its intelligent construction. Starting 2020, the 24 Mireo trains will operate regional rail services (Regionalbahn RB) on the Offenburg – Freiburg – Basel/Neuchâtel (Switzerland) line, and on Sundays in the Kaiserstuhl from Freiburg to Endingen/Breisach. They will cut travel time for this route by 30 minutes.
- DB Regio orders 57 articulated trains based on the new Mireo platform
- Service in network of Rhine-Neckar S-Bahn
- Staged commissioning beginning in December 2020
DB Regio AG has ordered 57 three-car Mireo trainsets. Following the product's launch in the summer of 2016, this is the second order for Siemens' new regional and commuter train platform. The trains will be built at the company's factory in Krefeld, Germany. Commissioning will follow in two stages: Service on routes in the states of Baden-Württemberg and southern Hesse will begin in December 2020, while service on the Mannheim – Mainz route largely in the state of Rhineland-Palatinate will begin operation in December 2021.