- Contract worth around €340 million
- Maintenance contract for three years
- Velaro fleet will grow to 17 trains
Turkish State Railways (TCDD) has signed a contract for ten Velaro high-speed trains with Siemens, which submitted the most favorable bid in the tender. The contract is worth around €340 million and also includes maintenance, repair and cleaning of the trains for a period of three years. With this contract, the Turkish Velaro fleet will grow to 17 trains.
- High-power charging stations for electric buses
- Elimination of noise pollution and harmful emissions
Siemens signed a frame contract with Movia, the largest public transport authority in Denmark, to deliver charging stations with a top-down pantograph for electric buses on request of their municipalities. The contract is a good example of how corporation between public authorities and private companies can help to improve climate change.
In December 2010, Siemens received an order from Eurostar International Ltd. for ten interoperable 16-car high-speed trains, and the company ordered an additional seven in January 2015. The trains are based on the Velaro, the world's most diverse high-speed platform. Service with the first Eurostar Velaro was inaugurated in November 2015 between London and Paris through the Channel Tunnel. In May 2017, service also began on the route between London and Brussels. And the Velaro has been running between London and Amsterdam via Brussels since April 2018.
The train, designated as the "e320" by Eurostar, provides around 20 more passenger capacity than the previous Eurostar trains. With an overall length of 400 meters, the e320 is the longest member of the Velaro family and has seating for 900 passengers.
All 17 trains are currently in operation and cover a total of around 37,000 kilometers a month in service. Passengers are offered free WLAN access, USB ports and services such as TV streaming and films via an onboard entertainment system. In view of these special amenities, the e320 was named "Train of the Year 2017" by the National Rail Awards in the United Kingdom.
In a consortium with the general infrastructure contractor Per Aarsleff A/S, Siemens has received an order to build a light rail system in Copenhagen, Denmark, from urban transport development company Greater Copenhagen Light Rail I/S. The contract will be implemented as a turnkey project. Commissioning of the system is planned for 2024.
At the Intertraffic 2018, Siemens was showcasing a whole range of pioneering smart solutions, setting the trend for road traffic technology: Among the highlights, Vehicle2x was part of the growing "Internet of Things". Sitraffic ESCoS Road Side Units provides key data for a more precise picture of the current traffic situation. This enables more efficient traffic control, a significant reduction in accident numbers and an even greater cut in emissions than possible up to now. Tunnel management offers road users and tunnel operators a maximum of safety, system reliability and sustainability. The controller Sitraffic sX can adapt optimally to every city, from small and smart, to complex and challenging. Integrated Mobility allows easier and more comfortable travel even across different modes of transportation. Innovative start-up companies from Siemens next 47 had also shown their ideas for future mobility.
- Tram system as turnkey project
- 28 km double track with 29 stations
- 27 four-car Avenio trams
- 15-year maintenance included
In a consortium with the general infrastructure contractor Per Aarsleff A/S, Siemens has received an order to build a light rail system in Copenhagen, Denmark, from urban transport development company Greater Copenhagen Light Rail I/S. The contract includes 27 four-car Avenio trams, rail electrification, signaling, communication, workshop equipment, overall project management and system integration. The contract will be implemented as a turnkey project. The contract also includes maintenance services for 15 years. Commissioning of the system is planned for 2024.
- Award for the Doha Avenio
- Jury convinced by futuristic design
The Siemens Avenio tram for Doha, in the Emirate of Qatar, has been honored with the iF Design Award 2018. Siemens developed the prize-winning design together with the "Yellow Window" design agency. Clean lines, generous white surfaces and darkened windows characterize the tram's exterior. The interior has a bright and airy ambience, while special sun shades on the roof and tinted insulated glass maintain comfortable interior temperatures. Subtly styled seat fabrics and elegantly designed grab poles underscore the tram's modern character and provide a pleasing passenger experience.
Siemens has received an order from the Qatar Foundation for the turnkey construction of a tram system in the capital Doha aimed at transforming Qatar into a knowledge-based society. The order is worth more than 100 million euros. The scope of supply also includes signaling and communication systems, electrification as well as the depot equipment. Siemens will also be equipping four of the stations with platform edge doors. Nineteen Avenio trams will run on 11.5 kilometers of track without any overhead contact lines. The system will be installed on the university campus and serve 25 stations. The trams will be equipped with the Sitras HES energy storage system from Siemens, with energy being supplied at the tram stops.
- Siemens to build 34 fully automated metro trains for Vienna
- New passenger information system for improved travel comfort
- Higher capacity and more flexible use thanks to new interior design
- Contract signed at the end of 2017
Vienna's Environment Councilor Ulli Sima, Wiener Linien GmbH & Co KG, the mass transit operator of Austria's capital, and Siemens today presented the design for the new Vienna metro. The six-car trains, called "X cars," carry on the design elements of the city's existing trains and at the same time fulfill the most modern international safety standards. The trains can be walked through from end to end and feature an open and bright interior. The newly arranged seating layout offers an improved sense of spaciousness, optimizes passenger flows and provides barrier-free access to wheelchair and multiple-purpose spaces. A transparent partition behind the driver's cab offers passengers a new perspective of the metro line.