- Snälltåget
implements Sqills S3 Passenger from Sqills, a subsidiary of Siemens Mobility
- Implementation
to support with longest night train route in the EU
- Increased
capacity, improved passenger experience
Swedish open-access rail operator Snälltåget has announced
that it will be implementing S3 Passenger, the dynamic pricing, inventory management,
and reservation system offered by Sqills, a Siemens Mobility
subsidiary. Snälltåget
and Sqills have opted for a phased approach in terms of
implementation: The Swedish operator will benefit from a short time-to-market
while adding more functionalities in the months after go-live. One feature that
Snälltåget will be using from the start is the support for cross-operator
cooperation as a way for providing through tickets. This will further improve
passenger comfort when booking long-
distance trips. S3 Passenger is based on the
Software-as-a-Service (SaaS) model and is part of the open, digital business
platform, Siemens Xcelerator, that enables customers to accelerate their
digital transformation easier,
faster and at scale.
- Sinumerik One is in operation at the BMW Group plant in Steyr, Austria
- High performance through integrated Simatic S7-1500F
Siemens supplies automation hardware and software to the BMW Group. The automation solution includes, among other things, the new generation of the Sinumerik One CNC control, which offers digital possibilities to increase productivity in production. The new automation portfolio will be used at the Steyr production plant in Austria to produce the electric drive housing. It will also help to transform production for the digital age. Siemens and the BMW Group have a long-standing partnership. The success of both companies is based on driving innovation and developing forward-looking technologies, while at the same time focusing on sustainability.
- ‘Digirail’ project to modernize Finland’s train
control system
- Siemens Mobility selected to equip first phase
with European Train Control System Level 2 and Hybrid Train Detection
- Finland's first
implementation of the European Train Control System drives
rail digitalization
Siemens Mobility will upgrade the
first section of Finland's rail network under the Finnish government's
"Digirail project", which involves renewing the country's train control system. The contract was
recently awarded and includes the installation of the European Train Control
System Levels 2 [ETCS L2] and the Hybrid Train Detection [HTD] for the first
time in Finland on the 191-kilometer stretch between Lielahti and Rauma-Pori. This marks another milestone in the
implementation of Siemens
Mobility's latest interlocking and radio block center technology on the new DS3
platform, which is entirely based on commercial-off-the-shelf [COTS] hardware. The
new train control system aims to increase the network's capacity, improve
punctuality, minimize disruptions, and enhance the safety of operation. It will
pave the way for a more sustainable, efficient, and safe railway network and is
expected to be in commercial service by 2027.
City of Hamburg, Deutsche Bahn, and Siemens
Mobility sign cooperation agreement for Digitale S-Bahn Hamburg 2.0New
intelligent operations control system to be tested until UITP Congress 2025Partners jointly invest 35 million euros
(Hamburg, July 18,
2023) With the Digitale S-Bahn Hamburg, train travel will become even more
environmentally friendly in the future. Deutsche Bahn (DB), the city of
Hamburg, and Siemens Mobility are introducing a new intelligent operations
control system for the Digitale S-Bahn in Hamburg, aiming to reduce the trains'
power consumption by up to 30 percent. The system will be tested until the UITP
World Congress 2025. The project, costing 35 million euros, is jointly funded
by DB, the city of Hamburg, and Siemens Mobility. A cooperation agreement for
the Digitale S-Bahn Hamburg 2.0 was signed by representatives of the partners
today.
- Brightline
to implement Sqills S3 Passenger system
- Implementation
to support service expansion to Orlando
- Increased
capacity, improved passenger experience
Brightline will begin implementing S3 Passenger, the inventory,
ticketing, and reservation system offered by Sqills, a Siemens Mobility
subsidiary, beginning with revenue service connecting Orlando. Brightline currently
operates in Florida between Miami, Aventura, Fort Lauderdale, Boca Raton and
West Palm Beach with its Orlando station beginning service in 2023.
- Performance optimized, easy to use and future-proof servo drive system
- Flexible and compact – scalable depending on the application
- Easy engineering thanks to integration in TIA, integrated web server and one-button tuning function
With Sinamics S200, Siemens is launching a new servo drive system designed
for a variety of standard applications in the battery, electronics as well as other
industries. It consists of a precise servo drive, powerful servo motors and
easy-to-use cables and offers high dynamic performance. Applications that
require precision in speed and torque, such as winding and unwinding machines in
battery manufacturing and cell assembly, particularly benefit from the new
servo drive system. For this purpose, Sinamics S200 offers optimized speed
ripple, cogging torque compensation, 17/21-bit ST and 21-bit MT encoders, and
cycle-synchronous communication for optimized performance by
Profinet IRT in minimum 250us.
- Y-turning and Advanced Rapid Movement for even more machine tool productivity
- Reduced Dynamic Mode reduces wear and increases availability
- End-to-end keyboard and machine control panel portfolio from 15 to 24 inches
Siemens is expanding its
offering around the Sinumerik One "digital native" CNC. The new CNC
generation from Siemens, which was introduced to the market in 2019, is also
coming up with innovations in software and hardware this year. With the new
Sinumerik V6.20 software, there are new technology functions for the Sinumerik
One that simplify operation, reduce machine wear, and increase productivity.
Siemens is thus demonstrating once again how the powerful Sinumerik One machine
tool control system can be optimally used for digital transformation in a
highly productive, flexible, and modular way.
- Acquisition strengthens Siemens Mobility's
position as a leading software supplier to rail customers
- Optrail S.r.l. provides algorithms for a new
generation of optimization-based Traffic Management Systems for rail
Siemens
Mobility has completed the acquisition of Optrail S.r.l., an Italian-based
technology company, that provides unique algorithms for Traffic Management
Systems – TMS – based on mathematical optimization methods and operations
research. The acquisition complements Siemens Mobility’s existing Train
Planning System – TPS – portfolio and strengthens its position as a leading
supplier of software solutions to rail customers. Optrail
will remain based in Rome, Italy, and its technology will be integrated into
Hacon’s existing TPS products. Hacon, a Siemens Company, is based in Hanover,
Germany, and an essential part of Siemens Mobility’s software unit.
- New V6 software generation with new functions like a single positioner to reduce the load of the controller, and EtherNet/IP to allow third-party controllers to be connected
- Simulation via DriveSim Advanced enables virtual commissioning in advance, ensuring drive process requirements are met efficiently and cost-effectively
- New hardware architecture with functional enhancements like a second encoder interface and 3C3 (H2S and SO2) coating increases precision and robustness
Siemens is innovating the well-established Sinamics S210 servo drive system with a new hardware architecture and new V6 software generation that expand the system's range of applications. The servo drive system is especially suitable for applications with high dynamics in the power range between 50 W and 7 kW: for example, machines for packaging, pick & place applications, and digital printing.
- Siemens presents a new CNC for woodworking machines at the Ligna
- Sinumerik MC is the open CNC for customized processing machines
At the Ligna Woodworking Trade Fair 2019, Siemens is showcasing the Sinumerik MC control as a universal, open CNC system. Its optimized motion control, high-performance automation and the integrated Windows 10 operating system make it the ideal control, especially for wood, glass and stone cutting machines. With its open operating concept, the control system is also suitable for additive manufacturing, adhesive application, plate cutting, straightforward grinding, and laser or water jet cutting.