- Enhanced reliability and efficiency through easier energy monitoring without data cables
- Suitable for the transmission of more than double the electricity of comparable systems
- Modular design for flexible planning and cost-effective expansion
At this year’s Light+Building, Siemens Smart Infrastructure is introducing LData, a busbar trunking system specially designed for data centers wanting to improve their efficiency, availability and adaptability. The more internet traffic, mobile users as well as Internet of Things connections increase, the more data has to be processed. That is why high-performance data centers are emerging as the backbone of a digital society. These data centers must offer the highest degree of availability to protect critical data as well as business-critical applications and industrial processes. At the same time, they must be energy efficient as well as easy to plan, install and expand. The energy distribution system plays a major role in this regard.
- New devices for electrical installations in industrial and infrastructure environments with a lower nominal current of 0.1 to 0.4 amperes
- Firmware update with improved control and diagnostic functions
- Failsafe group shutdown function without additional wiring
Siemens Smart Infrastructure is adding four new devices to its portfolio of Simatic ET 200SP motor starters, which can be used to start electric drives with a power output from 0.1 to 0.4 amperes (A). These types of drives are found in fans and coolant pumps, for example. The compact motor starters are installed in control cabinets and are designed to start single and three-phase motors of machines and systems, protecting them against overloads and short-circuits. They are each available in standard and safety variants.
- Safer and more efficient: Catania Airport is updated with integrated building automation by Siemens
- More reliable and accurate fire detection using Sinteso connected to the Desigo CC building management software
- Cloud-based Navigator software to optimize energy consumption
With almost ten million passengers in 2018, Catania Airport is continuing to grow, solidifying its number one position in southern Italy. This makes the hub an increasingly important strategic part of the Mediterranean aviation network. As a result, however, it faces greater security and energy efficiency challenges. This is the context in which the Sicilian airport made the decision to entrust Siemens with its integrated building automation project, intended to increase security levels and monitor overall energy consumption at the hub.
- Spectrum Power ADMS to provide reliable energy supply for 1.5 million people
- One multi-site system to handle all voltage levels
Hafslund Nett, Norway's largest grid company has contracted Siemens to supply a new Advanced Distribution Management System (ADMS) for the operation of the regional power grid in Akershus, Oslo and Østfold. The fully integrated grid operating center will enable monitoring and control of the complete power grid covering all (high-, medium-, low-) voltage levels. At the same time, it will allow easy integration of third-party IT/OT systems, such as customer information systems, workforce management or geographical information systems. The project is expected to be operational at the beginning of 2022.
- Siemens successfully completed the first phase of its shallow water test of the Subsea Power Grid.
- The development program was conducted in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge.
- This will be the world's first Subsea Power Grid for medium voltage power distribution using pressure compensated technology.
Siemens has successfully concluded the first phase of its Subsea Power Grid shallow water test in Trondheim, Norway. Siemens, in collaboration with industry partners Chevron, Equinor, ExxonMobil, and Eni Norge, is in the final stages of a program to develop a barrier-breaking system that will become the world’s first Subsea Power Grid designed for distribution of medium voltage power using pressure compensated technology.
Siemens has received an order from the regional grid operator EWE Netz GmbH to supply the key components of a Siharbor shore power supply system in Cuxhaven. The order includes the complete transformer station as well as the cable feed system for ro-ro (roll-on/roll-off) ships. The plant owner will be the northern German Gesellschaft für Hafeninfrastruktur Niedersachsen Ports (NPorts). With a power output of 630 kilowatts (kW), the plant will supply these ships with electricity during their lay time. They will thus be able to turn off their diesel generators, significantly lowering exhaust gas and noise pollution. The berth is located next to the new factory for wind turbines operated by Siemens Gamesa, which will be the plant's main user in the future. Siemens Gamesa will ship wind turbine components to its sister factory in Hull, UK. The Siharbor system is expected to go into operation by April 2018.
In May 2014 Siemens, together with the public utilities of Mainz, Linde and the RheinMain University of Applied Sciences, has laid the foundation stone for a new type of energy storage system. Now, time has come: By pressing a symbolic button, the Chairman of the Board of Linde Group, Dr. Wolfgang Büchele, Siemens board member Professor Siegfried Russwurm, two board members of Stadtwerke Mainz AG, Detlev Höhne and Dr. Tobias Brosze, and Professor Dr. Detlev Reymann, President of RheinMain University, officially launched a hydrogen production plant at the Energiepark Mainz on July 2, 2015. With the support of the German Federal Ministry of Economics and Technology as part of the Energy Storage Funding Initiative the 17-million-project could be realized. The system, equipped with an electrolyzer from Siemens, will convert surplus electricity from wind farms to hydrogen from now on. In this way, it will be possible to store electricity from renewable sources over longer periods of time. With a peak rating of up to 6 megawatts the plant is the largest of its kind in the world.The principle of electrolysis has been tried and tested for decades. What is special about the Mainz system is that it involves highly dynamic PEM high-pressure electrolysis which is particularly suitable for high current density and can react within milliseconds to sharp increases in power generation from wind and solar sources. In this electrolyzer a proton exchange membrane (PEM) separates the two electrodes at which oxygen and hydrogen are formed. On the front and back of the membrane are precious-metal electrodes that are connected to the positive and negative poles of the voltage source. This is where the water is split. The system in Mainz will thus have a capacity relevant for bottlenecks in the grid and small wind farms.
- Siemens provides sustainable heating, cooling and ventilation solutions and thus, supports partners and customers in the decarbonization of buildings
- One of the highlights will include an energy efficient magnetic expansion valve, with which OEMs can gain up to 21% more heating capacity
- Also being showcased is a heat pump automation system as part of Siemens Xcelerator
At this year's Mostra Convegno Expocomfort (MCE) trade show, Siemens Smart Infrastructure will present a broad range of innovative and sustainable products, systems, and solutions for Original Equipment Manufacturers (OEM) and installers to accelerate the decarbonization of real-estate. The global marketplace and event, that takes place from March 12 to 15 in Milan, Italy, brings together companies and industry experts from the heating, ventilation, air conditioning and refrigeration (HVACR), renewable energy sources and energy efficiency fields.
- Siemens has supplied 200 VersiCharge wallboxes and an intelligent charging management system to the Portuguese Infinity building
- The contract includes SICAM Dynamic Load Management, a solution to use grid capacity in an efficient way
- Hardware and software are part of Siemens Xcelerator, an open digital business platform that enables customers to accelerate their digital transformation
Siemens Smart Infrastructure has supplied and installed 200 VersiCharge wallboxes and an intelligent charging management
system to the Infinity building, one of the tallest residential sites in
Lisbon, Portugal.
- Siemens exhibition at ISH 2023 introduces IoT-based smart building solutions which marks a major shift for sustainable operations
- Addressing simple small buildings as well as complex campuses
ISH 2023, Frankfurt a. M. (Germany),
March 13 – 17, hall 10.2, booth C55