- Buildings connected in a microgrid support decentralized energy markets of the future
- Flexible energy consumption, storage and load balancing
- Ecological benefits for society as well as new revenue streams for buildings customers
Siemens Finland has created a new business to expand its virtual power plant activity: Vibeco (Virtual Buildings Ecosystem) is an innovative approach to increase the benefits of increasingly decentralized energy systems. The heart of the virtual power plant is a software platform, operated by Siemens, that intelligently balances electrical loads from buildings that have been connected in a microgrid, incorporating renewable energy and energy storage.
On the path to the future of energy, decarbonization, decentralization, and digitalization are inextricably linked. The goal, after all, is intelligent, sustainable generation, provision, and use of energy. This requires integrative thinking and an eye for the big picture – from intelligent energy concepts to sector coupling, electromobility, and the integration of renewable energies in the power grid. At The smarter E Europe trade show, Siemens demonstrated how this combination of power generation, storage, distribution, and use functions in practice. The event brought together four exhibitions under one roof covering the core topics for the energy world of the future (Intersolar, Power2Drive, ees, EM-Power). In line with the trade fair motto "Take control: Be energy intelligent!" we presented innovative products and solutions for the grid integration of PV power plants, local energy systems, and for e-mobility ecosystems.
- AnalyzeMyWorkpiece /Monitor enables continuous monitoring of workpiece production
- Quality control takes place immediately during production
- New application extends the range of existing applications for quality assurance
With AnalyzeMyWorkpiece /Monitor, Siemens is extending its software portfolio for machine tools for workpiece quality. The Edge application based on high-frequency data, which will be presented at EMO 2019, enables continuous monitoring of workpiece production in machine tools. Measured values such as position data, torque values or control deviations together with context information, for example the tool currently being used, are acquired from the machine with high frequency and without feedback via Sinumerik Edge. The measured values are compared continuously with a reference model. In the event of deviations that exceed a predefined level, the application logs the result, sends it to the machine tool and enables prompt responses by the operator. This means, for example, that unique process-parallel quality control is supported during production.
- Siemens drives forward digital transformation in the machine tool industry with a brand new Sinumerik generation
- Sinumerik ONE enables seamless interaction between virtual and real world for significantly increased productivity in the production and use of machine tools
- Scalable CNC-portfolio for highest performance requirements and optimum surface quality
With Sinumerik ONE, the first digital native CNC, Siemens is driving forward digital transformation in the machine tool industry. The new controller works with software to create the machine controller and associated digital twin from one engineering system and thus contributes to the seamless integration of hardware and software. Thanks to its seamless interaction between virtual and real world as well as high-performance hardware, Sinumerik ONE is setting new standards in terms of productivity, performance and digitalization. It is the future-proof CNC for machine tools in the increasingly digital world of manufacturing. Both machine manufacturers and machine operators benefit from the universal digital twin for the product, production and performance.
- Slogan: "Digitalization in Machine Tool Manufacturing – Thinking further!"
- New Sinumerik ONE controller generation as a digital native
- Software portfolio for workpiece quality extended to include another Edge app
Under the slogan "Digitalization in Machine Tool Manufacturing – Thinking further!", Siemens is presenting numerous extensions to its Digital Enterprise portfolio for the machine tool industry in around 1700 square meters at EMO in Hanover in Hall 9, Booth H50. The company has already integrated future technologies in its portfolio, such as its new machine tool controller specifically designed for digitalization, Edge and cloud computing, artificial intelligence and additive manufacturing, and is leading the machine tool world to the next level of digital transformation. "With our unique range of digitalization solutions, we are paving the way for the future of the machine tool industry and helping our customers, machine builders and machine users, to find new and more comprehensive ways of using rapidly growing data volumes to increase their productivity, quality and competitive edge", explains Dr. Wolfgang Heuring, CEO of Business Unit Motion Control. The basis for innovative technologies is the availability and transparency of data which can be used to create digital twins – of the product, production and performance – and which map and link together all the steps of industrial manufacturing processes in a virtual environment. "The key is to use this data innovatively and to convert it into valuable knowledge in order to improve performance and flexibility and reduce the time to market", Heuring continues.
At this year's "The smarter E-Europe," Siemens is demonstrating its role in shaping an increasingly decentralized energy landscape. Siemens will show how the digitalization of renewable energy generation, storage and distribution positively impact the energy transition and sustainability goals.
- New firmware adds Fast PTI mode for precise positioning at even higher speeds
- Fast PTI mode comes with auto-tuning function
- Firmware update opens up new applications for Sinamics V90
New functions are being added to the proven Sinamics V90 servo drive system with the V1.11 version of the Sinamics firmware. The Fast PTI mode is now available for the drive system, increasing Pulse Train Input (PTI) performance by 70 percent. This improves the reaction time from the Pulse Train Input command to the actuation of the motor. The improved reaction time opens up new application areas for the Sinamics V90 which require higher dynamic performance such as high speed labeling as well as in the field of LED production (LED pick & place).
- New IP routers and IP interfaces ensure secure data and access-proof KNX communication over IP
- KNX IP Secure devices meet the highest security requirements in smart buildings
- More flexibility in power supply minimizes KNX bus current consumption
Siemens Smart Infrastructure expands the proven Gamma instabus building system with new IP routers and IP interfaces that support the latest KNX IP Secure standard. This extension of the KNXnet/IP protocol enables fully encrypted transmission of data telegrams, thus ensuring secure data- and access-proof communication between KNX IP routers within a single network.