As urban populations continue to grow, the need to provide
reliable and efficient transportation that allows passengers to connect
seamlessly door-to-door becomes more critical. From public transportation to
ride-sharing, bike-sharing and scooter-sharing, passengers are increasingly
looking for options that allow them to select their transportation options on
demand, planning and paying for their commutes in one easy-to-use application.
Together, Siemens Mobility, HaCon, eos.uptrade, Bytemark and Padam are
providing these digital solutions that are making commutes easier and faster.
In September 2012, Munich city utility company (SWM) was the first customer to order the new Avenio for the light rail network of the MVG (Munich transport company). In the meantime, SWM has continually expanded its Avenio fleet.
Siemens Water Solutions successfully installed and started up a Zimpro® wet air oxidation (WAO) system at a global petrochemical company’s olefins plant in the Southern U.S.
The order, received in November 2017, is the second Zimpro® wet air oxidation system supplied to the customer. The first system was supplied in 2004.
The Zimpro® WAO system will treat spent caustic generated in the production of ethylene by destroying odorous and high chemical oxygen demand (COD) pollutants. The system also generates an effluent that can be safely neutralized and sent to a biological treatment plant, where it is further treated for discharge.
Siemens Water Solutions addresses water and wastewater needs of the oil and gas industry with a portfolio that includes physical and chemical separation, biological treatment, and complex hydrothermal technologies.
With six lines and a total route length of 176 kilometers, Riyadh is constructing one of the world’s largest metro projects. Riyadh currently has a population of 6.5 million people which is set to increase to 8.3 million by 2030 due to its rapid urban growth. As part of a consortium with the US company Bechtel and the local construction firms Almabani and Consolidated Contractors Company, Siemens Mobility is responsible for building lines 1 (Blue Line) and 2 (Red Line). Siemens Mobility, as Engineering and Maintenance partner, is supplying the rolling stock for driverless operation. Moreover, the scope includes project management, signaling, power supply, communication systems, depot and workshop equip¬ment, platform screen doors, testing and commissioning and system integration in a turnkey approach.
New research from Siemens Financial services explains how manufacturers are in a race against time to gain competitive advantage from Industry 4.0 investment, before the “tipping point” of majority adoption. A must-read for future focused manufacturing financial managers, the Whitepaper explains how Finance 4.0 solutions are providing practical methods of helping companies to urgently invest in Industry 4.0 and gain early mover advantage.
Ostdeutsche Eisenbahn GmbH (ODEG) has ordered 23 Desiro HC regional trains from Siemens for service on the Elbe-Spree network. The order is worth around €300 million. Delivery of the 21 six-car and two four-car trains is scheduled to begin in the summer of 2022. In January 2019, ODEG was awarded the contract to operate these lines following a Europe-wide tender by Verkehrsverbund Berlin-Brandenburg (VBB).
The Desiro trainsets will be used on the regional express line RE1 (lot 1) connecting Magdeburg with Cottbus via Berlin and Frankfurt (Oder). During rush hours, trains will operate three times an hour between Brandenburg a. d. Havel and Frankfurt (Oder). The four-car Desiros are planned for service on the RE8 line connecting Wismar and Wittenberge with Baruth and Elsterwerda/Finsterwalde via Berlin, as well as on the RB17 line connecting Wismar and Ludwigslust.
The trains have generous space available for bicycles, strollers and wheelchairs and a multipurpose car with a barrier-free WC. Sliding steps enable barrier-free access at stations with 550 mm and 760 mm platform heights. Wider doors than in older trains speed and ease passenger boarding and exiting. Free WLAN on board enhances passenger convenience. A passenger safety system provides live camera coverage of activities in the cars. In case of a conflict or problem, supervisors at the operations control center can communicate directly with the car via loudspeakers. The cars are equipped inside and outside with real-time capacity displays, and this information can also be accessed via the VBB app.
- Real-time data analysis from 29 gas turbines across multiple locations will increase availability, reduce forced outages and enable proactive, prescriptive maintenance
- Digitalization to improve availability, efficiency, productivity and flexibility
Siemens will install state-of-the-art Remote Diagnostic Services (RDS) for GAIL (India) Limited covering 29 gas turbines operating across the Hazira-Vijaipur-Jagdishpur (HVJ) pipeline and the Vijaipur C2/C3 Plant. The scope includes the supply of RDS hardware, site installation and commissioning including remote Operational Service Desk (OSD) and helpdesk services. The OSD will be accessible 24/7, equipped with machine learning tools and manned by technical experts to provide faster, high quality troubleshooting and guidance for problem resolution.
- Designed to optimize customers' asset value and performance for coal and steam-based power plants
- Siemens experts will work alongside customers to co-create solutions that help deliver higher efficiency, reliability and flexibility in operations
Siemens experts will work alongside customers to co-create solutions that help deliver higher efficiency, reliability and flexibility in operationsSiemens has officially opened its new MindSphere Application Center in India. The facility is a state-of-the-art digitalized technology center, supported by Siemens’ MindSphere, an open, cloud-based IoT operating system that lets customers connect machines and physical infrastructure to the digital world and their thermodynamic digital twins.
On September 26, 2017 Siemens and Alstom have signed a Memorandum of Understanding to combine Siemens' mobility business, including its rail traction drives business, with Alstom. The transaction brings together two innovative players of the railway market with unique customer value and operational potential. The two businesses are largely complementary in terms of activities and geographies. Siemens will receive newly issued shares in the combined company representing 50 percent of Alstom's share capital on a fully diluted basis.On February 6, 2019 the European Commission has announced its decision to prohibit the proposed combination of the Siemens and Alstom mobility businesses. As a result of this prohibition, the merger will not proceed. Siemens and Alstom regret that the remedies they offered, including recent improvements, have been considered insufficient by the EU Commission.