Highlighting its commitment to supporting Pakistan in meeting its growing power needs, Siemens has announced the signing of a long-term service agreement with Punjab Thermal Power (Private) Limited to provide comprehensive maintenance, parts and repair services for Punjab Power Plant Jhang for the next 12 years. The agreement includes Siemens' Power Diagnostics, part of the company's "Digital Services for Energy" portfolio of data-driven solutions.With the fifth-largest population in the world, Pakistan is working to spur socio-economic development by delivering reliable and efficient power supply to industries and homes. Located in Haveli Bahadur Shah, Punjab Power Plant Jhang, is expected to add 1.3 gigawatts (GW) to Pakistan's grid, making it one of the largest gas-fired, combined cycle power plants in the country. It will also see the first deployment of Siemens' SGT5-8000H gas turbines in the country, selected for their high power output and record-breaking efficiency. Anticipated benefits of the agreement include increasing the availability of the power plant and reducing the maintenance costs. The agreement covers all the scheduled and un-scheduled outage services for two SGT5-8000H gas turbines, generators, related auxiliaries as well as the supply of spare parts and field services."Pakistan's energy sector is undergoing a transformational period to meet the increasing demand of electricity. We are very proud to contribute to this significant project," said Gianluigi Di Giovanni, Senior Executive Vice President of Siemens Power Generation Services in the Middle East. "With our services, cross-fleet experience and digital capabilities, we look forward to bringing value and on-ground support to Punjab Thermal Power, helping maximize the potential of the plant's overall operations."Siemens' Power Diagnostics use advanced data analytics to help predict and eliminate unplanned downtime, and improve power plant productivity by identifying operational challenges in advance. It will also allow the power plant's team to manage outages more efficiently.The current agreement builds on Siemens' contributions towards strengthening Pakistan's power sector. It comes three months after the company signed the largest ever power generation contract in the country to provide a complete power island solution for Punjab Power Plant Jhang.
Building on its commitment to supporting the energy infrastructure in Sudan, Siemens has signed a long-term agreement with the Sudanese Thermal Power Generating Company (STPGC) to provide service and maintenance for the power generating assets and related components operating at the 337 megawatt (MW) Port Sudan and 502 MW Garri power plants.
On January 24, 2018, the most powerful high-voltage direct-current (HVDC) transformer began its journey from the transformer factory in Nuremberg, Germany, to China. The transformer will first be transported to the harbor in Nuremberg by special heavy load transporter, where it will be loaded onto a ship. Its journey will take it to Rotterdam via the Main-Danube Canal, and from there it will be shipped to China, where it will arrive after several weeks on the high seas. In July 2016, Siemens received an order to manufacture four transformers of this type. About a year later, the world’s first 1,100 kV transformer was completed and successfully passed the tests in the testing facility. The enormous dimensions of the transformer – 37.5 meters long, 14.4 meters tall, and 12 meters wide – posed a logistical challenge for the team. In operation, the transformer weighs just under 900 tons and its efficiency is well above 99% of the rated power. For the first time, the transformer will enable a high-voltage direct-current (HVDC) transmission with low losses over a record distance of 3,284 kilometers with a transmission capacity of 12 gigawatts. HVDC transformers are part of the converter station that convert alternating current into direct current at the beginning of the transmission line and convert it back again at the end of the line. The conversion from alternating current to direct current helps to transmit energy over long distances with low losses. Transformers are key components of an HVDC line: Thanks to the transformer, the Changji-Guquan project will be able to transmit direct current with a huge 1,110 kilovolts for the first time in the world. The new transformer not only makes the transmission of this record voltage level possible, but it is also the world’s most powerful tested transformer with a capacity of 587 megavoltamperes. Siemens has thus achieved a new dimension in high-voltage direct-current transmission. The HVDC line between Changji and Guquan will be operated by State Grid Corporation (SGCC), a Chinese grid operator. The connection is expected to begin operation in 2019.
Scandinavia is the first region in the world to rely increasingly on battery-powered and thus environmentally-friendly technologies in the shipbuilding industry. After "Ampere", the world's first electrical ferry in Norway, and a follow-up order of the Finnish shipping company FinFerries, Siemens has now received an order from Norwegian ferry operator Fjord1. Ampere was put into operation in Norway in May 2015, and has traveled a distance equivalent to more than 1.5 times around the equator. With the change from diesel propulsion to battery, Norwegian ship owner Norled has reduced the cost of fuel by 60 percent. Now Siemens has tailor-made a suitable technical solution for Fjord1. With this contract, the first four battery-driven ferries in the world will run on technology developed and manufactured by Siemens.
"Elektra" - the newest member of the electric ferry fleet: In June 2017, the Elektra began regular operation between Nauvo and Parainen in the Turku archipelago. Battery packs, which are charged via the land-based charging stations in the harbor for use by the ferry, serve as the primary source of energy, with Diesel engines used as emergency power units. The Elektra is also Europe's largest car ferry. At nearly 98 meters long and 16 meters wide, the Elektra can transport up to 90 cars per trip. The ferry purchased by FinFerries will now be traveling this route every 15 minutes. The batteries will be charged in roughly five minutes while cars move off and onto the ferry. The two lithium-ion batteries each have a capacity of 530 kWh.
In many areas of the world, existing power infrastructure is stretched to the limit by growing demand for electricity. Reliable power supply systems are a major enabler of economic development, yet needs are growing at a pace faster than the ability to erect conventional power plants. The task at hand in these regions is to deploy efficient mobile power generating capacity quickly to fuel economic development. In some cases the need is temporary, and after some time the mobile power plant might be relocated to a different location to perform a similar duty.
Siemens has now specially developed its SGT-A45 TR gas turbine for this rapidly growing market – a new aero-derivative gas turbine integrated into a mobile unit that delivers an electrical output of up to 44 megawatts, can be installed and commissioned in less than two weeks and begin generating electricity immediately. This light-weight gas turbine offers outstanding power density, high fuel efficiency and good operational flexibility, making it an ideal choice for customers who urgently need power and regions with less developed infrastructures.
Demonstrating the company's commitment to supporting Iraq's power sector, Siemens has expanded an existing service agreement with KAR Group in Iraq to provide comprehensive operations and maintenance (O&M) for two newly added SSC5-2000E power plant units at the Khormala plant in the Kurdistan region.The 930-megawatt (MW) natural gas-fired power plant meets nearly 30 percent of the power demand targeted by the Kurdistan Regional Government (KRG), supplying more than four million Iraqi people with reliable electricity. The extension of the service agreement is set to improve operational flexibility, availability, and performance of gas turbines for the next 15 years.The agreement between Siemens and KAR Group aligns with Iraqi energy production goals. According to the Mena Power Report 2017, the current power demand in Iraq stands at 21GW and is growing faster than supply. The Kurdistan Regional Government plans to increase capacity by building new power plants and increasing the efficiency of existing facilities."With more than 20 years of experience in O&M of power plants, we currently manage approximately 2,800 MW across the Middle East and North Africa region and over 16,000 MW globally," said Gianluigi Di Giovanni, Senior Executive Vice President of Siemens Power Generation Services in the Middle East. "Our global resources and fleet expertise enable us to provide complete plant services and management. The plant is truly a landmark project, supporting the development goals of the Kurdistan region. That's why we are proud to expand our collaboration with KAR Group to deliver reliable and stable electricity supply to people's homes."The Khormala multi-year agreement with Siemens covers the operation and maintenance of six SGT5-2000E gas turbines, six SGen5-100A generators along with the associated auxiliary and ancillary systems. It also includes the implementation of Siemens Power Diagnostics®, which is part of the company's "Digital Services for Energy" portfolio, to improve asset visibility, reliability and availability.Siemens data-driven services enable valuable data from different assets to be analyzed. From there, data is transformed into actionable insights—such as diagnostics, troubleshooting and condition forecasting—that can help improve plant reliability and reduce downtime. In addition, the data processed by Siemens Power Diagnostics® can help balance maintenance costs, improve inspection intervals and provide invaluable insights into operational risks.Siemens has managed the operation and maintenance of Khormala since 2013 under a multi-year services agreement. Currently, the company has more than 40 personnel on-site managing the power plant on behalf of KAR Group.
Siemens and The AES Corporation announced on July 11, 2017 their agreement to form a new global energy storage technology and services company under the name Fluence. The joint venture will deliver the Advancion and Siestorage energy storage platforms and will continue to develop new storage solutions and services. Fluence will empower customers around the world to better navigate the fragmented but rapidly growing energy storage sector and meet their pressing needs for scalable, flexible, and cost-competitive energy storage solutions. Its global headquarters will be located in the Washington, DC area with additional offices located in Erlangen, Germany and other cities worldwide. The transaction is expected to close in the fourth quarter of calendar year 2017, subject to regulatory and other approvals.
For many holiday-makers, a cruise on board a luxury liner is right up at the top of their wish list. No wonder that the leisure cruising market has been booming for many years. In the past year alone, more than 20 million cruise passengers embarked in locations around the world – and the trend is upwards. This year saw the launch of the Aida shipping company's ninth ship fitted out with automation technology from Siemens.
Building on its commitment to innovative power plant solutions, Siemens has been awarded a contract from Colbún S.A. to upgrade the Central Termoeléctrica Nehuenco-I plant with Siemens' Power Plant Automation T3000 Cue (SPPA-T3000) system. The 368-megawatt (MW) combined cycle power plant is located in Quillota, Valparaíso Region, in Chile and provides electricity to approximately 350,000 homes in the region.