Wiener Linien commissioned Siemens at the end of 2017 with the delivery of 34 fully automated metro trains. The contract also includes the maintenance of the trains for a period of 24 years and an option for an additional eleven trains. The "X cars" will be operated fully automated on the new U5 line in Vienna beginning in 2024. The trains can also operate semi-automated or manually on previously existing lines. Delivery of the trains is scheduled to begin in mid-2020 and to be completed by 2030. The trains will be manufactured at the Siemens factory in Vienna.
As urban populations continue to grow, the need to provide
reliable and efficient transportation that allows passengers to connect
seamlessly door-to-door becomes more critical. From public transportation to
ride-sharing, bike-sharing and scooter-sharing, passengers are increasingly
looking for options that allow them to select their transportation options on
demand, planning and paying for their commutes in one easy-to-use application.
Together, Siemens Mobility, HaCon, eos.uptrade, Bytemark and Padam are
providing these digital solutions that are making commutes easier and faster.
In September 2012, Munich city utility company (SWM) was the first customer to order the new Avenio for the light rail network of the MVG (Munich transport company). In the meantime, SWM has continually expanded its Avenio fleet.
Siemens and Rolls-Royce signed an agreement on June 18, 2019 at the International Paris Air Show in Le Bourget (France) for the sale of Siemens' eAircraft unit. Closing is subject to the usual conditions and is expected to take place in late 2019.
His Royal Highness The Prince of Wales has visited the headquarters of Siemens AG while on a trip to Germany. The Prince's trip is focused on the bilateral relations between the United Kingdom and Germany. During his roughly 45-minute tour of the company's headquarters, Prince Charles learned about topics such as sustainability, the new world of work and Siemens' Cents4Sense initiative. He also signed the company's visitors' book.
With six lines and a total route length of 176 kilometers, Riyadh is constructing one of the world’s largest metro projects. Riyadh currently has a population of 6.5 million people which is set to increase to 8.3 million by 2030 due to its rapid urban growth. As part of a consortium with the US company Bechtel and the local construction firms Almabani and Consolidated Contractors Company, Siemens Mobility is responsible for building lines 1 (Blue Line) and 2 (Red Line). Siemens Mobility, as Engineering and Maintenance partner, is supplying the rolling stock for driverless operation. Moreover, the scope includes project management, signaling, power supply, communication systems, depot and workshop equip¬ment, platform screen doors, testing and commissioning and system integration in a turnkey approach.
Siemens has developed a comprehensive concept for energy systems worldwide – the first such concept that takes into account and brings together not only technology but also the areas of regulation and social engagement. The Energy Value Charter aims to create customized solutions that will empower countries to make their energy systems fit for the future. The concept encompasses suggestions for implementing sustainable power-generation technologies, together with recommendations on how legal frameworks must be adapted to ensure that the full potential of these technologies can be tapped. In addition, the concept specifies options for promoting social engagement, such as work-study programs, as well as for refinancing infrastructure while simultaneously reducing greenhouse gas emissions. Siemens presented the concept at the 2019 Energy Transition Dialogue in Berlin, in the presence of energy ministers from a range of countries.
Siemens developed the concept to create a global framework for energy solutions for its businesses. With its Energy Value Charter, the company wants to enter into a dialogue with governments in order to shape energy systems in such a way that they provide the basis for economic growth, social engagement and sustainable development.
New research from Siemens Financial services explains how manufacturers are in a race against time to gain competitive advantage from Industry 4.0 investment, before the “tipping point” of majority adoption. A must-read for future focused manufacturing financial managers, the Whitepaper explains how Finance 4.0 solutions are providing practical methods of helping companies to urgently invest in Industry 4.0 and gain early mover advantage.
Ostdeutsche Eisenbahn GmbH (ODEG) has ordered 23 Desiro HC regional trains from Siemens for service on the Elbe-Spree network. The order is worth around €300 million. Delivery of the 21 six-car and two four-car trains is scheduled to begin in the summer of 2022. In January 2019, ODEG was awarded the contract to operate these lines following a Europe-wide tender by Verkehrsverbund Berlin-Brandenburg (VBB).
The Desiro trainsets will be used on the regional express line RE1 (lot 1) connecting Magdeburg with Cottbus via Berlin and Frankfurt (Oder). During rush hours, trains will operate three times an hour between Brandenburg a. d. Havel and Frankfurt (Oder). The four-car Desiros are planned for service on the RE8 line connecting Wismar and Wittenberge with Baruth and Elsterwerda/Finsterwalde via Berlin, as well as on the RB17 line connecting Wismar and Ludwigslust.
The trains have generous space available for bicycles, strollers and wheelchairs and a multipurpose car with a barrier-free WC. Sliding steps enable barrier-free access at stations with 550 mm and 760 mm platform heights. Wider doors than in older trains speed and ease passenger boarding and exiting. Free WLAN on board enhances passenger convenience. A passenger safety system provides live camera coverage of activities in the cars. In case of a conflict or problem, supervisors at the operations control center can communicate directly with the car via loudspeakers. The cars are equipped inside and outside with real-time capacity displays, and this information can also be accessed via the VBB app.