Siemens is modernizing 15 converter transformers at the Cahora Bassa dam in Mozambique for the operator Hidroeléctrica de Cahora Bassa (HCB). The transformers form part of the HVDC transmission link built in the 1970s to transmit electrical power from the hydropower plant over a distance of 1,450 kilometers. The order volume is about €26 million, and the project as scheduled by Siemens will take three years.
- Siemens and UL Solutions demonstrate a transformative shift from relying
solely on physical tests to reliable integrating digital simulations.
- Reduced costs, accelerated time-to-market and seamless integration of
digital modeling tools will redefine the future of verification.
- Siemens’ digital twin technology breaks through traditional testing
boundaries, serving as a testament to the industrial metaverse’s potential
for reshaping product development possibilities.
For the first time ever, an industrial product has been certified for the United States
after parts of the required tests were conducted through digital simulation. That
simulation was verified and validated with physical testing. This remarkable
achievement is a global first in a national safety-certification process. To make this
advance possible, Siemens collaborated with UL Solutions, an esteemed global
leader in applied safety science. The result is a testimony to the remarkable
accuracy and reliability of modern digital twin simulations. It marks a step forward
into a future in which digital twins and the industrial metaverse streamlines product
development, enhances innovation, safety and accelerates time-to-market.
- Connect Box, part of Siemens Xcelerator, connects, monitors and operates small to medium-sized buildings
- Easy integration of wireless and wired devices into existing building automation systems, building management systems (BMS) or cloud applications
- Increases building operations efficiency, reduces energy consumption and meets regulatory requirements for sustainable and healthy buildings
Siemens Smart Infrastructure has launched
Connect Box, an open and easy-to-use IoT solution designed to manage small to
medium-sized buildings. The latest addition to the Siemens Xcelerator
portfolio, Connect Box is a user-friendly approach for monitoring building performance,
with the potential to optimize energy efficiency by up to 30 percent and to substantially
improve indoor air quality in small to medium sized buildings such as schools, retail
shops, apartments or small offices. Siemens Xcelerator is an open digital business
platform that enables customers to accelerate their digital transformation
easier, faster and at scale.
- Potential reduction of more than 8,000 tons of CO2 annually
- Emissions and noise while berthed can be significantly reduced
- Sustainable solution contributes to climate protection
- 16-megavolt ampere shore power system to supply two ships simultaneously with certified eco-power
The Port of Kiel commissioned Siemens to build Germany’s largest shore power system to date. With a power of 16 megavolt amperes (MVA), the Siharbor solution will supply two ships simultaneously with certified eco-power, for the first time. This will reduce annual CO2 emissions by more than 8,000 tons. The system is expected to go into test operation within the 2020 cruise ship season. Maritime shipping plays a special role in Kiel. The port is the point of departure for cruises and has ferry connections to the Baltic states and Scandinavia. 32 different cruise ships stopped in 174 times at the port facilities in 2018.
- Integration of cutting-edge technologies into the Digital Enterprise portfolio enables flexible and intelligent production
With its Digital Enterprise, Siemens is taking the next step of the digital transformation – on the way to highly flexible modular production. Siemens presents numerous innovations for the discrete and process industries as well as for energy and building infrastructure. The integration of cutting-edge technologies such as edge and cloud computing, artificial intelligence or additive manufacturing into the portfolio offers users new opportunities to achieve more flexible and intelligent production. Communicative networking through Industrial 5G plays a key role.
- Innovative woodworking control system
- Digitalization boosts productivity and flexibility
Under the banner "Digital Enterprise – Thinking industry further", Siemens is showcasing an extensive portfolio of innovative control and automation solutions for digitalizing the entire value chain in the woodworking and wood processing industry at the Ligna 2019 in Hannover from May 27-31, 2019 in Hall 16 at Booth C14.
- Siemens will supply four 400 kV HVDC transformers for cross-channel link
- Efficient 2,000 MW power transmission link between France and the UK will supply up to 3 million homes with electricity
Siemens will deliver four transformers, each with a capacity of 400 kilovolts (kV) and 315 megavolt amperes (MVA), on behalf of the British grid operator National Grid. The grid operator will replace the old transformers in the high-voltage direct-current (HVDC) cross-channel link. The new transformers are quieter, have lower transmission losses and will significantly improve the system's reliability. The HVDC link connects France and England and makes it possible to efficiently exchange energy in both directions. The order includes the supply, installation and commissioning of the transformers for the Sellindge converter station in England. Siemens will complete the work by mid-2019.
- Leading experts in latest HVDC converter and cable technology join forces
- India's first HVDC link featuring state-of-the-art VSC technology
- Transmission link to support Government’s Vision of 24x7 power for all
A consortium between Siemens and Sumitomo Electric Industries Ltd. has been awarded an HVDC order from Indian transmission operator Power Grid Corporation of India (POWERGRID) to supply a high-voltage direct current (HVDC) transmission system. The about 200 km long HVDC connection will be India’s first DC link featuring voltage-sourced converter (VSC) technology. VSC is the latest innovation in HVDC technology offering a very stable and highly flexible reactive power control independent of active power control and additional features to support the AC systems like blackstart capability. Furthermore, this solution is ideal to be combined with XLPE cable technology. Siemens will be supplying two converter stations with two parallel converters, each rated 1000 Megawatts (MW), featuring its VSC HVDC technology while Sumitomo Electric will be responsible for the XLPE HVDC cable system in the DC circuit. The combined order volume for Siemens and Sumitomo Electric is approximately $520 million. The grid connection is scheduled to go into operation in the first half of 2020.
Siemens has received an order from the regional grid operator EWE Netz GmbH to supply the key components of a Siharbor shore power supply system in Cuxhaven. The order includes the complete transformer station as well as the cable feed system for ro-ro (roll-on/roll-off) ships. The plant owner will be the northern German Gesellschaft für Hafeninfrastruktur Niedersachsen Ports (NPorts). With a power output of 630 kilowatts (kW), the plant will supply these ships with electricity during their lay time. They will thus be able to turn off their diesel generators, significantly lowering exhaust gas and noise pollution. The berth is located next to the new factory for wind turbines operated by Siemens Gamesa, which will be the plant's main user in the future. Siemens Gamesa will ship wind turbine components to its sister factory in Hull, UK. The Siharbor system is expected to go into operation by April 2018.
- Booth slogan "Discover the value of the Digital Enterprise"
- Digitalization enhances flexibility, speed, efficiency and quality
- Innovations in power distribution, automation and drive technology as well as industrial software
- MindSphere extended to include partnerships, apps and interfaces
At the Hannover Messe 2017, Siemens will be demonstrating how industrial companies of all sizes can benefit from the digital transformation. The central focus of the 3,500-square meter booth in Hall 9 will be on the company's further extended portfolio for the achievement of end-to-end digitalization, known as the "Digital Enterprise". An array of examples from practice will allow visitors to experience applications and innovations demonstrating the competitive benefits to be gained by merging the real and the virtual worlds. These include greater flexibility, efficiency and quality as well as a reduced time-to-market. The examples on show range from smart energy management systems through customized food and pharmaceutical production to industrial-scale additive manufacturing based on innovative automation and drive technology. Siemens is also driving forward the expansion of its cloud-based, open IoT operating system MindSphere with the addition of new partnerships, interfaces and apps.