Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens builds Germany’s largest “power outlet” for ships for Port of Kiel 

“By building this new shore power system we will actively support the climate objectives of the Schleswig-Holstein state capital,” said Dr. Dirk Claus, managing director with the Port of Kiel. “The shore connection system lets us draw electricity from renewable energy sources, both for cruise ships docked at the Ostseekai and for the ferry at the Schwedenkai. We thereby take on a leading role and consistently implement our Blue Port concept for a sustainable and future-oriented development of the Port of Kiel. In future 60 percent of the energy demand required by the ships entering Kiel will be covered by climate-friendly shore power as diesel generators will be shut down while they are berthed.”
The Siemens installation consists of one substation with four Geafol cast resin transformers, four air-insulated medium-voltage Nxair switchgears as well as one 16-MVA frequency converter. The cast resin transformers with a rated power of six and 16 MVA are especially suited for challenging environmental conditions, such as the salty air present at the port. The switchgear is robust and has a compact design, making it suitable for this application.
For an uninterrupted and efficient power supply of the mooring ships the Siemens converter system “Siplink” is used. It features a frequency converter and a software for central controlling of the two berths. With the system, two medium-voltage networks with different frequencies can be connected. In this case the local distribution grid with 50 Hz and the ship’s onboard electrical system with 60 Hz. Siplink synchronizes both networks and takes over the power supply automatically within a few minutes. In addition, it coordinates the energy supply of the ships’ two networks so that power can be supplied to both simultaneously.
“With this set up, we are able for the first time to supply two ships simultaneously with the necessary 60-Hz onboard frequency by means of one shore power system,” said Axel Mohr, head of sales for Distribution Systems, Region North, at Siemens Smart Infrastructure. “We’re excited to support the Port of Kiel with this sustainable solution, thereby taking on a leading role in Europe together. Such systems will become increasingly important in the future, also outside of Germany, as climate protection goals are implemented.
With its “Master Plan for 100% Climate Protection”, the City of Kiel has an ambitious roadmap to be CO2-neutral by 2050. The new shore power system at the Port of Kiel aims to support this goal with the reduction in CO2 emissions it will bring. The shoreside power supply installed by Siemens in the spring of 2019 at the Norwegenkai has already started operations. To date, it has helped slash CO2 emissions by about 1,000 tons.
For further information on Siemens Smart Infrastructure, please see
www.siemens.com/smartinfrastructure
For further information on Siharbor shore connection, please see
www.siemens.com/siharbor
Siemens Smart Infrastructure (SI) is shaping the market for intelligent, adaptive infrastructure for today and the future. It addresses the pressing challenges of urbanization and climate change by connecting energy systems, buildings and industries. SI provides customers with a comprehensive end-to-end portfolio from a single source – with products, systems, solutions and services from the point of power generation all the way to consumption. With an increasingly digitalized ecosystem, it helps customers thrive and communities progress while contributing toward protecting the planet. SI creates environments that care. Siemens Smart Infrastructure has its global headquarters in Zug, Switzerland, and has around 72,000 employees worldwide.
Read more
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for more than 170 years. The company is active around the globe, focusing on the areas of power generation and distribution, intelligent infrastructure for buildings and distributed energy systems, and automation and digitalization in the process and manufacturing industries. Through the separately managed company Siemens Mobility, a leading supplier of smart mobility solutions for rail and road transport, Siemens is shaping the world market for passenger and freight services. Due to its majority stakes in the publicly listed companies Siemens Healthineers AG and Siemens Gamesa Renewable Energy, Siemens is also a world-leading supplier of medical technology and digital healthcare services as well as environmentally friendly solutions for onshore and offshore wind power generation. In fiscal 2019, which ended on September 30, 2019, Siemens generated revenue of €86.8 billion and net income of €5.6 billion. At the end of September 2019, the company had around 385,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more
Reference Number: PR201912065723en

Contact

Anna Korb

Smart Infrastructure

Freyeslebenstr. 1
91058 Erlangen
Germany

+49 9131 173 663 7

Christian Stuart Wilson

Siemens AG

Werner-von-Siemens-Str. 1
80333  Munich
Germany

+49 (89) 636-22642