- Re-use of domain-specific simulation models
- Standardized interfaces for more system openness
- Real-time simulation of systems and machinery
Siemens has extended its Simit simulation platform for virtual commissioning and operator training to include numerous new functions. The additions in Version 10.1 improve the simulation of automation applications through the re-use of various domain-specific simulation models over the entire lifecycle of manufacturing and process systems. Improved performance, openness and flexibility make the solution even easier to use, supporting the user in the creation of a comprehensive and integrated simulation.
- Simit Unit Administration integrated into the Simit user interface
- Simplified configuration of PLCSIM advanced coupling
- Bulk engineering using Chem Basic Library spreadsheet calculation – for chemical and pharmaceutical plant simulation
- Data transmission now also via OPC UA client coupling
Siemens has upgraded its Simit simulation platform for virtual commissioning and operator training with a new release. Version 9.1 enables Simit to also be used for virtual commissioning and operator training in modular plants, speeding up actual commissioning by as much as 60 percent and reducing unwanted standstill periods to a minimum, particularly during plant conversion and migration processes. Simit can also be used to implement a realistic operator training system. Version 9.1 comes with an array of innovations designed to improve operating convenience, support simulation modeling and contribute towards improved efficiency, openness and flexibility.
- This new technology has been used in one of the biggest desalination plants in the Middle East to analyze, optimize and improve productivity, reducing operating times and finding faults early
- Simit software can be used to simulate field equipment and even the process of an entire plant, in real time.
- The Digital Twin enables virtual commissioning of the plant and remote training for operators.
Siemens has been collaborating with Acciona to create a Digital Twin to improve treatment plant management in one of the biggest desalination plants in the Middle East. This new technology is used to analyze, optimize and improve productivity, reducing operating times and finding faults early.
- New NCU 1740 for higher scalability of Sinumerik One
- Sinumerik Run MyRobot /Direct Control V2.0 and Run MyRobot /Direct Handling V2.0 available for Sinumerik One
- New functions for the Digital Twin in Create MyVirtual Machine and Run MyVirtual Machine
Siemens is expanding its offering for the "Digital Native" CNC Sinumerik One. Two years after its market launch, the technology company is presenting numerous innovations in hardware and software for the Sinumerik One at EMO Milano and the virtual Siemens Machine Tool Days. In this context, Siemens is demonstrating how the powerful machine tool controller can be used in a highly productive, flexible, and modular way and in the best possible way for digital transformation. In terms of hardware, the new NCU 1740 complements the existing NCU 1750 and 1760 as well as the PPU 1740, thus expanding its use in modular machines.
- New Sinamics DriveSim Basic software solution for fast and easy simulation of drive constellations
- Seamless integration of models into commercially available simulation programs
- Validated function units accelerate development phase
With Sinamics DriveSim Basic, Siemens presents a new software solution with which for the first-time drive constellations and their behavior in machines and plants can be simulated, adapted, and optimized. With the new solution, Siemens offers a quick and easy entry into the simulation of drive technology and enables machine and plant manufacturers to accelerate their own development phase.
- Simatic PCS 7 Plant Automation Accelerator V3.0 plant and automation engineering software closes the gap between plant engineering and the process control system
- More powerful, more open version
- Increased system openness based on GSDML and NE150 standards
- Seamless engineering through the integration of various Simatic components
Siemens has extended its engineering software for planners and automation engineers, Simatic PCS 7 Plant Automation Accelerator 3.0 (PAA), to include new functions for even more flexible and integrated automation engineering. With this latest software version, Simatic PCS 7 automation projects can be configured even more easily and efficiently. With Version 3, the PAA software closes the gap between plant engineering and the process control system. The entire plant structure including measuring point data can be generated easily and synchronized between the systems. Automation engineers are supported in all phases from tender preparation (such as bills of material), automatically generated process control data from electrical engineering in the Siemens Simatic PCS 7 process control system (including controlled mass data engineering), to as-is documentation of the process automation.
- Booth slogan: "Digital Enterprise – Implement now"
- The time for implementation has arrived: Focus on industry solutions
- Practical examples and applications demonstrate competitive advantages gained by merging the virtual and real worlds
- MindSphere-Version 3.0 on Amazon Web Services (AWS)
At the Hannover Messe 2018, Siemens will be showcasing a comprehensive series of examples which demonstrate how users can harness the potential of Industrie 4.0 by implementing Digital Enterprise solutions. The focus of the 3,500-square meter booth in Hall 9 is on industry-specific implementation of Digital Enterprise solutions over the whole life cycle. Examples from aerospace, automotive, food and beverage, electronics and machine building as well as the chemical, fiber and oil and gas industries illustrate how companies of any size and from any industry can increase their competitiveness with individual digital solutions – through greater flexibility, efficiency and quality as well as shorter times to market. MindSphere Version 3, concrete use cases and references from Siemens and partners such as OEMs as well as the new global user organization MindSphere World will all be presented in the 700-square meter MindSphere Lounge. Siemens will also be demonstrating how producers can already benefit now from industrialized additive manufacturing, and showcasing Sidrive IQ, the new digital platform for the MindSphere-based evaluation of drive data. Also featured on the Siemens booth will be integrated solutions for industrial enterprises and infrastructure projects in the power utility sector, with the focus on smart energy management using MindApps.
- Extended Digital Enterprise portfolio for discrete and process industries
- Machine and plant builders use digitalization to develop new business models and speed up time-to-market
- Digitalization applications enhance flexibility, efficiency and quality
- Extended "MindSphere-Lounge" over an area of 1,400 square meters
Siemens will be exhibiting at the "SPS IPC Drives" 2017 with an array of applications and examples of how machine and plant builders can sharpen their competitive edge with digitalization. Exhibiting under the banner "Discover the Value of the Digital Enterprise" in Hall 11 across an impressive 4,400 square meter exhibition space, the company will be presenting the latest additions to its Digital Enterprise portfolio. Innovations featured range from new software versions for more efficient engineering through digital drive systems to the open cloud-based IoT operating system MindSphere, which opens up scope for new business models to machine and plant builders. This allows companies across the discrete and process industries to enhance their flexibility, efficiency and speed, for instance by using a "digital twin" to simulate products, production processes or plants and optimize them across the entire value chain.