- High-frequency data exchange between Sinamics drives and the Industrial Edge platform
- Drive System Framework for connectivity, management, and configuration of the Digital Twin
- Paving the way for new business models
As part of
the Digital Enterprise SPS Dialog, Siemens is launching Analyze MyDrives Edge,
its first edge application for drives. The company is thus demonstrating in
concrete terms how edge computing can make Sinamics drive systems even more
intelligent and what benefits users and machine builders can derive from it.
Analyze MyDrives Edge is being launched with basic functionalities similar to
the proven Mindsphere application Analyze MyDrives but will be enhanced with
intelligent features based on high-frequency data exchange. The Edge
application thus allows users of machines and industry applications to perform
complex analyses of data that is already collected in the drive. Machine
learning and AI algorithms on which the edge application is based identify
patterns and detect anomalies and their causes, thus providing timely
indications of any pending machine maintenance. This minimizes downtimes and
reduces the consumption of resources.
- Siemens presents liquid-cooled, robust power conversion system based on proven Sinamics S120 platform
- Grid converter comes with certification in accordance to VDE-AR-N 4110 and with validated simulation model for easy project planning, optimization and integration into the power grid
With Sinamics PCS, Siemens presents a new power conversion system for battery storage applications. The Sinamics PCS grid converter makes locally generated battery power usable for industrial and public power grids. Sinamics PCS controls the charging and discharging process of the battery and helps to handle load peaks and grid disturbances via the battery storage, to store the electricity in an energy- and cost-efficient manner and to bring the energy stored in batteries efficiently and reliably into the grid.
- TIA Selection Tool enables mechanical, electrical and automation planning on a single platform
- Complete standards know-how for electrical planning integrated in one software program
- Time-saving dimensioning of protection and switching devices, including essential design calculations
With “Control Panel Design” Siemens Smart
Infrastructure has integrated new electrical planning features into TIA
Selection Tool, the Siemens configuration and ordering software. This makes
electrical pre-planning completely digital. Now, electrical planners can design
and dimension the main electrical components of a machine quickly, easily, and
in accordance with IEC and UL standards. This reduces the required effort to
perform the task, minimizes potential error sources, and helps machine and
control panel builders improve their competitiveness. TIA Selection Tool is
designed to make it easy and convenient to configure and select all components
of industrial control panels. By integrating the new features, the tool allows
users to design electrical as well as mechanical and automation components
using one set of data and one platform. This lays the foundation for
significantly more efficient development processes, faster lead times, and
smarter electrification solutions for industrial environments.
- Process bus significantly increases level of digitalization in substations
- Faster installation and commissioning
- Improved system reliability
- Benchmark for future-proof design
Siemens Smart Infrastructure has installed process bus technology at the new high-voltage substation in Los Sauces for one of the largest Peruvian distribution network operators, Luz del Sur. This process bus installation with Siprotec merging units and Siprotec protection devices is one of the first fully digitized energy automation system in operation. The new technology sets benchmarks with its future-proof design and will help optimize the entire operation of the power grid.
- Siemens Mobility supplying the complete system technology for C-ITS in Austria
- C-ITS allows for exchange of information between vehicles and the road via ITS-G5 broadcast technology
- ASFiNAG is the first infrastructure provider in Europe to install C-ITS
Siemens Mobility is pleased to announce that it is
partnering with ASFiNAG, the operating authority for the Austrian highway network,
to provide the technology for an intelligent traffic
management system that facilitates the exchange of safety information between
vehicles and the road. The “Cooperative Intelligent Transport System”
(C-ITS) is a next generation traffic management system that uses
broadcast technology to analyze roadway conditions and disseminates information
to motorists relating to traffic jams, accidents, and lane
closures. ASFiNAG is the first infrastructure
provider in Europe to reach the milestone of installing a network connecting
the vehicle and road. The process of implementing the system across 2,200
kilometers of highway and expressway in Austria has already started.
- Growing demand for remote access via public 5G networks for remote maintenance
- Scalance MUM856-1 connects local industrial applications to the public 5G network
- Sinema Remote Connect management platform provides secure access to remote plants and machines
Siemens presents the first industrial 5G router for connecting local industrial applications to a public 5G network. The device will be available in spring 2021. Using the newly developed Scalance MUM856-1, industrial applications such as machines, control elements, and other devices can be accessed remotely via a public 5G network, providing a simple remote maintenance option for these applications using the high data rates offered by 5G. The Sinema Remote Connect management platform for VPN connections can be used to provide easy and secure access to these remote plants or machines – even if they are integrated in other networks.
- Simatic Robot Integrator with Simatic Robot Library makes engineering easy for robots in the TIA Portal
- Universal interface supports integration by all robot manufacturers
- Re-usable program codes thanks to standard programming language
- Time savings of up to 30 percent for engineering
Siemens presents the Simatic Robot Library for the Simatic Robot
Integrator - a new universal robot library for the TIA (Totally Integrated
Automation) Portal, which replaces the previous manufacturer-specific
libraries. The specification has been developed in close cooperation with robot
manufacturers ABB Robotics, Comau, Epson, FANUC, Kawasaki Robotics, KUKA,
Panasonic Industry, STÄUBLI, Techman Robot, Yamaha, and YASKAWA. In future,
users will be able to program most of the robots available on the market in the
TIA Portal using the Simatic Robot Library, and make use of standard operating
concepts based on the Simatic Robot Integrator and Simatic HMI.
We released our financial figures for the fourth quarter and fiscal year 2020 on November 12, 2020. The Press Conference and the Analyst Call were broadcast live.
- At €57.1 billion, revenue at prior-year level; orders decline slightly to €60.0 billion
- At €7.6 billion, adjusted EBITA for Industrial Businesses only slightly below prior-year level; adjusted EBITA margin of 14.3 percent (FY 2019: 14.4 percent) stable at a high level
- Net income of €4.2 billion (FY 2019: €5.6 billion)
- Free cash flow up substantially to €6.4 billion (FY 2019: €5.8 billion); highest level in past ten years
- Vision 2020+ execution successfully driven
- Total dividend of €3.50 per share (FY 2019: €3.90)
- Outlook: Siemens expects moderate rise in net income for FY 2021 despite significant burdens from currency translation effects
In extremely difficult economic times, Siemens AG delivered a strong financial performance in fiscal 2020 (ended September 30), while successfully driving the Group’s historic transformation. Despite the major challenges worldwide caused by the COVID-19 pandemic, Siemens successfully completed its fiscal year with a strong fourth quarter. In appreciation of their outstanding performance during the crisis, Siemens is paying about €200 million in bonuses to its employees worldwide. Shareholders are also to participate in the company’s business success and financial strength. For this reason, the Managing Board and Supervisory Board are proposing to the Annual Shareholders’ Meeting a dividend of €3.00 plus an additional €0.50, for a total of €3.50 per share. Adjusted by ten percent to take account of the market value of the Siemens Energy spin-off, this amount is at the same level as the prior-year dividend of €3.90.
Estonian Railways (Eesti Raudtee) and Siemens Mobility – GRK Rail
Consortium signs a large-scale contract to modernize the railways in Estonia.
Estonian Railways has initiated a very ambitious investment plan which
will take the service quality, traffic management and safety of its rail infrastructure
to a new level by 2030. Between 2020 and 2024 it plans to upgrade the safety
systems on six lines of the rail network and upgrade approximately 50 stations
across the country. To deliver this modernization of the rail safety systems
(CCS), the contract is worth over € 115 million.
The agreement on modernizing the safety systems paves the way for
migrating the entire rail network to the European signalling standard, the
European Rail Traffic Management System (ERTMS / ETCS) in the future. The
agreement relates to the first and second phases of the modernization plan.
Migrating to ERTMS/ETCS is subject to the third phase.