- Compact device providing combined functionality for measurement, monitoring and data transmission
- Separate detection of energy consumption and energy recovery
- Operating hour and switching cycle counters enable preventive maintenance
- Commissioning, measured values and status information via Profinet
Siemens has just launched its SIRIUS 3UG546 DC load monitoring relay on the market. The new device is the most compact of its kind for direct current (DC) applications, enabling simple and precise power measurement. The SIRIUS 3UG546 is unique in our industry: It is the first and only DC load monitoring relay to combine current and voltage measurement, power monitoring, communication and various other useful functions in one single, compact device. Until now, several individual components were required for each of these functions. The innovative new approach saves space and costs.
- Voltage
regulation system for the Kusenhorst substation
- Two-thirds
of the multilevel STATCOMs installed worldwide are from Siemens
In handing over the converter for a state-of-the-art grid
stabilization system for voltage regulation to the German transmission grid
operator Amprion, Siemens is celebrating delivery of its one-hundredth STATCOM
(static synchronous compensator) from the SVC PLUS series. The turnkey
installation will be deployed in the important Kusenhorst node in North Rhine
Westphalia, Germany. STATCOM systems stabilize fluctuations in the grid by
absorbing or feeding in voltage-supporting reactive power, depending on the
requirements. This approach significantly reduces the risk of voltage drops and
blackouts. Two-thirds of the globally installed STATCOM systems with modular
multilevel converter technology (MMC) are from Siemens, making the company the
world market leader in this segment.
- New combined cycle power plant Yerevan 2
- Plant operation and maintenance for 20 years
- Siemens to hold equity in special-purpose project company
Siemens will supply a complete power island for the new Yerevan 2 combined cycle power plant at the existing plant site in the Armenian capital. The company will also operate and maintain the plant for a period of 20 years. Siemens Financial Services (SFS) – Siemens' financing arm – holds a 40 percent share in the special-purpose project company ArmPower founded specifically for this project. Yerevan 2 is the largest single order that Siemens has ever received from Armenia.
- Fully integrated electric-drive centrifugal compression configuration will significantly reduce footprint, capital, and operating costs
- Project marks this Delaware Basin gas plant customer's first order with Siemens
Siemens was recently awarded a contract to provide three residue compression trains for two, 250 million (500 million total) standard cubic feet per day (MMSCFD) cryogenic gas plants in the Delaware Basin. The customer, a key producer in the region and long-term user of reciprocating compression equipment, recognized the benefits of centrifugal compression and looked to Siemens for a fully integrated, turnkey solution that includes compressors, motors, variable frequency drives, and associated process equipment.
- Sinamics Intelligent Operator Panel IOP-2 supports local operation, monitoring, setup, diagnostics and service of all Sinamics G series converters
- IOP-2 also includes applications and functions for advanced setup of the Sinamics G120X
Siemens is extending the functionality of the proven Sinamics IOP-2 for Sinamics G series converters to include the FW V2.3 SP1 firmware update. This improves local setup, operation, monitoring, diagnostics and service of all Sinamics G series converters. The FW V2.3 SP1 update also provides users with the additional benefit of transferring special application functions into the project menu. These application functions are then easily accessible from a list which simplifies the setup of the selected functions using the Quick Start or Advanced Startup options. As a result, users can run their applications without requiring any specialist knowledge of the operating parameters.
- Replacement of gas turbine from another OEM with an SGT-800
- Installation of a SIESTART battery storage solution for blackstart capability
- Customized solution requires comprehensive engineering expertise
Siemens has received an order from BASF Schwarzheide GmbH, a wholly owned subsidiary of BASF SE, to modernize the industrial power plant in Schwarzheide, Germany with key components. The Brownfield Exchange project involves replacing a gas turbine from another original equipment manufacturer (OEM) with a new, highly efficient industrial gas turbine from Siemens as well as servicing this machine for a period of 15 years. In addition, Siemens will install a SIESTART battery storage solution that will enable the entire power plant to start up independently of an external power supply.
- Siemens presents a new CNC for woodworking machines at the Ligna
- Sinumerik MC is the open CNC for customized processing machines
At the Ligna Woodworking Trade Fair 2019, Siemens is showcasing the Sinumerik MC control as a universal, open CNC system. Its optimized motion control, high-performance automation and the integrated Windows 10 operating system make it the ideal control, especially for wood, glass and stone cutting machines. With its open operating concept, the control system is also suitable for additive manufacturing, adhesive application, plate cutting, straightforward grinding, and laser or water jet cutting.
- Innovative woodworking control system
- Digitalization boosts productivity and flexibility
Under the banner "Digital Enterprise – Thinking industry further", Siemens is showcasing an extensive portfolio of innovative control and automation solutions for digitalizing the entire value chain in the woodworking and wood processing industry at the Ligna 2019 in Hannover from May 27-31, 2019 in Hall 16 at Booth C14.