- Load-break switch with vacuum interrupter in secondary current path
- Economical alternative to circuit breakers
- Safety through switching using a consistent operating concept
Siemens Smart infrastructure is continually expanding its portfolio for climate-neutral power distribution. In the medium-voltage switchgear of the blue portfolio, the company has completely eliminated fluorine-based gas mixtures (F-gases) while retaining the compact design and safe, proven operation. An innovative load-break switch equipped with a special vacuum interrupter is the new centerpiece for F-gas-free medium-voltage applications in secondary distribution grids from 12 to 24 kV.
As part of the pebbles research project,
Siemens, the regional utility Allgäuer Überlandwerk (AÜW) and their project
partners are developing a local electricity market using blockchain technology.
Today, the parties launched pebbles’ electricity trading platform, bringing
them one step closer to creating the first local marketplace for optimized
electricity trading based on blockchain. The platform will be utilized in in
the town of Wildpoldsried in the Bavarian Allgäu region of Germany. Now, during
the platform’s demonstration phase, private producers can use an app to market
their electricity directly to local consumers without going through marketers
or traditional grid operators. The market platform also supports flexible power
from battery storage or controllable loads such as heat pumps or charging
stations for electric vehicles. The blockchain technology, which forms the
basis for managing market transactions, is designed to create end-to-end
transparency and trust between users.
- Siemens and Netze BW cooperating on multi-year field test
- First distribution substation with innovative blue GIS 24 kV ring main unit live in Oberallgäu
- Fluorine gas-free Clean Air switchgear and bio-ester transformer boost sustainability
In conjunction with their ongoing research
cooperation, Siemens Smart Infrastructure and Netze BW GmbH, headquartered in
Stuttgart, have co-developed an intelligent and environmentally-friendly distribution
substation. For the first time, the new station combines the F-gas-free 24
kilovolt (kV) ring main unit (RMU) from the Siemens blue GIS portfolio with a
630 kilovolt-ampere (kVA) distribution grid transformer. Instead of mineral
oil, the Eco Design 2-certified transformer uses fully biodegradable, natural
bio-ester oil for insulation. The integrated automation system from the Siemens’
Sicam portfolio is designed for the special requirements of distributed grids
and enables reliable monitoring and control of the grid. The innovative
substation, which will connect the medium-voltage distribution grid and the
low-voltage local grid in the town of Kreuzthal in the Oberallgäu region, is now
being tested under real-life conditions.
- Adaptable modular solution to deal with short-term needs of hospitals, e.g. during epidemic or temporary construction works
- Ergonomic solution ensuring safety of patients and medical staff
- Compliant with healthcare facilities regulations
- Autonomous care units, fast to deploy, deliver high added value
Siemens Smart Infrastructure has teamed up with Toutenkamion Group to jointly develop an agile container system of highly innovative mobile intensive care units, designed to take pressure off hospital infrastructure. The solution was a response to the Covid-19 pandemic, which forced nursing staff, doctors and hospital managers to urgently come up with practical solutions to ensure adequate care was provided to extremely contagious patients, while maintaining other emergency and conventional care. One of the major challenges of the epidemic has been the need to equip and increase the number of resuscitation and intensive care beds.
- Calibrant Energy to bundle latest distributed energy technologies and financing expertise of global leaders Macquarie and Siemens
- The joint venture will create Energy-as-a-Service solutions from a full range of energy technologies for corporate and municipal clients
Macquarie’s Green Investment Group (GIG), Siemens Smart Infrastructure and Siemens Financial Services (SFS) today announced the formation of Calibrant Energy (Calibrant), a joint venture that offers comprehensive onsite Energy-as-a-Service (EaaS) solutions at no up-front cost for its customers, which include corporate and industrial clients, as well as municipalities, universities, schools and hospitals.
- Flexible addition of features via software protects investments
- New protection technologies prevent failures with distributed power supply
- Seamless integration in digital environments
With the new 3WA series, Siemens Smart Infrastructure is updating its Sentron portfolio of air circuit breakers. As a core element of low-voltage switchboards, they reliably protect electrical installations in buildings, infrastructures and industrial facilities from damage caused by short circuits, ground faults or overload faults. At the same time, the new 3WA circuit breakers meet all low-voltage power distribution requirements in digital environments. They support software-based planning and engineering, digital testing and monitoring, and seamless integration in automation and IoT systems. For the first time, upgrades can be completed 100 percent digitally. Users simply download new features from the Internet and add them using an app.
- Hydrogen production solely from renewable energy
- Exclusive hydrogen source for northern Bavaria and the border region in Czech Republic
- Cross-sector use of renewable energy as a model for the future
Siemens Smart Infrastructure and WUN H2 GmbH
signed a contract to build one of the largest hydrogen production plants in
Germany. It will be built in Wunsiedel in the north of Bavaria. With a power
intake of six megawatts in the initial development phase, the plant will run
solely on renewable energy and will be CO2-free. The electrolysis
plant from Siemens Energy will have the capacity to produce over 900 tons of
hydrogen per year in this first phase. When fully expanded, it will be able to
supply up to 2,000 tons. Groundbreaking is scheduled for the end of this year
and commissioning at the end of 2021.
- Built-in sensors, control functions, input/output and flexible power supply in one device
- Open KNX communication for integration from simple to advanced building management systems
- New slim and smooth design with touch buttons and rotary knob
- Fast installation and commissioning with the new ‘PCT Go’ app
Siemens Smart Infrastructure (SI) is
launching its new RDG200 thermostat range for a healthy and productive indoor
climate. Room automation is key for protecting and enhancing the occupants'
health as well as increasing productivity at the same time for a safe return to
work. The new range follows this approach and includes two digital thermostat
variants for temperature and humidity control as well as advanced KNX
communication between sensors and actuators to Siemens’ building management
systems such as Desigo and Synco. This ensures good air quality with peace in
mind to have indoor climate under control. Designed for most commercial
buildings, including hotels, offices and educational buildings, the new RDG200
thermostats support all conceivable energy-saving strategies in rooms for more
cost-efficiency, including occupancy-based
savings via presence detection, key-card reader or system time program as well
as different setpoint limitations. With their modern design and the one-touch
Green Leaf button, the new thermostats display the energy efficiency status and
puts the user in charge of energy savings.
- Siemens Energy Corporate Center in Berlin
- Joint location and structural concept planned with the State of Berlin
- Company's administrative
headquarters remain in Bavaria
Siemens Energy, as a stand-alone company,
will locate its Corporate Center in Berlin. The energy technology company with
worldwide 91,000 employees, which in 2019 generated revenue of €28.8 billion,
is thus returning to its roots: Werner von Siemens and Johann Georg Halske
founded their company in Berlin in 1847 and with the discovery of the
electrodynamic principle in 1866 laid a foundation for today's Siemens Group
and therefore today's Siemens Energy.