Messe Berlin, hub 27, Booth 230, and outdoor area,
September 24th to September 27th, 2024, in Berlin.
- Siemens Mobility’s digital ecosystem
approach, allowing data from different sources to be integrated via APIs, leads
to more capacity and energy reduction
- Innovation
within train procurement: Mireo Smart and Smart Train Lease
- Presenting
the high-speed train Velaro for Egypt
- Siemens Mobility is showcasing its innovations
and solutions in hub27 at booth 230 and in the outdoor exhibition area
Siemens
Xcelerator’s unveiling at InnoTrans 2022 signaled the advent of a truly open
ecosystem for seamless digital collaboration. At InnoTrans 2024, Siemens
Mobility will showcase the rail industry’s huge potential to reduce society’s
overall carbon footprint, with digitalization as a key enabler. This includes optimizing
maintenance, maximizing the use of existing infrastructure, and providing
solutions for seamless travel. One of the biggest barriers to a full-hearted
adoption of digitalization, however, is vast quantities of data locked in
closed systems. The answer lies in accessing these data via standardized
application programming interfaces (APIs) and connecting them with AI-driven
analysis and evaluation tools. As a leading provider of technology, Siemens
Mobility has identified around 100 APIs within the rail ecosystem and has already
fully developed a dozen of them.
- Contract for
locomotives includes their maintenance for 15 years
- XLoad increases
hauling capability for Vectron locomotive
- Operating
approval for Switzerland, Germany, the Netherlands, Austria, and Italy
The Swiss company SBB
Cargo International AG, in cooperation with Südleasing GmbH, has ordered an
additional 20 Vectron multi-system locomotives equipped with the XLoad package.
The locomotives will be leased by SBB Cargo International from SüdLeasing in a
long-term contract with a flexible term. The contract also includes maintenance
of the locomotives by Siemens Mobility for 15 years. The Vectron XLoad package
improves the locomotive’s traction capability in order to increase its hauling
capacity and efficiency. Among other advantages, XLoad enables heavier trains
to be run in single traction on the Swiss north-south axis, eliminating the
need for a second four-axle booster locomotive. The Vectron locomotives have a
maximum speed of 160 km/h.
- Berlin as a pioneer: World’s first installation
of an obstacle detection system on an S-Bahn in daily operation
- Installation and practical testing of an
innovative obstacle detection system in the latest 484 series S-Bahn train
conducted by Siemens Mobility with
S-Bahn Berlin and the Digital Rail Germany (DSD) initiative
- Goal: Develop assistance system for accident
prevention and driverless operation at low speeds
Automated operation is a key function for expanding
rail capacity and strengthening the performance of railways. Working together
with S-Bahn Berlin, Siemens Mobility has installed and will be testing an
obstacle detection system – a key technology component for enabling fully
automated driving – for the first time during regular daily operation.
- U5 and U8 metro lines to receive modern
Trainguard MT train control system for semi-automated (GoA2) operation
- With CBTC, headways can be shortened, and line capacity increased
by up to 30%; conversion to be completed by 2032 during ongoing operations
Siemens
Mobility has won the tender from Berliner Verkehrsbetriebe [BVG] and will
introduce a Communications-Based Train Control System [CBTC] on the U5 and U8
metro lines in Berlin for the first time. The state-of-the-art Trainguard MT CBTC
solution will enable semi-automated operation (GoA2: Grade of Automation) on
the U5 line by 2029 and on the U8 line by 2032, increasing capacity on these
lines by around 30%. Technically speaking, CBTC technology even allows headways
of less than 100 seconds. This technological advance will also significantly
improve the reliability and punctuality of the two metro lines. Siemens
Mobility will carry out the conversion during ongoing operations so that trains
on both lines of Germany’s largest metro system can continue to run
uninterrupted throughout the entire project. The contract has a volume of
approximately 200 million euros, plus additional long-term technology
maintenance contracts.
-
World premiere: Existing GoA4 line upgraded to
latest generation CBTC driverless automation system to boost capacity, reliability,
and efficiency for Paris metro operator RATP on behalf of Île-de-France
Mobilités
- Upgraded
line enables driverless automated train operation along the route doubled
in length, now also connecting Orly Airport to central Paris
- Line
remained in operations throughout the project that will serve one million
passengers daily by 2025
Siemens Mobility and RATP (Régie
autonome des transports Parisiens) have successfully modernized and extended the
automated Line 14 of the Paris metro. This world premiere marks the first
migration of an automated driverless (GoA4 – Grade of Automation) metro line to
the latest generation GoA4 driverless automated system “Trainguard MT CBTC”. The
new system, which was implemented during the past six years during passenger
services, enables more efficient and reliable services on the line that has
doubled in length by 14 kilometers due to extensions to the North and South.
With a remarkable headway of 85 seconds along its entire 28 km route, Line 14
is now the longest line in the Paris network and will eventually accommodate
over one million passengers daily. The expansion enables passengers to travel
from Orly Airport to Paris city center in 20 minutes and from the northern business
districts in Saint-Denis Pleyel to Orly Airport in just 40 minutes. With its
improved capacity, reliability, and efficiency, Line 14 serves as the backbone
of Paris' public transportation system, connecting to the future Grand Paris
Express network. Over six years, more than 250 Siemens Mobility engineers
contributed to this project, with over 500,000 hours of engineering.
- Production capacity increased, workforce expanded to meet growing
demand.
- New gearbox production line inaugurated, competence center for converter
cabinets established.
- Cornellà, an important supplier of traction motors, converters, and
converter cabinets, now produces rail gearboxes.
- Traction components (trademark: MoComp) from Cornellà (Barcelona) used
worldwide by numerous rail vehicle manufacturers.
Siemens Mobility has invested in its Cornellà factory to significantly
expand production capacity and the product portfolio
- DB Regio trains speed at 190 kilometers per hour between Bavaria and Thuringia
- Higher capacity, better service, new travel options to the north and south
Germany’s fastest regional train between
Bavaria and Thuringia is set to go. The new Franconia-Thuringia Express (FTX)
operated by Deutsche Bahn (DB) is inaugurating service on the Nuremberg-Erfurt
high-speed line on June 9, with the scheduled so-called small timetable change.
The modern Siemens trains, ordered by the Free States of Bavaria and Thuringia,
will run at a top speed of up to 190 kilometers per hour. To date, only
long-distance trains have operated on the northern section of the VDE 8.1, the
designation for this new and upgraded line.
- Depot to be expanded to 87,550 m²
- New capacity for meeting growing demand
- 100% system availability thanks to digitalized depot operation
- Creation of attractive jobs in the region
- Up to 250 employees at the location in 2026
Siemens Mobility is investing approximately €150 million to expand its service depot in
Dortmund-Eving to 87,550 m² to meet the growing demand for rail services.
Plans call for constructing an additional 12,300 m² service hall
with storage facility, offices, and workshops to handle the maintenance of
trains up to 400 meters long. Construction
of the new building is scheduled to begin in 2024 and be completed by 2026. The
Siemens Mobility depot in Dortmund previously had a total area of
70,000 m² and will cover 157,550 m² when the project is
completed.
Today,
Brightline announced that Siemens Mobility (Siemens) has been designated the
“preferred bidder” to build train sets for the Brightline West high-speed rail
project that will connect Las Vegas and Southern California. The contract will
include a fleet of ten “American Pioneer 220” (AP 220) train sets to be
manufactured, delivered to Nevada and tested to support Brightline West’s
timeline of initiating service in 2028.